This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc584_3_0_0 [24 May 2023 10:54] Vasileios Bimpikas |
resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc584_3_0_0 [25 May 2023 11:09] Vasileios Bimpikas |
||
---|---|---|---|
Line 105: | Line 105: | ||
\\ | \\ | ||
==== Building the example ==== | ==== Building the example ==== | ||
- | You can build three different versions of the root filesystem; tiny, minimal, ramdisk and full. | + | You can build two different versions of the root file system; minimal and full. |
To build the example images invoke bitbake from within the build directory created previously. | To build the example images invoke bitbake from within the build directory created previously. | ||
<code bash> | <code bash> | ||
- | $ bitbake adsp-sc5xx-tiny | ||
$ bitbake adsp-sc5xx-minimal | $ bitbake adsp-sc5xx-minimal | ||
$ bitbake adsp-sc5xx-full | $ bitbake adsp-sc5xx-full | ||
Line 134: | Line 133: | ||
<code bash> | <code bash> | ||
$ ls tmp/deploy/sdk | $ ls tmp/deploy/sdk | ||
- | adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.host.manifest | + | adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.host.manifest |
- | adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.sh | + | adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.sh |
- | adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.target.manifest | + | adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.target.manifest |
- | adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.testdata.json | + | adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.testdata.json |
</code> | </code> | ||
- | The ''adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.sh'' is a self-extracting archive containing the SDK. | + | The ''adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.sh'' is a self-extracting archive containing the SDK. |
=== Installing the SDK === | === Installing the SDK === | ||
Line 147: | Line 146: | ||
For the minimal image on SC584 | For the minimal image on SC584 | ||
<code bash> | <code bash> | ||
- | $ ./adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.sh | + | $ ./adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc584-ezkit-toolchain-3.0.0.sh |
- | Analog Devices Inc Reference Distro SDK installer version 3.0.0 | + | Analog Devices Inc Reference Distro (glibc) SDK installer version 3.0.0 |
- | =============================================================== | + | ======================================================================= |
- | Enter target directory for SDK (default: /opt/adi-distro/3.0.0): | + | Enter target directory for SDK (default: /opt/adi-distro-glibc/3.0.0): |
- | You are about to install the SDK to "/opt/adi-distro/3.0.0". Proceed [Y/n]? y | + | You are about to install the SDK to "/opt/adi-distro-glibc/3.0.0". Proceed [Y/n]? y |
- | Extracting SDK........................................................................done | + | Extracting SDK................................................................................................................done |
Setting it up...done | Setting it up...done | ||
SDK has been successfully set up and is ready to be used. | SDK has been successfully set up and is ready to be used. | ||
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | ||
- | $ . /opt/adi-distro/3.0.0/environment-setup-cortexa5t2hf-neon-adi-linux-musleabi | + | $ . /opt/adi-distro-glibc/3.0.0/environment-setup-cortexa5t2hf-neon-adi_glibc-linux-gnueabi |
</code> | </code> | ||
Line 196: | Line 195: | ||
;''**Terminal2: OpenOCD**'' | ;''**Terminal2: OpenOCD**'' | ||
:<code bash> | :<code bash> | ||
- | $ sdk_usr=/opt/adi-distro/3.0.0/sysroots/x86_64-adisdk-linux/usr/ | + | $ sdk_usr=/opt/adi-distro-glibc/3.0.0/sysroots/x86_64-adi_glibc_sdk-linux/usr/ |
$ $sdk_usr/bin/openocd -f $sdk_usr/share/openocd/scripts/interface/<ICE>.cfg -f $sdk_usr/share/openocd/scripts/target/adspsc58x.cfg</code> | $ $sdk_usr/bin/openocd -f $sdk_usr/share/openocd/scripts/interface/<ICE>.cfg -f $sdk_usr/share/openocd/scripts/target/adspsc58x.cfg</code> | ||
Where ''<ICE>'' should be replaced with ''ice1000'' or ''ice2000'' depending on your hardware. | Where ''<ICE>'' should be replaced with ''ice1000'' or ''ice2000'' depending on your hardware. | ||
Line 227: | Line 226: | ||
: <code bash> | : <code bash> | ||
$ cd /tftpboot | $ cd /tftpboot | ||
- | $ /opt/adi-distro/3.0.0/sysroots/x86_64-adisdk-linux/usr/bin/arm-adi-linux-gnueabi/arm-adi-linux-gnueabi-gdb u-boot-spl-sc584-ezkit.elf | + | $ /opt/adi-distro-glibc/3.0.0/sysroots/x86_64-adi_glibc_sdk-linux/usr/bin/arm-adi_glibc-linux-gnueabi/arm-adi_glibc-linux-gnueabi-gdb u-boot-spl-sc584-ezkit.elf |
... | ... | ||
(gdb) target extended-remote :3333 | (gdb) target extended-remote :3333 | ||
Line 508: | Line 507: | ||
==== Booting Linux from SPI Flash ==== | ==== Booting Linux from SPI Flash ==== | ||
- | The ADSP-SC584-EZKIT comes equipped with 16 MiB of SPI Flash. The ''adsp-sc5xx-tiny'' image can be stored into it and used to boot Linux from it. You can do this from the U-Boot prompt. Following the guide so far, you'll have U-Boot installed into SPI Flash and getting the U-Boot prompt when powering up the board with the boot selector set to '1'. | + | The ADSP-SC584-EZKIT comes equipped with 16 MiB of SPI Flash. There's the option of building the ''adsp-sc5xx-tiny'' image, after changing the Libc implementation from the default GNU to musl, to further reduce the image's size. Follow the guide in [[resources:tools-software:linuxdsp:docs:quickstartguide:boot-flash-sc58x-573|Boot from SPI Flash on the SC58x & SC573]] |
- | + | ||
- | You'd first need to copy the fitImage and the ''tiny'' root filesystem on the TFTP server directory of the Host machine: | + | |
- | + | ||
- | <code bash> | + | |
- | $ cp tmp/deploy/images/adsp-sc584-ezkit/fitImage /tftpboot/ | + | |
- | $ cp tmp/deploy/images/adsp-sc584-ezkit/adsp-sc5xx-tiny-adsp-sc584-ezkit.jffs2 /tftpboot/ | + | |
- | </code> | + | |
- | + | ||
- | In order to flash the kernel on the flash, run the below command and observe a similar output: | + | |
- | + | ||
- | <code bash> | + | |
- | => run update_spi_fit | + | |
- | Speed: 1000, full duplex | + | |
- | Using eth0 device | + | |
- | TFTP from server 10.37.33.116; our IP address is 10.37.33.113 | + | |
- | Filename 'fitImage'. | + | |
- | Load address: 0x89000000 | + | |
- | Loading: ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################ | + | |
- | 2.2 MiB/s | + | |
- | done | + | |
- | Bytes transferred = 6192194 (5e7c42 hex) | + | |
- | SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB | + | |
- | device 0 offset 0xe0000, size 0x5e7c42 | + | |
- | SF: 6192194 bytes @ 0xe0000 Written: OK | + | |
- | </code> | + | |
- | + | ||
- | Now run the following command to also flash the root filesystem: | + | |
- | <code bash> | + | |
- | => run update_spi_rfs | + | |
- | Speed: 1000, full duplex | + | |
- | Using eth0 device | + | |
- | TFTP from server 10.37.33.116; our IP address is 10.37.33.113 | + | |
- | Filename 'adsp-sc5xx-tiny-adsp-sc584-ezkit.jffs2'. | + | |
- | Load address: 0x89000000 | + | |
- | Loading: ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ################################################################# | + | |
- | ## | + | |
- | 2.1 MiB/s | + | |
- | done | + | |
- | Bytes transferred = 9568256 (920000 hex) | + | |
- | SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB | + | |
- | device 0 offset 0x6e0000, size 0x920000 | + | |
- | SF: 9568256 bytes @ 0x6e0000 Written: OK | + | |
- | </code> | + | |
- | + | ||
- | You are now ready to boot into Linux, by entering ''run spiboot'' on the U-Boot prompt: | + | |
- | + | ||
- | <code bash> | + | |
- | => run spiboot | + | |
- | SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB | + | |
- | device 0 offset 0xe0000, size 0x5e7c42 | + | |
- | SF: 6192194 bytes @ 0xe0000 Read: OK | + | |
- | ## Loading kernel from FIT Image at 89000000 ... | + | |
- | Using 'conf-1' configuration | + | |
- | Verifying Hash Integrity ... OK | + | |
- | Trying 'kernel-1' kernel subimage | + | |
- | Description: Linux kernel | + | |
- | Type: Kernel Image | + | |
- | Compression: uncompressed | + | |
- | Data Start: 0x890000dc | + | |
- | Data Size: 4774688 Bytes = 4.6 MiB | + | |
- | Architecture: ARM | + | |
- | OS: Linux | + | |
- | Load Address: 0x80008000 | + | |
- | Entry Point: 0x80008000 | + | |
- | Hash algo: sha1 | + | |
- | Hash value: 0bddc73f1c3fbbd1777023e676edbf51f8cd663f | + | |
- | Sign algo: sha1,rsa2048: | + | |
- | Sign value: unavailable | + | |
- | Verifying Hash Integrity ... sha1+ sha1,rsa2048:- OK | + | |
- | + | ||
- | ... | + | |
- | + | ||
- | [ OK ] Reached target Host and Network Name Lookups. | + | |
- | [ OK ] Started D-Bus System Message Bus. | + | |
- | [ OK ] Started User Login Management. | + | |
- | [ OK ] Reached target Multi-User System. | + | |
- | + | ||
- | + | ||
- | @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ | + | |
- | + | ||
- | Analog Devices Yocto Distribution | + | |
- | www.analog.com | + | |
- | www.yoctoproject.org | + | |
- | + | ||
- | adsp-sc584-ezkit login: root | + | |
- | Password: adi | + | |
- | root@adsp-sc584-ezkit:~# | + | |
- | + | ||
- | </code> | + | |
\\ | \\ |