Wiki

This version (09 Feb 2023 13:09) was approved by Henrik Mau.The Previously approved version (21 Dec 2022 12:10) is available.Diff

Yocto Linux 2.1.0 Quickstart Guide for ADSP-SC573

The following instructions are for the ADSP-SC573-EZKIT development board. For instructions for other processors and development boards please refer to Linux for ADSP-SC5xx Processors 2.1.0

Setting Up Your Host PC

The build system is currently supported on host PCs running Ubuntu 20.04 LTS 64-bit.


Installing Required Packages

In order to build and deploy Linux to your ADSP-SC573-EZKIT development board you will need to install the following packages on your host PC.

$ sudo apt-get update
$ sudo apt-get install -y gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm u-boot-tools openssl curl tftpd-hpa python


Installing CrossCore Embedded Studio

CrossCore Embedded Studio contains OpenOCD which is used to transfer U-Boot into RAM for the first initial boot of the device. The tools are created for 32-bit architecture and therefore requires a 32-bit libz package to run. Download and install it.

$ wget https://download.analog.com/tools/CrossCoreEmbeddedStudio/Releases/Release_2.10.0/adi-CrossCoreEmbeddedStudio-linux-x86-2.10.0.deb
$ sudo dpkg -i ./adi-CrossCoreEmbeddedStudio-linux-x86-2.10.0.deb
$ sudo apt install lib32z1


Configuring TFTP Service

A TFTP server on the host is used to transfer images to the development board. Install and configure.

$ sudo vi /etc/default/tftpd-hpa

#Replace the existing file with the following
TFTP_USERNAME="tftp"
TFTP_DIRECTORY="/tftpboot"
TFTP_ADDRESS="0.0.0.0:69"
TFTP_OPTIONS="--secure"
#End of File

$ sudo mkdir /tftpboot
$ sudo chmod 777 /tftpboot
$ sudo service tftpd-hpa restart


Configure Minicom

In order to communicate with the U-Boot bootloader, a UART connection must be made between the host PC and the development board. It is recommended that you use minicom to do this. Minicom must be configured to connect to U-Boot correctly.

On the host PC open a terminal and execute the following commands:

$ sudo apt-get install -y minicom
$ sudo minicom -s

            +-----[configuration]------+
            | Filenames and paths      |
            | File transfer protocols  |
            | Serial port setup        |
            | Modem and dialing        |
            | Screen and keyboard      |
            | Save setup as dfl        |
            | Save setup as..          |
            | Exit                     |
            | Exit from Minicom        |
            +--------------------------+


# Select Serial port setup
     Set Serial Device to /dev/ttyUSB0
     Set Bps/Par/Bits to 115200 8N1
     Set Hardware Flow Control to No
     
     Close the Serial port setup option by press Esc
 Select Save setup as dfl
 Select Exit


Installing the Sources

The example is fully contained in the Analog Devices Yocto Linux github repositories.

To install the sources: TODO: Make sure its the correct repo, branch, manifest file etc

$ mkdir ~/lnxdsp
$ cd ~/lnxdsp
$ mkdir bin
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ./bin/repo
$ chmod a+x ./bin/repo
$ ./bin/repo init \
   -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git \
   -b release/yocto-2.1.0 \
   -m release-yocto-2.1.0.xml
$ ./bin/repo sync


Building the Image

Preparing the buildtool

Yocto requires the environment to be configured before building is possible. A setup-environment script in the lnxdsp folder contains all the required environment settings for your build target. Source the setup script for your board:

$ source setup-environment -m adsp-sc573-ezkit

Sourcing the script will configure your build environment and create a build folder along with a local build configuration file. See the Yocto Manual for further details.

Note that the build environment needs to be sourced once only before building. If later working in a different terminal the setup-environment script should be sourced again. If sourcing the setup-environment script is done without specifying the machine Yocto will reuse the previous configuration settings and retain any changes made to the files in the conf folder.


Building the example

You can build three different versions of the root filesystem; minimal, ramdisk and full. To build the example images invoke bitbake from within the build directory created previously.

$ bitbake adsp-sc5xx-minimal
$ bitbake adsp-sc5xx-ramdisk
$ bitbake adsp-sc5xx-full

When the build completes you will see a warning that the ELF binary has relocations in .text. It is OK to ignore this warning

Running U-Boot on the Board for the first time

Copy the U-Boot & the init binary files to the /tftpboot directory, so that U-Boot can be ran from the board's RAM, along with the U-Boot loader file so that it can be uploaded to the target board:

$ cp tmp/deploy/images/adsp-sc573-ezkit/u-boot-sc573-ezkit /tftpboot/ 
$ cp tmp/deploy/images/adsp-sc573-ezkit/init-sc573-ezkit.elf /tftpboot/ 
$ cp tmp/deploy/images/adsp-sc573-ezkit/u-boot-sc573-ezkit.ldr /tftpboot/ 

Before installing the software on to the development board, ensure that the following cables are connected:

  • Board connected to network via ethernet cable using J13 connector.
  • Board connected to host PC using USB micro cable, connected to USB/UART port on the development board
  • Board connected to the ICE 1000 or ICE 2000 via the DEBUG port on the board
  • ICE is also connected to host PC via USB mini cable

  • The BOOT MODE selector on the EV-SC573-EZKIT board should be turned to “0”.

The console output from U-Boot and later on Linux will appear on the USB serial port configured in minicom earlier so open up minicom.

Terminal1: minicom
$ sudo minicom 

In a separate console launch OpenOCD and connect to the development board.

Terminal2: OpenOCD
$ cd /opt/analog/cces/2.10.0/ARM/openocd/share/openocd/scripts
$ sudo /opt/analog/cces/2.10.0/ARM/openocd/bin/openocd -f interface/<ICE>.cfg -f board/adspsc573_ezkit.cfg

Where <ICE> should be replaced with ice1000 or ice2000 depending on your hardware. When successful you should see a message similar to the console output below

Open On-Chip Debugger (Analog Devices CCES 2.10.0 OpenOCD 0.9.0-ge8d0a22) 0.9.0
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
adapter speed: 1000 kHz
Info : transports supported by the debug adapter: "jtag", "swd"
Info : auto-select transport "jtag"
halt and restart using CTI
trst_only separate trst_push_pull
adspsc58x_init
Info : ICE-1000 firmware version is 1.0.2
Info : clock speed 1000 kHz
Info : JTAG tap: adspsc573.adjc tap/device found: 0x428080cb (mfg: 0x065, part: 0x2808, ver: 0x4)
Info : JTAG tap: adspsc573.dap enabled
Info : adspsc573.dap: hardware has 3 breakpoints, 2 watchpoints
Info : adspsc573.dap: but you can only set 1 watchpoint

In a third console window launch GDB and type target extended-remote :3333. This will make GDB to connect to the gdbserver on the local host using port 3333. Then, load the init file into RAM by typing load init-sc573-ezkit.elf and run it by typing c. Hit Ctrl+C to interrupt thereafter.

Terminal3: GDB
$ cd /tftpboot
$ /opt/analog/cces/2.10.0/ARM/arm-none-eabi/bin/arm-none-eabi-gdb u-boot-sc573-ezkit 
...
(gdb) target extended-remote :3333
Remote debugging using :3333
0x00004884 in ?? ()
(gdb) load init-sc573-ezkit.elf
Loading section .text, size 0x744 lma 0x20080000
Start address 0x20080028, load size 1860
Transfer rate: 22 KB/sec, 1860 bytes/write.
(gdb) c
Continuing.
^C
Program received signal SIGINT, Interrupt.
0x20080024 in ?? ()

Now, load U-Boot into RAM.

Terminal3: GDB
(gdb) load
Loading section .text, size 0x3a8 lma 0x89200000
Loading section .efi_runtime, size 0xe30 lma 0x892003a8
Loading section .text_rest, size 0x4dd10 lma 0x892011e0
Loading section .rodata, size 0xfbe0 lma 0x8924eef0
Loading section .hash, size 0x18 lma 0x8925ead0
Loading section .dtb.init.rodata, size 0x360 lma 0x8925eaf0
Loading section .data, size 0x3468 lma 0x8925ee50
Loading section .got.plt, size 0xc lma 0x892622b8
Loading section .u_boot_list, size 0xe80 lma 0x892622c4
Loading section .efi_runtime_rel, size 0xd0 lma 0x89263144
Loading section .rel.dyn, size 0xb180 lma 0x89263214
Loading section .dynsym, size 0x30 lma 0x8926e394
Loading section .dynstr, size 0x1 lma 0x8926e3c4
Loading section .dynamic, size 0x90 lma 0x8926e3c8
Loading section .gnu.hash, size 0x18 lma 0x8926e458
Start address 0x89200000, load size 451677
Transfer rate: 31 KB/sec, 11581 bytes/write.
(gdb) c
Continuing.

At this point U-Boot will now be running in RAM on your target board. You should see U-Boot booting in the minicom console (Terminal 1). Press a key to interrupt the boot process before the countdown terminates:

Terminal1: minicom
U-Boot 2020.10 (Aug 23 2022 - 13:09:23 +0000)

CPU:   ADSP ADSP-SC573-0.0 (Detected Rev: 1.1) (spi flash boot)
VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 225 MHz
OCLK: 150 MHz
Model: ADI sc573-ezkit
I2C:   ready
DRAM:  224 MiB
MMC:   SC5XX SDH: 0
In:    serial@0x31003000
Out:   serial@0x31003000
Err:   serial@0x31003000
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
other init
Net:   dwmac.3100c000
Hit any key to stop autoboot:  0
=>


Flash U-Boot to SPI Flash


In the U-Boot console, set the IP address of the Host Linux PC that hosts the U-Boot loader file (u-boot-sc573-ezkit.ldr) on TFTP.

Terminal1: minicom
=> setenv serverip <SERVERIP>
To find the IP address of your host Linux PC you can issue the ip addr command from the shell or console.

If your network supports DHCP, run:

=> dhcp

If your network does NOT support DHCP, run:

=> set ipaddr <ADDR>

Where <ADDR> is the IP address you want to assign.

Next, run the U-Boot update command to copy the U-Boot loader file from the host PC to the target board, and write it into flash:

=> run update

You will see an output similar to the one below:

=> run update
Speed: 1000, full duplex
Using dwmac.3100c000 device
TFTP from server 192.168.1.223; our IP address is 192.168.1.218
Filename 'u-boot-sc573-ezkit.ldr'.
Load address: 0x82000000
Loading: ############################
         2.7 MiB/s
done
Bytes transferred = 399416 (61838 hex)
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
SF: 524288 bytes @ 0x0 Erased: OK
device 0 offset 0x0, size 0x61838
SF: 399416 bytes @ 0x0 Written: OK
=>

At this point the U-Boot binary is stored in flash. You can now disconnect the ICE-1000 or ICE-2000 from the development board and make sure to switch the BMODE to position 1. You will only need to reconnect this if your board fails to boot and you need to re-follow these instructions.


Booting Linux Using TFTP

In order to boot Linux, the TFTP server should be setup as above and (for both NFS and RAM boot) a copy of the kernel image should be copied into the /tftpboot directory.

$ cp tmp/deploy/images/adsp-sc573-ezkit/fitImage /tftpboot


RAM Boot

For RAM boot a copy of the image containing the filesystem needs copied to the /tftpboot directory.

$ cp tmp/deploy/images/adsp-sc573-ezkit/adsp-sc5xx-ramdisk-adsp-sc573-ezkit.cpio.xz.u-boot /tftpboot/ramdisk.cpio.xz.u-boot


NFS Boot

For NFS boot we use the Network File System which is stored in local Ubuntu Host. This is suggested when you do application development. To setup the NFS server:

$ sudo apt-get install nfs-kernel-server
$ sudo vi /etc/exports

#Add following commands
/romfs *(rw,sync,no_root_squash,no_subtree_check)

$ sudo mkdir /romfs/
$ sudo chmod 777 /romfs/
$ sudo service nfs-kernel-server start

The output will indicate that the server is active, i.e.

● nfs-server.service - NFS server and services
     Loaded: loaded (/lib/systemd/system/nfs-server.service; enabled; vendor preset: enabled)
    Drop-In: /run/systemd/generator/nfs-server.service.d
             └─order-with-mounts.conf
     Active: active (exited) since Tue 2022-09-06 14:38:31 BST; 3 months 14 days ago
   Main PID: 953 (code=exited, status=0/SUCCESS)
      Tasks: 0 (limit: 18797)
     Memory: 0B
     CGroup: /system.slice/nfs-server.service

Sep 06 14:38:29 $YOUR_HOSTNAME systemd[1]: Starting NFS server and services...
Sep 06 14:38:31 $YOUR_HOSTNAME systemd[1]: Finished NFS server and services.

If it's reported as inactive, wait a few moments and check the status again.

The root filesystem should then be copied to /romfs.

$ sudo tar -xf tmp/deploy/images/adsp-sc573-ezkit/adsp-sc5xx-full-adsp-sc573-ezkit.tar.xz -C /romfs


Booting into Linux from TFTP

Next, on the target, from u-boot, run one of the following command:

=> run ramboot
 or
=> run nfsboot
......
......
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.


     @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@     @@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@        @@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@            @@@@@@@@@@@@@@@@@@@
     @@@@@@@@               @@@@@@@@@@@@@@@@
     @@@@@@@@                   @@@@@@@@@@@@
     @@@@@@@@                     @@@@@@@@@@
     @@@@@@@@                        @@@@@@@
     @@@@@@@@                     @@@@@@@@@@
     @@@@@@@@                   @@@@@@@@@@@@
     @@@@@@@@               @@@@@@@@@@@@@@@@
     @@@@@@@@            @@@@@@@@@@@@@@@@@@@
     @@@@@@@@        @@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@     @@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

        Analog Devices Yocto Distribution
                 www.analog.com
              www.yoctoproject.org

adsp-sc573-ezkit login: root
Password: adi
root@adsp-sc573-ezkit:~# 

The username is root and the password is adi.


Building the SDK

To build the SDK follow the instructions here Building the SDK.

resources/tools-software/linuxdsp/docs/quickstartguide/quickstart_sc573.txt · Last modified: 09 Feb 2023 12:18 by Prasanth Ramesh