Wiki

This version is outdated by a newer approved version.DiffThis version (11 May 2023 17:04) was approved by Vasileios Bimpikas.

This is an old revision of the document!


The following instructions are for the ADSP-SC598-EZKIT development board (the EV-SC598-SOM System-on-Module (SOM) board attached to the EV-SOMCRR-EZKIT carrier board). Furthermore, this is supported on version 3.0.0 of Linux for ADSP-SC5xx

Introduction

This example will guide you through some changes that are needed in order to store the kernel and rootfs on the eMMC, with U-Boot still booting out of QSPI.

This allows for storing larger images without having to plug in an external device, as the SC598-SOM comes with eMMC present on the SOM.

Prepare the build

You should follow the steps up to and including the 'Preparing the buildtool' step in Yocto Linux 3.0.0 Quickstart Guide for ADSP-SC598

Apply patches

Two patches should be applied. The directory the changes needed to take place is $PROJECTDIR/sources/meta-adi/.

From 9d88cecc5ed849fb35192257138e6f3e3577858c Mon Sep 17 00:00:00 2001
From: Nathan Barrett-Morrison <nathan.morrison@timesys.com>
Date: Wed, 3 May 2023 11:27:55 -0400
Subject: [PATCH] Adjust update_mmc to boot from separate fitImage-emmc-tools
 with proper provisioning initramfs (sshd, gzip, etc)
 
---
 include/configs/sc_adi_common.h | 2 +-
 1 file changed, 1 insertion(+), 1 deletion(-)
 
diff --git a/include/configs/sc_adi_common.h b/include/configs/sc_adi_common.h
index f7b5f8ca8e..a15686521e 100644
--- a/include/configs/sc_adi_common.h
+++ b/include/configs/sc_adi_common.h
@@ -178,7 +178,7 @@
 	"spiboot=run spi_boot\0"
 
 #define ADI_MMC_BOOT \
-	"update_mmc=setenv bootcmd \'run mmcboot\'; saveenv; run ramboot\0" \
+	"update_mmc=setenv bootcmd \'run mmcboot\'; saveenv; setenv imagefile fitImage-emmc-tools; run ramboot\0" \
 	"mmcargs=setenv bootargs " ADI_BOOTARGS_MMC "\0" \
 	"mmcload=" ADI_MMC_LOAD "\0" \
 	"mmc_boot=" ADI_MMC_BOOTCMD "\0" \
-- 
GitLab
From 2cf70574c8146cac16cf5b8f3895c557c0e23a2f Mon Sep 17 00:00:00 2001
From: Nathan Barrett-Morrison <nathan.morrison@timesys.com>
Date: Wed, 3 May 2023 11:26:21 -0400
Subject: [PATCH] Fixup adsp-sc5xx-minimal-emmc + adsp-sc5xx-ramdisk-emmc-tools
 so that we can provision and boot from MMC
 
---
 .../classes/adsp-fit-generation.bbclass         | 12 ++++++++++--
 .../images/adsp-sc5xx-minimal-mmc.bb            | 17 ++++++++++-------
 .../images/adsp-sc5xx-ramdisk-emmc-tools.bb     |  5 +++--
 3 files changed, 23 insertions(+), 11 deletions(-)
 
diff --git a/meta-adi-adsp-sc5xx/classes/adsp-fit-generation.bbclass b/meta-adi-adsp-sc5xx/classes/adsp-fit-generation.bbclass
index c6cd418..5001b82 100644
--- a/meta-adi-adsp-sc5xx/classes/adsp-fit-generation.bbclass
+++ b/meta-adi-adsp-sc5xx/classes/adsp-fit-generation.bbclass
@@ -58,7 +58,7 @@ emit_its() {
 
 		ramdisk-3 {
 			description = "Initial Ram File System";
-			data = /incbin/("adsp-sc5xx-ramdisk-${MACHINE}.cpio.gz");
+			data = /incbin/("adsp-sc5xx-${1}-${MACHINE}.cpio.gz");
 			type = "ramdisk";
 			arch = "${ARCH}";
 			os = "linux";
@@ -95,7 +95,15 @@ EOF
 
 do_assemble_fitimage() {
 	cd ${DEPLOY_DIR_IMAGE}
-	emit_its;
+
+	#Provisioning fitImage for flashing MMC
+	if [ "${IMAGE_BASENAME}" = "adsp-sc5xx-minimal-mmc" ]; then
+		emit_its ramdisk-emmc-tools;
+		uboot-mkimage -D "${UBOOT_MKIMAGE_DTCOPTS}" -f fit-image.its fitImage-emmc-tools
+	fi
+
+	#Normal fitImage for booting
+	emit_its ramdisk;
 	uboot-mkimage -D "${UBOOT_MKIMAGE_DTCOPTS}" -f fit-image.its fitImage
 }
 
diff --git a/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-minimal-mmc.bb b/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-minimal-mmc.bb
index eb1bcfe..b856841 100644
--- a/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-minimal-mmc.bb
+++ b/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-minimal-mmc.bb
@@ -1,13 +1,13 @@
 inherit adsp-sc5xx-minimal
 
-IMAGE_INSTALL += "kernel kernel-devicetree"
+DEPENDS += "adsp-sc5xx-ramdisk-emmc-tools"
 
-#We do not need these files in the rootfs -- remove them to reduce the minimal rootfs size
-fakeroot do_rootfs_cleanup(){
-
-	#We need this for eMMC boot -- do not delete
-	#rm -rf ${IMAGE_ROOTFS}/boot
+do_rootfs[depends] += " \
+	adsp-sc5xx-ramdisk-emmc-tools:do_image_complete \
+"
 
+fakeroot do_rootfs_cleanup(){
+	#We do not need these files in the rootfs -- remove them to reduce the minimal rootfs size
 	rm -rf ${IMAGE_ROOTFS}/etc/udev/hwdb.bin
 	rm -rf ${IMAGE_ROOTFS}/etc/udev/hwdb.d
 
@@ -16,8 +16,11 @@ fakeroot do_rootfs_cleanup(){
 
 	rm -rf ${IMAGE_ROOTFS}/usr/lib/libX11.so.6
 	rm -rf ${IMAGE_ROOTFS}/usr/lib/libX11.so.6.3.0
+
+	#Pack fitImage into MMC RFS:
+	cp ${DEPLOY_DIR_IMAGE}/fitImage ${IMAGE_ROOTFS}/boot
 }
 
-addtask rootfs_cleanup after do_rootfs before do_image
+addtask rootfs_cleanup after do_assemble_fitimage before do_image_ext4
 
 IMAGE_FSTYPES:append = " wic.gz ext4 "
diff --git a/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-ramdisk-emmc-tools.bb b/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-ramdisk-emmc-tools.bb
index e7872eb..dbf441e 100644
--- a/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-ramdisk-emmc-tools.bb
+++ b/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-ramdisk-emmc-tools.bb
@@ -1,4 +1,4 @@
-inherit core-image extrausers adsp-sc5xx-compatible
+inherit adsp-sc5xx-ramdisk adsp-fit-generation
 
 SUMMARY = "eMMC/MMC provisioning ramdisk image for Analog Devices ADSP-SC5xx boards"
 LICENSE = "MIT"
@@ -6,6 +6,7 @@ LICENSE = "MIT"
 #For transferring data to flash eMMC/SD via ramdisk
 MMC_UTILS = " \
     openssh \
+    openssh-sshd \
     e2fsprogs-resize2fs \
     gzip \
     adi-flash-emmc \
@@ -15,4 +16,4 @@ MMC_UTILS = " \
 
 IMAGE_INSTALL:append = " \
     ${MMC_UTILS} \
-"
+"
\ No newline at end of file
-- 
GitLab

You can copy and paste the contents of the above two patches in files under the target directory ($PROJECTDIR/sources/meta-adi/), e.g. patch1.patch & patch2.patch, and apply them with git, e.g. $ git apply patch1.patch && git apply patch2.patch

Build and boot the eMMC image

Return to the build directory of your project, i.e. $PROJECTDIR/build/ and build the eMMC provisioning ramdisk:

bitbake adsp-sc5xx-minimal-mmc

When that's done, Boot U-Boot from JTAG on the target board and flash SPI. This is described in detail in Yocto Linux 3.0.0 Quickstart Guide for ADSP-SC598 during the 'Running U-Boot on the Board for the first time' section.

Now that you have U-Boot flashed on the target board, you can boot the eMMC provisioning ramdisk like so:

Target board
=> env default -a
 
=> setenv tftpserverip xxx.xxx.xxx.xxx;
 
=> run update_mmc

Flash the eMMC form your host/build machine via SSH

You need to start sshd on your target board:

Target board
$ ssh-keygen -A
 
$ mkdir /var/run/sshd
 
$ /usr/sbin/sshd

On your build machine, you need to flash the image to the target board via SSH:

Build machine
$ cd $PROJECTDIR/build/tmp/deploy/images/adsp-sc598-som-ezkit
 
$ dd if=adsp-sc5xx-minimal-mmc-adsp-sc598-som-ezkit.wic.gz | ssh root@<your board's ip> 'adi-flash-emmc.sh'
 
Flashing image...
75396+1 records in
75396+1 records out
38602977 bytes (39 MB, 37 MiB) copied, 23.0113 s, 1.7 MB/s
Image flashed...
Resizing partition to fill empty space...
Resized!
Complete!

Finally, reboot your target board:

Target board
$ echo b > /proc/sysrq-trigger

It should now reset and boot from eMMC.

resources/tools-software/linuxdsp/docs/quickstartguide/emmc-kernel-rfs-storage.1683817480.txt.gz · Last modified: 11 May 2023 17:04 by Vasileios Bimpikas