This page provides the resources which are required by Linux to boot on ADI SC5XX boards.
Type | Hardware | Notes |
---|---|---|
CPU | ARM Cortex A5 | Core 0 running u-boot & Linux |
Core Timer | GPTimer 0 & 1 | Used by Linux as the Core Timer |
Non-Volatile Memory | Nor flash | Stores u-boot LDR file |
Volatile Memory | DDR | Used by u-boot and Linux |
L2 | Used by u-boot and Linux | |
GPIO | gpio | Used by u-boot/Linux |
Serial I/O | UART0 | Used by Linux as the default UART Log output |
Ethernet | ETH0 | Used by u-boot/Linux as the default network |
Machine | Start Address | size | usage |
---|---|---|---|
adsp-sc589-ezkit | 0x20080000 | 0x1000 | Core0 ICC |
adsp-sc584-ezkit | 0x20080000 | 0x1000 | Core0 ICC |
adsp-sc573-ezkit | 0x20000000 | 0x1000 | Core0 ICC |
ads-sc589-mini | 0x20080000 | 0x1000 | Core0 ICC |
Machine | Start Address | size |
---|---|---|
adsp-sc589-ezkit | 0xc2000000 | depends on the image |
adsp-sc584-ezkit | 0xc2000000 | depends on the image |
adsp-sc573-ezkit | 0x82000000 | depends on the image |
adsp-sc589-mini | 0xc2000000 | depends on the image |