This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp [22 Sep 2020 10:53] – [Device tree configuration] cathy fang | resources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp [22 Sep 2020 11:14] (current) – [Device tree configuration] Sunny Feng | ||
---|---|---|---|
Line 46: | Line 46: | ||
\\ | \\ | ||
==== Device tree configuration ==== | ==== Device tree configuration ==== | ||
- | The timestamps that are the basis of PTP can be acquired with greater accuracy when they are captured by the ethernet PHY hardware. The RGMII and RMII PHY interface support hardware timestamps, the default phy mode is RGMII. | + | The timestamps that are the basis of PTP can be acquired with greater accuracy when they are captured by the ethernet PHY hardware. The PHY interface |
- | The phy-mode can be changed to " | + | |
+ | The phy-mode | ||
<WRAP info> | <WRAP info> | ||
... : ellipsis, means other properties in EMAC0 node stay the same\\ | ... : ellipsis, means other properties in EMAC0 node stay the same\\ |