Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp [17 Sep 2020 16:27]
Matt Prewett ↷ Page moved from resources:tools-software:linuxdsp:docs:linux_yocto_distrubution_and_applications:linuxptp to resources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp
resources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp [22 Sep 2020 11:11]
Sunny Feng [Device tree configuration]
Line 46: Line 46:
 \\ \\
 ==== Device tree configuration ==== ==== Device tree configuration ====
-The timestamps that are the basis of PTP can be acquired with greater accuracy when they are captured by the ethernet PHY hardware. The RMII PHY interface ​supports ​hardware timestamps ​but the RGMII PHY interface does not. In order to obtain a higher accuracy of time synchronization the RMII PHY is the better choice, even though this means being limited to 10/100 Mbps operation+The timestamps that are the basis of PTP can be acquired with greater accuracy when they are captured by the ethernet PHY hardware. The PHY interface ​can support ​hardware timestampsthe default phy-mode is RGMII. 
-The phy-mode can be changed to "​rmii"​ in the device tree header in the linux kernel source arch/​arm/​boot/​dts/​sc589-ezkit.dts other board specific sc5xx.dts files. Run "//​**bitbake linux-adi -c devshell**//"​ to enter into linux kernel source code.+ 
 +The phy-mode ​also can be changed to "​rmii"​ in the device tree header in the linux kernel source arch/​arm/​boot/​dts/​sc589-ezkit.dts other board specific sc5xx.dts files. Run "//​**bitbake linux-adi -c devshell**//"​ to enter into linux kernel source code.
 <WRAP info> <WRAP info>
 ... : ellipsis, means other properties in EMAC0 node stay the same\\ ... : ellipsis, means other properties in EMAC0 node stay the same\\
Line 144: Line 145:
 \\ \\
 ---- ----
-**Back to** [[resources/tools-software/linuxdsp/docs/​linux_yocto_distrubution_and_applications/​start|Yocto Linux Distrubution and Applications]]+**Back to** [[resources:tools-software:linuxdsp:docs:​linux_yocto_distribution_and_applications:​start|Yocto Linux Distrubution and Applications]]
resources/tools-software/linuxdsp/docs/linux_yocto_distribution_and_applications/linuxptp.txt · Last modified: 22 Sep 2020 11:14 by Sunny Feng