Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_wifi [27 Jan 2021 22:35]
Robin Getz use wp> interwiki links
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_wifi [04 Feb 2021 03:20]
cathy fang
Line 139: Line 139:
 **Adding the corresponding Firmware** **Adding the corresponding Firmware**
  
-Standard Yocto layer provides a "//__sources/​poky/​meta/​recipes-kernel/​linux-firmware/​[[https://​git.yoctoproject.org/​cgit.cgi/​poky/​plain/​meta/​recipes-kernel/linux-firmware/​linux-firmware_20200619.bb|linux-firmware_git.bb]]__//" for user to get some common firmware. please modify and add the below codes to ''​sources/​meta-adi/​meta-adi-adsp-sc5xx/​recipes-adi/​images/​adsp-sc5xx-full.bb''​ to enable the **wpa-supplicant ** and **wireless-tools ** tools and the chipset corresponding Firmware.+Standard Yocto layer provides a "sources/​poky/​meta/​recipes-kernel/​linux-firmware/​linux-firmware_git.bb"​ for user to get some common firmware. please modify and add the below codes to ''​sources/​meta-adi/​meta-adi-adsp-sc5xx/​recipes-adi/​images/​adsp-sc5xx-full.bb''​ to enable the **wpa-supplicant ** and **wireless-tools ** tools and the chipset corresponding Firmware.
 <code java> ​ <code java> ​
 USB_WIFI = " \ USB_WIFI = " \
Line 154: Line 154:
 Add the additional Firmware: Add the additional Firmware:
 <​hidden>​ <​hidden>​
-If we can't find the target chipset supported firmware from the **//linux-firmware_git.bb//**, we should write our own .bb file to fetch the corresponding Firmware or just adding it manually.+If we can't find the target chipset supported firmware from the linux-firmware_git.bb,​ we should write our own .bb file to fetch the corresponding Firmware or just adding it manually.
  
 **1. Manually fetch Firmware** **1. Manually fetch Firmware**
resources/tools-software/linuxdsp/docs/linux-kernel-and-drivers/usb/host_mode/usb_wifi.txt · Last modified: 04 Feb 2021 03:20 by cathy fang