This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_camera [14 Jul 2020 08:04] – [Software Configuration] cathy fang | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_camera [27 Jul 2020 08:28] – [Hardware Configuration] cathy fang | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== USB Camera Support | ====== USB Camera Support | ||
- | |||
---- | ---- | ||
+ | ===== Hardware Configuration ===== | ||
+ | Connect the USB micro-A plug to A receptacle adapter cable (found in the EZ-Board box) to the OTG port, below photo shows when it acts as Host and connected to a USB Camera device. | ||
- | + | {{ : | |
- | ===== Hardware Configuration ===== | + | |
- | Connect the USB micro-A plug to A receptacle adaptor cable (found in the EZ-Board box) to the OTG port, below photo shows when it acts as Host and connected to a USB Camera device. | + | |
- | <WRAP center round todo 100%> | + | |
- | To do: add a diagram of board and Camera connection | + | |
- | </ | + | |