This page introduces the remoteproc support in linux kernel on ADI sc5xx platforms. The remoteproc framework allows users to control(load firmware, start and stop) remote processors from ARM side.
No connections are required except the uart, ethernet and power connections.
$ bitbake linux-adi -c menuconfig Device Drivers ---> Remoteproc drivers ---> <*> Support for Remote Processor subsystem <*> ADI remoteproc support
Then run bitbake linux-adi -C compile to generate kernel image zImage and dtb file.
Add the firmware package in the filesystem, it's enabled in adsp-sc5xx-full image by default.
vim build/conf/local.conf IMAGE_INSTALL_append = "linux-firmware-adau1761"
Then run “bitbake adsp-sc5xx-minimal -C compile” or “bitbake adsp-sc5xx-full -C compile” to generate the filesystem.
The firmware components are stored in the /lib/firmware/ folder by default in the file system. Optionally another location can be set. Below the command for adding a new path for firmware parsing:
root@adsp-sc589-ezkit:~# echo -n <firmware_path> > /sys/module/firmware_class/parameters/path
root@adsp-sc589-ezkit:~# echo blinky_Core1_sc589.ldr > /sys/class/remoteproc/remoteproc0/firmware
The blinky_Core1_sc589.ldr is one SHARC LED blinking application generated through ADI CrossCore® Embedded Studio. Refer this page for How to generate remoteproc LDR file in CCES
.
root@adsp-sc589-ezkit:~# echo start > /sys/class/remoteproc/remoteproc0/state
The LED will start blinking on sc589-ezkit board.
Run the below command, one SOFT irq would be raised through SEC interface to SHARC core, SHARC core will release all related resources(interrupts, hardwares, etc) and set itself to IDLE state once receiving the interrupt.
root@adsp-sc589-ezkit:~# echo stop > /sys/class/remoteproc/remoteproc0/state
ADI sets a specified name called adi_adsp_core1_fw.ldr or adi_adsp_core2_fw.ldr to auto boot when kernel starts. If you want to auto boot the remote processor, rename your own ldr file to adi_adsp_core1_fw.ldr or adi_adsp_core1_fw.ldr and put it in /lib/firmware directory.
Back to Kernel Features and Device Drivers for ADSP-SC5xx Yocto Linux