This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:mcapi_example [26 Jul 2020 05:30] – [Get the Source Code Ready] Sunny Feng | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:mcapi_example [03 Jan 2021 21:43] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Get the Source Code Ready ===== | ===== Get the Source Code Ready ===== | ||
- | The MCAPI example for ARM core (Running Linux) is included in the YOCTO, and you can get the MCAPI example for SHARC+ Cores from the gitbub [[https://bitbucket.analog.com/projects/ | + | The MCAPI example for ARM core (Running Linux) is included in the YOCTO, and you can get the MCAPI example for SHARC+ Cores from the gitbub [[https://github.com/analogdevicesinc/ |
=== - MCAPI Examples for SHARC Cores=== | === - MCAPI Examples for SHARC Cores=== | ||
Line 24: | Line 24: | ||
**__Git Usage__** | **__Git Usage__** | ||
<code bash> | <code bash> | ||
- | git clone https://bitbucket.analog.com/scm/dte/ | + | git clone https://github.com/analogdevicesinc/ |
cd lnxdsp-examples | cd lnxdsp-examples | ||
git branch -a | git branch -a | ||
- | git checkout -b develop/ | + | git checkout -b release/ |
git pull | git pull | ||
</ | </ | ||
Line 37: | Line 37: | ||
=== - CCES=== | === - CCES=== | ||
- | * Analog Devices [[https:// | + | * Analog Devices [[adi>en/ |
---- | ---- | ||
Line 133: | Line 133: | ||
; **'' | ; **'' | ||
: Click the **Select root directory** radio button and then click the **Browse** button | : Click the **Select root directory** radio button and then click the **Browse** button | ||
- | : Browse the root folder where you previously | + | : Browse the root folder where you previously |
: Click **OK** to close the file browser dialog | : Click **OK** to close the file browser dialog | ||
; **'' | ; **'' |