Wiki

This version is outdated by a newer approved version.DiffThis version (03 Jul 2020 09:03) was approved by Sunny Feng.

This is an old revision of the document!


Linux LCD device driver

Introduction

This section describes the steps required to build and use LCD device driver on Linux using an ADSP-SC58x board and a WVGA/LCD EI3 extender board.

WVGA/LCD EI3 Extender LCD board is not supported on the ADSP-SC573 EZ-KIT due to some board level hardawre confilict, the SC573 processor itself is capable of doing this. 

Hardware Setup

  • ADSP-SC58x EZ-KIT: ADSP-SC589/SC584 EZ-Board
  • A WVGA/LCD EI3 Extender Board

Connect the J1 connector on the LCD EI3 Extender Board to the P1A connector on the SC58x-EZKIT

Software Configuration

The following configuration should be done on top of the sc589-ezkit/sc584-ezkit default configuration.

Configure Linux Kernel

Run bitbake linux-adi -c menuconfig and configure the kernel as follows:

Enable touchscreen and backlight

Device Drivers  --->
     Input device support  --->
         [*]   Touchscreens  --->
             <*> Analog Devices AD7879-1/AD7889-1 touchscreen interface
             <*> support SPI bus connection

Enable NL8048HL WVGA LCD for ADSP-SC58x

Device Drivers  --->
     Graphics support  --->
          Frame buffer Devices  --->
              <*> Support for frame buffer devices  --->
              <*> NEC NL8048HL WVGA LCD for ADI SC5XX boards

Avoid LCD driver probe failure by disabling CAN bus support

[*] Networking support  --->
          < >   CAN bus subsystem support  ----

Enable Packages

Add the video test program in the filesystem images, it's default enabled in adsp-sc5xx-full image.

vim build/conf/local.conf
IMAGE_INSTALL_append = "video-test"

Example

Enable LCD Back-light

# cat /sys/kernel/debug/gpio 
mcp230xx 0-0022: restoring reg 0x00 from 0x0000 to 0xffff (power-loss?)
mcp230xx 0-0021: restoring reg 0x00 from 0x0000 to 0xffff (power-loss?)
gpiochip0: GPIOs 0-15, adi-gpio:
gpiochip1: GPIOs 16-31, adi-gpio:
 gpio-30  (                    |mdio-reset          ) out hi    
gpiochip2: GPIOs 32-47, adi-gpio:
 gpio-32  (                    |spi0.32             ) out hi    
 gpio-39  (                    |spi0.39             ) out hi    
 gpio-44  (                    |spi0.44             ) out hi    
gpiochip3: GPIOs 48-63, adi-gpio:
gpiochip4: GPIOs 64-79, adi-gpio:
gpiochip5: GPIOs 80-95, adi-gpio:
gpiochip6: GPIOs 96-101, adi-gpio:
gpiochip9: GPIOs 479-479, parent: spi/spi0.32, AD7879-GPIO, can sleep:
gpiochip8: GPIOs 480-495, parent: i2c/0-0022, mcp23017, can sleep:
gpiochip7: GPIOs 496-511, parent: i2c/0-0021, mcp23017, can sleep:
# echo 479 > /sys/class/gpio/export 
# echo high > /sys/class/gpio/gpio479/direction 

Make sure your LCD screen becomes white at this point.

Soft Switch Configuration

The settings in this section is only apply to ADSP-SC584 EZ-Board.

# echo 484 > /sys/class/gpio/export
# echo high > /sys/class/gpio/gpio484/direction
# echo 491 > /sys/class/gpio/export
# echo high > /sys/class/gpio/gpio491/direction

Run video_test Program

You will see a  crossing curve like an “8” in the LCD window.

# video_test

How to Install Modules

Select these drivers as modules:

<M>   Analog Devices AD7879-1/AD7889-1 touchscreen interface    
<M>     support SPI bus connection
<M> Support for frame buffer devices  --->
<M> NEC NL8048HL WVGA LCD for ADI SC5XX boards

Then bitbake adsp-sc5xx-full -C compile

If AD7879 module has already been installed, removed it first:

# lsmod
Module                  Size  Used by 
ad7879_spi              2222  0 
ad7879                  3763  1 ad7879_spi 
# modprobe -r ad7879_spi
# lsmod
Module                  Size  Used by

Then install the modules as follows:

# modprobe adi_nl8048
adi_nl8048 31040000.lcd: LCD fb0 registered@cf15f846,dma=28,irq=48,cs=39
# modprobe ad7879_spi
input: AD7879 Touchscreen as /devices/platform/scb/31042000.spi/spi_master/spi0/spi0.32/input/input0

Now you can run LCD test as above.

Back to Kernel Features and Device Drivers for ADSP-SC5xx Yocto Linux

resources/tools-software/linuxdsp/docs/linux-kernel-and-drivers/lcd/lcd_display.1593746171.txt.gz · Last modified: 03 Jul 2020 05:16 by Sunny Feng