Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

resources:tools-software:linuxdsp:docs:linux-for-sc5xx-overview [07 May 2020 12:53] – created David Gibsonresources:tools-software:linuxdsp:docs:linux-for-sc5xx-overview [14 Sep 2023 10:11] (current) Vasileios Bimpikas
Line 1: Line 1:
 +<note warning>These pages are not updated anymore. Documentation has been moved to [[https://github.com/analogdevicesinc/lnxdsp-adi-meta/wiki|https://github.com/analogdevicesinc/lnxdsp-adi-meta/wiki]]</note>
 +
 ===== Linux For ADSP-SC5xx: Overview ===== ===== Linux For ADSP-SC5xx: Overview =====
 When we talk about Linux running on the ADSP-SC5xx we are generally talking about more than Linux. Linux itself refers to the Operating System. The software that is installed on to the processor consists of several components; a second-stage bootloader (U-Boot), a package file (uImage, or zImage if it is compressed) which contains the Linux kernel and a filesystem, and a .dtb file (device tree blob) which defines the system hardware. When we talk about Linux running on the ADSP-SC5xx we are generally talking about more than Linux. Linux itself refers to the Operating System. The software that is installed on to the processor consists of several components; a second-stage bootloader (U-Boot), a package file (uImage, or zImage if it is compressed) which contains the Linux kernel and a filesystem, and a .dtb file (device tree blob) which defines the system hardware.
resources/tools-software/linuxdsp/docs/linux-for-sc5xx-overview.txt · Last modified: 14 Sep 2023 10:11 by Vasileios Bimpikas