Wiki

This version (03 Apr 2023 16:50) was approved by Henrik Mau.

Internal Cores Communication

The Yocto Linux Product provides user space APIs that allow applications to easily communicate between individual cores of the ADSP-SC5xx processor.

Communication is performed using the Remote Processor Messaging Protocol (RPMsg) which defines an API and a semantics for communication and synchronization between processing cores in embedded systems. RPMsg is supported on ARM as part of Linux and as RPMsg-Lite on SHARC and ARM cores of the ADSP-SC5xx processors in both bare-metal and RTOS using CrossCore Embedded Studio.

ADSP-SC5xx is a series of products with multiple processor cores (two SHARC+ cores and an ARM® Cortex-A5 processor), this page provides some approaches to support the multi-core communication/control termed as the Internal Cores Communications (ICC) which contains the sections:

RPMsg
RPMsg-Lite
RemoteProc
Remoteproc
ICAP
Inter Core Audio Protocol
resources/tools-software/linuxdsp/docs/internal-cores-communication.txt · Last modified: 27 Feb 2023 15:23 by Henrik Mau