This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-software:zynq_images:windows_hosts [09 Mar 2022 21:04] – fix link Robin Getz | resources:tools-software:linux-software:zynq_images:windows_hosts [06 Feb 2023 07:25] (current) – Added an DISKPART as an extra option in reformatting an SD card ALEXIS CZEZAR TORRENO | ||
---|---|---|---|
Line 11: | Line 11: | ||
===== Download the SD Card File ===== | ===== Download the SD Card File ===== | ||
- | Download the software image file you want to write onto your SD Card. Typically this is going to be the standard [[: | + | Download the software image file you want to write onto your SD Card. Typically this is going to be the standard [[: |
* Save the .Zip file or .Xz file to your local hard drive, and remember the file location. | * Save the .Zip file or .Xz file to your local hard drive, and remember the file location. | ||
Line 43: | Line 43: | ||
This step should be used if the SD Card format is unknown or needs to be reconfigured. | This step should be used if the SD Card format is unknown or needs to be reconfigured. | ||
+ | |||
+ | ==== Using SD Card Formatter ==== | ||
Ensure you have the following application installed on your computer. | Ensure you have the following application installed on your computer. | ||
Line 54: | Line 56: | ||
- **Formatting Options** = Select Quick Format{{ : | - **Formatting Options** = Select Quick Format{{ : | ||
- Once set, click the **Format** button | - Once set, click the **Format** button | ||
- | - The program will notify you that the formatting is complete.(could take several | + | - The program will notify you that the formatting is complete.(could take several |
+ | |||
+ | ==== Using DISKPART via Windows command prompt==== | ||
+ | |||
+ | Windows command prompt has **DISKPART** that is also capable of reformatting SD cards and other drives. | ||
+ | - Run Windows command prompt as administrator. | ||
+ | - Type 'list disk'. All current dives will be shown. | ||
+ | - Type ' | ||
+ | - Type ' | ||
+ | - Type ' | ||
+ | - Type ' | ||
+ | - After the progress is at 100%, type ' | ||
===== Flash the SD Card ===== | ===== Flash the SD Card ===== |