Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linux-software:zynq_images:windows_hosts [31 Jan 2023 03:20] – Replaced the obsolete Kuiper Linux page link Joyce Velascoresources:tools-software:linux-software:zynq_images:windows_hosts [06 Feb 2023 07:25] (current) – Added an DISKPART as an extra option in reformatting an SD card ALEXIS CZEZAR TORRENO
Line 43: Line 43:
  
 This step should be used if the SD Card format is unknown or needs to be reconfigured.   This step should be used if the SD Card format is unknown or needs to be reconfigured.  
 +
 +==== Using SD Card Formatter ====
  
 Ensure you have the following application installed on your computer. Ensure you have the following application installed on your computer.
Line 54: Line 56:
   - **Formatting Options** = Select Quick Format{{ :resources:tools-software:linux-software:zynq_images:sd_card_formatter_gui.png?400 |}}   - **Formatting Options** = Select Quick Format{{ :resources:tools-software:linux-software:zynq_images:sd_card_formatter_gui.png?400 |}}
   - Once set, click the **Format** button    - Once set, click the **Format** button 
-  - The program will notify you that the formatting is complete.(could take several seconds){{ :resources:tools-software:linux-software:zynq_images:sd_card_format_success.png?400 |}} +  - The program will notify you that the formatting is complete.(could take several minutes){{ :resources:tools-software:linux-software:zynq_images:sd_card_format_success.png?400 |}}  
 + 
 +==== Using DISKPART via Windows command prompt==== 
 + 
 +Windows command prompt has **DISKPART** that is also capable of reformatting SD cards and other drives.  
 +  - Run Windows command prompt as administrator. 
 +  - Type 'list disk'. All current dives will be shown. 
 +  - Type 'select disk X' where X is the SD card drive number. (Do not mistake this part) 
 +  - Type 'clean' to clean the drive. If an error occurs simply retry typing 'clean'
 +  - Type 'create partition primary'
 +  - Type 'format fs=FAT32'. The formatting may take 45 minutes or so. FAT32 is the tested file system type.  
 +  - After the progress is at 100%, type 'assign' to finalize the drive letter for Windows.
  
 ===== Flash the SD Card ===== ===== Flash the SD Card =====
resources/tools-software/linux-software/zynq_images/windows_hosts.txt · Last modified: 06 Feb 2023 07:25 by ALEXIS CZEZAR TORRENO