This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-software:sigmadsp_genfirmware [02 Jan 2013 22:42] – eliminate box Robin Getz | resources:tools-software:linux-software:sigmadsp_genfirmware [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 88: | Line 88: | ||
It is also possible to install the firmware file on the root filesystem. This allows to update it without having to update the whole kernel. To install it on the root file system copy it to the **"/ | It is also possible to install the firmware file on the root filesystem. This allows to update it without having to update the whole kernel. To install it on the root file system copy it to the **"/ | ||
- | <note important> | + | <WRAP important> |
===== More information ===== | ===== More information ===== |