Wiki

This version (26 Nov 2014 15:34) was approved by CsomI.

Partial Reconfiguration Plugin

The Partial Reconfiguration plugin works with the IIO Oscilloscope. You always use the latest version if possible.

Read more about Partial Reconfiguration by following this link: Partial Reconfiguration.

Screenshots / Descriptions

Reconfigurable Partition

  • Reconfiguration File: Displays the full path of a .bin file that can be selected using the file-chooser button on the left side. The new configuration applies automatically without the need of an Apply button.

Register Access

  • Core: Selects a register map between the ADC and the DAC.
  • PR_STATUS: Status register of the Partial Reconfiguration. Read Only.
  • PR_CONTROL: Control register of the Partial Reconfiguration. Read/Write access.
  • Read Button: Reads and displays the PR_STATUS and PR_CONTROL registers.
  • Write Button: Writes data to PR_CONTROL register.
resources/tools-software/linux-software/partial_reconfiguration_plugin.txt · Last modified: 20 Oct 2014 16:28 by DNechita