This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-software:network-config [19 May 2021 04:08] – added work around for networking on Kuiper version Brandon Bushey | resources:tools-software:linux-software:network-config [10 Jun 2022 20:21] (current) – organization Brandon Bushey | ||
---|---|---|---|
Line 90: | Line 90: | ||
If you desire to directly connect the Ethernet port of your host platform to the Ethernet port of another host, such as a PC (without the use of a network or router) a static configuration is required. | If you desire to directly connect the Ethernet port of your host platform to the Ethernet port of another host, such as a PC (without the use of a network or router) a static configuration is required. | ||
+ | |||
+ | ==== Kuiper Linux ==== | ||
In order to change the default settings of ADI Kuiper Linux please use the following steps. | In order to change the default settings of ADI Kuiper Linux please use the following steps. | ||
Line 164: | Line 166: | ||
Once complete, you will need to change the networking configuration of your PC. I am going to use a Windows 10 PC as an example, but similar procedures can be done with MAC OS and Linux based Machines. | Once complete, you will need to change the networking configuration of your PC. I am going to use a Windows 10 PC as an example, but similar procedures can be done with MAC OS and Linux based Machines. | ||
- | Windows | + | ==== Windows |
- Open up Control Panel > Network and Internet > Network and Sharing Center | - Open up Control Panel > Network and Internet > Network and Sharing Center | ||
- Click on **Change Adaptor Settings**{{ : | - Click on **Change Adaptor Settings**{{ : |