Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:linux-software:network-config [19 May 2021 04:08]
Brandon Bushey added work around for networking on Kuiper version
resources:tools-software:linux-software:network-config [10 Jun 2022 20:21]
Brandon Bushey organization
Line 90: Line 90:
  
 If you desire to directly connect the Ethernet port of your host platform to the Ethernet port of another host, such as a PC (without the use of a network or router) a static configuration is required. If you desire to directly connect the Ethernet port of your host platform to the Ethernet port of another host, such as a PC (without the use of a network or router) a static configuration is required.
 +
 +==== Kuiper Linux ====
  
 In order to change the default settings of ADI Kuiper Linux please use the following steps. In order to change the default settings of ADI Kuiper Linux please use the following steps.
Line 164: Line 166:
 Once complete, you will need to change the networking configuration of your PC. I am going to use a Windows 10 PC as an example, but similar procedures can be done with MAC OS and Linux based Machines. ​ Once complete, you will need to change the networking configuration of your PC. I am going to use a Windows 10 PC as an example, but similar procedures can be done with MAC OS and Linux based Machines. ​
  
-Windows ​Procedure:+==== Windows ​Operating System ====
   - Open up Control Panel > Network and Internet > Network and Sharing Center   - Open up Control Panel > Network and Internet > Network and Sharing Center
   - Click on **Change Adaptor Settings**{{ :​resources:​tools-software:​linux-software:​network_sharing_adaptor.png?​600 |}}   - Click on **Change Adaptor Settings**{{ :​resources:​tools-software:​linux-software:​network_sharing_adaptor.png?​600 |}}
resources/tools-software/linux-software/network-config.txt · Last modified: 10 Jun 2022 20:21 by Brandon Bushey