Wiki

This version (10 Jun 2022 20:21) was approved by Brandon Bushey.The Previously approved version (19 May 2021 04:08) is available.Diff

Network Configuration

There are two types of network configuration supported by the Analog Devices Kuiper Linux Distribution:

  • Dynamic Configuration (default)
  • Static Configuration

Updating the networking configuration will require a serial connection (UART), existing network connection, or having a physical keyboard/mouse/monitor connected. In all cases, to find out what your Ethernet port IP address is within ADI Kuiper Linux all you need to do is type the following:

  1. Open up a terminal window
  2. Type in the following command and hit <Enter>
    ifconfig
  3. Check the inet address of eth 0 to view the IP address assigned

Dynamic Host Configuration Protocol (DHCP)

By default, the Ethernet port of your host platform is configured for DHCP when using the ADI Kuiper Linux Distribution. Typically the Ethernet port is named eth 0, but if a platform has multiple Ethernet ports than those ports get enumerated (For example - Port 1 will be named eth 0 and Port 2 will be named eth 1)

Request a New DHCP IP Address

If you require a new IP address for some reason (Perhaps your internet isn't working or there are multiple devices using the same address) use the following instructions.

  1. Open up a terminal window
  2. Type in the following command and hit <Enter>
    sudo dhclient -r eth0
    1. Password = analog
  3. Type in the following command and hit <Enter>
    sudo dhclient eth0
    1. Password = analog
  4. Type in the following command and hit <Enter>
    ifconfig
  5. Check the inet address of eth 0 to view the new IP address assigned

Return from Static IP Address Configuration to DCHP IP Address

If you are returning from a static IP configuration, and require to have a new DHCP IP address assigned to the host platform, follow these steps:

  1. Open a terminal window
  2. Type in the following command and hit <Enter>
    enable_dhcp.sh
  3. Type in the following command and hit <Enter>
    ifconfig
  4. Check the inet address of eth 0 to view the new IP address assigned

Some versions of Kuiper have an incompatible configuration script for enabling static addresses. If you receive the error “can't read /etc/NetworkManager/NetworkManager.conf: No such file or directory”, you will need to do the following.

  1. Use your PC to get the updated script enable_dhcp.sh
  2. Copy that script onto your clip board
  3. Using a UART connection to the target device, open up a serial terminal with the correct COM port and set the baud rate to 115200
  4. Type in the user/password which is analog/analog
  5. Then type in the following commands:
sudo cat > /usr/local/bin/enable_dhcp.sh
#!/bin/bash
#
# Re-enable the default DHCP-based NetworkManager support. Use to revert the
# static IP configuration performed by the enable_static_ip.sh script.
#
# Example usage:
# enable_dhcp.sh
#
# WARNING: Do not use this script if there is a custom network configuration
# set up in /etc/network/interfaces as it will be overwritten.

set -e

if [[ ${UID} -ne 0 ]]; then
	echo "This script must be run as root!"
	exit 1
fi

if grep -qi kuiper "/etc/os-release"; then
	cat <<-EOF > /etc/dhcpcd.conf
		hostname
	EOF
	systemctl daemon-reload
	systemctl restart dhcpcd.service
else
	echo "Re-enabling DHCP via NetworkManager for all network interfaces"

	cat <<-EOF > /etc/network/interfaces
		# interfaces(5) file used by ifup(8) and ifdown(8)
		# Include files from /etc/network/interfaces.d:
		source-directory /etc/network/interfaces.d
	EOF

	# enable DHCP via NetworkManager (assumes the config file hasn't been touched much)
	sed -i 's/^managed=true/managed=false/' /etc/NetworkManager/NetworkManager.conf

	service network-manager restart
fi
#<Then Press "Ctrl + D" to save>
sudo chmod +x /usr/local/bin/enable_dhcp.sh

Setting a Static IP Address Configuration

If you desire to directly connect the Ethernet port of your host platform to the Ethernet port of another host, such as a PC (without the use of a network or router) a static configuration is required.

Kuiper Linux

In order to change the default settings of ADI Kuiper Linux please use the following steps.

  1. Open up a terminal window
  2. Type in the following command and hit <Enter>
    enable_static_ip.sh <ip address> eth0

    Where <ip address> is a usable and unique value such as 192.168.255.1

  3. Type in the following command and hit <Enter>
    ifconfig
  4. Check the inet address of eth 0 to make sure that the new IP address has been set properly

Some versions of Kuiper have an incompatible configuration script for enabling static addresses. If you receive the error “can't read /etc/NetworkManager/NetworkManager.conf: No such file or directory”, you will need to do the following.

  1. Use your PC to get the updated script enable_static_ip.sh
  2. Copy that script onto your clip board
  3. Using a UART connection to the target device, open up a serial terminal with the correct COM port and set the baud rate to 115200
  4. Type in the user/password which is analog/analog
  5. Then type in the following commands:
sudo cat > /usr/local/bin/enable_static_ip.sh
#!/bin/bash
#
# Enable a static IP for eth0 (or another interface) on Ubuntu-based setups.
# Note that the wanted IP address should be specified as the first argument;
# otherwise, it defaults to 192.168.0.101. Also, the interface can be specified
# as the second argument if the default (eth0) isn't wanted.
#
# Example usage:
# enable_static_ip.sh [10.66.99.101] [eth1]
#
# WARNING: Do not use this script if there is a custom network configuration
# set up in /etc/network/interfaces as it will be overwritten.

set -e

IP_ADDR=${1:-192.168.0.101}
ETH_DEV=${2:-eth0}

if [[ ${UID} -ne 0 ]]; then
	echo "This script must be run as root!"
	exit 1
fi

echo "Enabling the static IP address ${IP_ADDR} on ${ETH_DEV}"

if grep -qi kuiper "/etc/os-release"; then
	cat <<-EOF > /etc/dhcpcd.conf
		interface ${ETH_DEV}
		static ip_address=${IP_ADDR}/24
	EOF
	systemctl daemon-reload
	systemctl restart dhcpcd.service
else
	# disable NetworkManager (assumes the config file hasn't been touched much)
	sed -i 's/^managed=false/managed=true/' /etc/NetworkManager/NetworkManager.conf

	# set up loopback and add static IP config for ${ETH_DEV} (defaults to eth0)
	cat <<-EOF > /etc/network/interfaces
		auto lo
		iface lo inet loopback

		auto ${ETH_DEV}
		iface ${ETH_DEV} inet static
		address ${IP_ADDR}
		netmask 255.255.255.0
	EOF

	service network-manager restart
fi
#<Then Press "Ctrl + D" to save>
sudo chmod +x /usr/local/bin/enable_static_ip.sh

Once complete, you will need to change the networking configuration of your PC. I am going to use a Windows 10 PC as an example, but similar procedures can be done with MAC OS and Linux based Machines.

Windows Operating System

  1. Open up Control Panel > Network and Internet > Network and Sharing Center
  2. Click on Change Adaptor Settings
  3. Find the Ethernet Port and right-click and select Properties
  4. Find the Internet Protocol Version 4 (IPv4) and click on Properties
  5. Select the radio button that says Use this IP Address
  6. Enter in the IP address you want to use. To connect with the host board above use an address such as the subnet is the same but the final address is different. For example 192.168.255.2

Now you will be ready to directly connect your ADI Kuiper Linux host directly to your PC using the Ethernet port of both devices.

Remember once you are done to come back into the setting on your PC to change the Ethernet port back to the Obtain an IP address automatically radio button. Otherwise anything connected to your PC using the Ethernet port will likely not work.

End of Document

resources/tools-software/linux-software/network-config.txt · Last modified: 10 Jun 2022 20:21 by Brandon Bushey