This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-software:libiio:clients:lte_example [22 Nov 2016 20:53] – edit the structure Di Pu | resources:tools-software:linux-software:libiio:clients:lte_example [24 Feb 2020 23:07] – [Using File I/O] Robin Getz | ||
---|---|---|---|
Line 77: | Line 77: | ||
We will provide a few more pointers. | We will provide a few more pointers. | ||
- | * [[http:// | + | * [[http:// |
+ | * The MathWorks documentation talks about the "test model number", | ||
Launch the tool to generate an E-UTRA Test Model (E-TM) waveform. In this case, we will generated a waveform for a few different tests. | Launch the tool to generate an E-UTRA Test Model (E-TM) waveform. In this case, we will generated a waveform for a few different tests. | ||
- | * EVM for 64QAM modulation (E-UTRA Test Model 3.1) | + | * EVM for 64QAM modulation |
- | * EVM for 16QAM modulation (E-UTRA Test Model 3.2) | + | * EVM for 256QAM modulation at max power (E-UTRA Test Model 3.1a) |
- | * EVM for QPSK modulation | + | * EVM for 1024QAM modulation at max power (E-UTRA Test Model 3.1b) |
+ | * EVM for 16QAM modulation | ||
+ | * EVM for QPSK modulation | ||
All should be generated for 20MHz, FDD, and we change the output variable three times ('' | All should be generated for 20MHz, FDD, and we change the output variable three times ('' | ||