This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-software:libiio:clients:beacon_frame_receiver_simulink [15 Jul 2015 14:05] – modify dimension of info section and shape of downloads section Lucian Sin | resources:tools-software:linux-software:libiio:clients:beacon_frame_receiver_simulink [20 Oct 2016 10:05] – change link for IEEE 802.11 WLAN - Beacon Frame Receiver with USRP® Hardware Lucian Sin | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Beacon Frame Receiver Example ====== | ====== Beacon Frame Receiver Example ====== | ||
- | In this section, we will show an IEEE 802.11b beacon frame receiver example. In this example, FMCOMMS2 is used as RF front-end, which captures the WiFi signals over the air. These signals are then streamed from target to Simulink via the iio_sys_obj block. The Simulink model is shown in the figure below, where the Receiver and PLCP Display are from an existing Simulink example [[mw> | + | In this section, we will show an IEEE 802.11b beacon frame receiver example. In this example, FMCOMMS2 is used as RF front-end, which captures the WiFi signals over the air. These signals are then streamed from target to Simulink via the iio_sys_obj block. The Simulink model is shown in the figure below, where the Receiver and PLCP Display are from an existing Simulink example [[mw> |
<WRAP round info> | <WRAP round info> |