This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-software:libiio:clients:beacon_frame_receiver_simulink [14 Feb 2021 05:20] – fix links Robin Getz | resources:tools-software:linux-software:libiio:clients:beacon_frame_receiver_simulink [14 Feb 2021 20:11] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 3: | Line 3: | ||
{{page>/ | {{page>/ | ||
- | In this section, we will show an IEEE 802.11b beacon frame receiver example. In this example, FMCOMMS2 is used as RF front-end, which captures the WiFi signals over the air. These signals are then streamed from target to Simulink via the iio_sys_obj block. The Simulink model is shown in the figure below, where the Receiver and PLCP Display are from an existing Simulink example [[mw> | + | In this section, we will show an IEEE 802.11b beacon frame receiver example. In this example, FMCOMMS2 is used as RF front-end, which captures the WiFi signals over the air. These signals are then streamed from target to Simulink via the iio_sys_obj block. The Simulink model is shown in the figure below, where the Receiver and PLCP Display are from an existing Simulink example [[mw> |
<WRAP round info> | <WRAP round info> | ||
Line 18: | Line 18: | ||
* [[https:// | * [[https:// | ||
</ | </ | ||
- | Its initialization functions are based on the ones of [[http:// | + | Its initialization functions are based on the ones of [[mw>help/ |