This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-software:jesd_eye_scan [18 Mar 2021 16:24] – [Related device drivers] Michael Hennerich | resources:tools-software:linux-software:jesd_eye_scan [22 Mar 2021 10:11] (current) – [Running the software] Michael Hennerich | ||
---|---|---|---|
Line 114: | Line 114: | ||
</ | </ | ||
- | === Running remote === | + | === Running remote |
- | The remote option uses the Secure SHell FileSystem (SSHFS). | + | When using the [[resources: |
+ | |||
+ | ssh -X root@IP-ADDRESS jesd_eye_scan | ||
+ | |||
+ | <WRAP box bggreen>< | ||
+ | < | ||
+ | dave@HAL9000:/ | ||
+ | root@10.44.3.53' | ||
+ | Select axi-adxcvr-rx device! | ||
+ | </ | ||
+ | |||
+ | |||
+ | |||
+ | === Running remote (sshfs) === | ||
+ | |||
+ | This remote option uses the Secure SHell FileSystem (SSHFS), and might be suitable for remote systems without X support, such as our minimal Microblaze systems. | ||
It therefore requires sshd running on the target. | It therefore requires sshd running on the target. | ||