Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:linux-software:gnuradio [20 Dec 2018 19:26]
travisfcollins Make Windows section header larger
resources:tools-software:linux-software:gnuradio [20 Dec 2018 19:28]
travisfcollins Move note about FMComms2
Line 2: Line 2:
  
 GNU Radio comes pre-installed on the [[../​../​tools-software/​linux-software/​zynq_images|SD card image]] that ships with the [[../​../​eval/​user-guides/​ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]],​ [[../​../​eval/​user-guides/​ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]],​ [[../​../​eval/​user-guides/​ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]],​ [[../​../​eval/​user-guides/​arradio|ARRADIO]]and [[../​../​eval/​user-guides/​ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]],​ as well as the gr-iio blocks. Gnu Radio can also be compiled for a host PC. GNU Radio comes pre-installed on the [[../​../​tools-software/​linux-software/​zynq_images|SD card image]] that ships with the [[../​../​eval/​user-guides/​ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]],​ [[../​../​eval/​user-guides/​ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]],​ [[../​../​eval/​user-guides/​ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]],​ [[../​../​eval/​user-guides/​arradio|ARRADIO]]and [[../​../​eval/​user-guides/​ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]],​ as well as the gr-iio blocks. Gnu Radio can also be compiled for a host PC.
- 
-<WRAP info> 
-Although the GNU Radio block is called "​FMCOMMS-2",​ it will work with the any of the AD-FMCOMMS[234],​ ADRV9361, ADRV9364, ADRV9363 or ARRADIO boards. The FMCOMMS-2 IIO blocks can run over the IP network or USB. By setting the "IIO context URI" parameter to the IP address of the target board, you can stream samples from/to the remote board. It should be preferred when possible, as it is faster, knowing that the target board does not have the processing power of your PC. 
-</​WRAP>​ 
  
 ===== Installing GNU Radio ===== ===== Installing GNU Radio =====
Line 87: Line 83:
  
  
 +<WRAP info>
 +Although the GNU Radio block is called "​FMCOMMS-2",​ it will work with the any of the AD-FMCOMMS[234],​ ADRV9361, ADRV9364, ADRV9363 or ARRADIO boards. The FMCOMMS-2 IIO blocks can run over the IP network or USB. By setting the "IIO context URI" parameter to the IP address of the target board, you can stream samples from/to the remote board. It should be preferred when possible, as it is faster, knowing that the target board does not have the processing power of your PC.
 +</​WRAP>​
  
 ==== Common ====  ​ ==== Common ====  ​
resources/tools-software/linux-software/gnuradio.txt · Last modified: 20 Dec 2018 19:28 by travisfcollins