This is an old revision of the document!
FMComms5 Plugin Description
The FMCOMMS5 plugin works with the IIO Oscilloscope. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the FMComms5 settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the AD9361 or the FPGA fabric) does not support that mode/precision.
If you want to go play with /sys/bus/iio/devices/….
and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the “refresh” button at the bottom of the GUI.
If you think the device has a setting that isn't managed by this tab, check out the fmcomms5 Advanced Plugin for the IIO Oscilloscope.
The FMComms5 view is divided in four sections:
Device Global Settings
Receive Chain
Transmit Chain
FPGA Settings
Device Global Settings
Active ENSM: Displays the active mode of the Enable State Machine.
Read More
ENSM Modes: Selects one of the available modes: FDD and TDD.
Read More
Calibration Mode: Displays the active calibration mode.
Read More
Calibration Modes: Selects one of the available modes: auto, manual, rf_dc_offs and tx_quad.
Read More
TRX Rate Governor: Displays the active option of the Rate Governors.
Read More
TRX Rate Governor Available: Selects one of the available options: nominal and highest_osr.
Read More
Filter FIR configuration
RX Path Rates: Lists the rates of: BBPLL, ADC, R2, R1, RF, RXSAMP.
Read More
TX Path Rates: Lists the rates of: TXSAMP, TF, T1, T2, DAC, BBPLL.
Read More
DCXO Coarse Tune: Selects the attribute for a coarse tune.
Read More
DCXO Fine Tune: Selects the attribute for a fine tune.
Read More
Note that all settings above apply to both ad9361 devices.
Receive Chain
RF Bandwidth(MHz): Configures RX analog filters: RX
TIA LPF and RX BB LPF.
Read More
Sampling Rate(MSPS): Selects the sample rate of the ADC.
Read More
RF Port Select: Selects the RF Port of the receive channels.
Read More
RX LO Frequency(MHz): Selects the RX local oscillator frequency. Range 70MHz to 6GHz with 1Hz tuning granularity.
Read More
-
Fastlock Profile: Selects a profile to be stored or recalled.
Store: Stores the selected profile.
Recall: Recalls the selected profile.
-
RX
Hardware Gain(dB): Controls the RX gain only in Manual Gain Control Mode (MGC).
Read More
RSSI(dB): Displays the received strength signal level.
Read More
Gain Control: Displays the active gain mode.
Read More
Gain Control Modes: Selects one of the available modes: manual, slow_attack, hybrid and fast_attack.
Read More
Note that only RF Bandwidth, Sampling Rate, RF Port Select and Tracking settings apply to both ad9361 devices.
Transmit Chain
RF Bandwidth(MHz): Configures TX analog filters: TX BB LPF and TX Secondary LPF.
Read More
Sampling Rate(MSPS): Selects the sample rate of the DAC.
Read More
RF Port Select: Selects the RF Port of the transmit channels.
Read More
TX LO Frequency(MHz): Selects the TX local oscillator frequency. Range 70MHz to 6GHz with 1Hz tuning granularity.
Read More
-
Fastlock Profile: Selects a profile to be stored or recalled.
Store: Stores the selected profile.
Recall: Recalls the selected profile.
TX
Attenuation(dB): Individually controlls attenuation for TX1 and TX2. The range is from 0 to -89.75
dB in 0.25dB steps.
Read More
Note that only RF Bandwidth, Sampling Rate and RF Port Select settings apply to both ad9361 devices.
FPGA Settings