Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linux-software:fmcomms2_plugin [12 Apr 2019 17:20] – More name changes to AD936X Travis Collinsresources:tools-software:linux-software:fmcomms2_plugin [12 Apr 2019 20:09] (current) – add note on relation of plugin naming Travis Collins
Line 1: Line 1:
 ===== AD936X Plugin Description ===== ===== AD936X Plugin Description =====
  
-The AD936X plugin works with the [[iio_oscilloscope|IIO Oscilloscope]]. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the AD936X settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the AD9361 or the FPGA fabric) does not support that mode/precision.+The AD936X plugin (formerly known as the FMComms2/3/4 Plugin) works with the [[iio_oscilloscope|IIO Oscilloscope]]. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the AD936X settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the AD9361 or the FPGA fabric) does not support that mode/precision.
  
 If you want to go play with ''/sys/bus/iio/devices/....'' and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the "refresh" button at the bottom of the GUI. If you want to go play with ''/sys/bus/iio/devices/....'' and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the "refresh" button at the bottom of the GUI.
resources/tools-software/linux-software/fmcomms2_plugin.txt · Last modified: 12 Apr 2019 20:09 by Travis Collins