This version (08 Feb 2021 10:18) was approved by Dan Nechita.
CN0357 Plugin Description
The CN0357 view is divided in three sections:
ADC Settings: Lists the available options of the
AD7790 converter.
Feedback Settings: Lists the available options of the
AD5270 rheostat or fixed resistor feedback.
System: Lists measurements and parameters of the
CN0357 system.
ADC Settings
Feedback Settings
Feedback Type: Allows user to declare the type of the feedback resistance that is being used on the CN0357 Board. It can be either the digital rheostat or a fixed resistor.
RDAC Value / Resistor (Ohm): The raw value to be written to the RDAC register of the rheostat. / The value of the resistor used instead.
Program Rheostat: Writes the value at RDAC Value field to the device.
System
Measurements
Data
Sensor Sensitivity (nA/ppm): The maximum amount of current in nanoamps (nA) the sensor will use per part per million (ppm).
Feedback Resistance (Ohm): The feedback resistance of the transimpedance amplifier on the CN0357 Board.
ppm/mV: The system conversion coefficient of ppm/
mV.
mV/ppm: The system conversion coefficient of
mV/ppm.
The measurements are being continuously displayed at regular intervals of 1 second.