This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-software:build-the-zynqmp-boot-image [30 Apr 2020 16:42] – Updated cygwin configuration to include microblaze compiler path Adrian Costina | resources:tools-software:linux-software:build-the-zynqmp-boot-image [10 Jan 2022 09:24] – [Usage] Stefan-Robert Raus | ||
---|---|---|---|
Line 40: | Line 40: | ||
< | < | ||
- | usage: build_zynqmp_boot_bin.sh system_top.hdf u-boot.elf (download | bl31.elf | < | + | usage: build_zynqmp_boot_bin.sh system_top.xsa u-boot.elf (download | bl31.elf | < |
</ | </ | ||
- | * Path to '' | + | * Path to '' |
* The 3rd argument must either be '' | * The 3rd argument must either be '' | ||
* An optionally 4th '' | * An optionally 4th '' | ||
* Build output is located in a local directory named: output_boot_bin. | * Build output is located in a local directory named: output_boot_bin. | ||
- | * This script requires Xilinx | + | * This script requires Xilinx |
* A simple way is to source vivado settings[32|64].sh for Linux: | * A simple way is to source vivado settings[32|64].sh for Linux: | ||
< | < | ||
- | $ source / | + | $ source / |
</ | </ | ||
Line 55: | Line 55: | ||
< | < | ||
- | export PATH=$PATH:/ | + | export PATH=$PATH:/ |
- | export PATH=$PATH:/ | + | export PATH=$PATH:/ |
- | export PATH=$PATH:/ | + | export PATH=$PATH:/ |
</ | </ | ||
- | <WRAP left tip round box 100%> | + | <WRAP left tip round box 100%> |
For those who don't want to build u-boot themselves.\\ | For those who don't want to build u-boot themselves.\\ | ||
The **u-boot.elf** can be extracted from the project folder on the [[resources/ | The **u-boot.elf** can be extracted from the project folder on the [[resources/ | ||
</ | </ |