Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:linux-software:adrv9002_plugin [17 Jul 2020 15:52]
Nuno Sá
resources:tools-software:linux-software:adrv9002_plugin [19 Mar 2021 10:18]
Michael Hennerich [ADRV9002 Plugin Description]
Line 1: Line 1:
 ===== ADRV9002 Plugin Description ===== ===== ADRV9002 Plugin Description =====
  
-The ADRV9002 plugin works with the [[.adrv9001:​iio_oscilloscope|IIO Oscilloscope]]. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the ADRV9002 settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the ADRV9002 or the FPGA fabric) does not support that mode/​precision.+The ADRV9002 plugin works with the [[resources:​tools-software:​linux-software:​iio_oscilloscope|IIO Oscilloscope]]. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the ADRV9002 settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the ADRV9002 or the FPGA fabric) does not support that mode/​precision.
  
 If you want to go play with ''/​sys/​bus/​iio/​devices/​....''​ and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the ''​Reload Settings''​ button at the bottom of the GUI. If you want to go play with ''/​sys/​bus/​iio/​devices/​....''​ and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the ''​Reload Settings''​ button at the bottom of the GUI.
resources/tools-software/linux-software/adrv9002_plugin.txt · Last modified: 19 Mar 2021 10:18 by Michael Hennerich