Wiki

This version is outdated by a newer approved version.DiffThis version (31 Jan 2023 01:59) was approved by Joyce Velasco.The Previously approved version (07 Nov 2022 18:34) is available.Diff

This is an old revision of the document!


ADI Kuiper Linux with support for Evaluation

This is a version of the standard ADI Kuiper Linux SD card image that has been customized to support product evaluation with the ACE software. This image is pre-configured to boot Linux on the ZedBoard and also enables the ZedBoard USB OtG port so that ACE can connect to the board for configuration and data capture using IIO over USB to simplify PC connections.

If you are looking for the normal ADI Kuiper Linux SD card image, that is available from this page: Kuiper Linux.

Requirements

  • You need a Host PC (Windows or Linux).
  • You need a SD card writer connected to above PC (Supported USB SD readers/writers are OK).

Download Linux Image

The BOLD is what you should type. It's not too much more than Special Agent Oso's three special steps, and it also allows you to go for that specialty coffee you have been craving.

Make sure you unzip the image using either 7-zip or on Linux it can be done via command-line unzip <image_name>.zip. The actual file that needs to be dumped to the SD card has to have the *.img extension.
Your SD-card needs to be at least 16 GB.
If your computer has security restrictions imposed by your company's IT department, which prevent you from writing data to SD-cards (or the data is encrypted when written on the SD-card), then consider using a computer that doesn't have such restrictions or communicating with your IT department to find a solution.
  • 28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 4, 16 September 2022
    • Supports EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ, EVAL-AD4630-16FMCZ and EVAL-ADAQ8092-FMCZ.
    • Default Image boot configuration expects an AD4630/4030 board.
    • To change to the ADAQ8092 board:
      • Configure the SD card boot project to be the zynq-zed-adv7511 per these Instructions and boot the ZedBoard
      • Connect to a ZedBoard USB serial port using putty or Teraterm at 115200 baud to get a terminal shell window.
      • Run the command eval-adaq8092 configure LVDS_MODE to change the boot configuration to the ADA8092 board.
      • Run the command eval-ad46430 to get a list of the options if you need to switch back to an AD4630/4030 board.
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r4-2022-09-16.zip 97f17a390601765bac28b4a5ba1a0fa5
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r4-2022-09-16.img 4a8ad263bd8a7de6ef68078135728ad7

Older Releases (Click to expand)

Older Releases (Click to expand)

  • 28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 3, 9 June 2022
    • Supports EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ and EVAL-AD4630-16FMCZ.
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r3-2022-06-09.zip ad07297789f48db0d3745f745f0eb19f
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace 2022-06-09.img 90385ab164742f4174a3e97400dcc4c1
  • 28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 2, 15 March 2022
    • Supports EVAL-AD4630-24FMCZ and EVAL-AD4030-24FMCZ.
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r2.zip de02c989dad3e6315962c4b411adb411
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace v2c.img 3ECF2D57FAAB86635EFA0E7EDC582C3B
  • 28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 1, 15 September 2021
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace.zip 4527bfa06821ba02160487d8a8b7dba0
  • Checksum 2021-07-28-ADI-Kuiper-full-for-ace.img f84e4f0094754d5eb84b48cbb50dfaba

Now, depending on if you are using Linux or Windows, follow these instructions to write the file to your SD card.

Once the SD card image is programmed it can be inserted into the host controller SD card slot. Follow the hardware setup guide for the evaluation board you are using to complete the setup to get up and running.

resources/tools-software/linux-software/adi-kuiper_images_for_ace.1675126784.txt.gz · Last modified: 31 Jan 2023 01:59 by Joyce Velasco