Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linux-software:adi-kuiper_images_for_ace [31 Jan 2023 01:59] – Replaced the obsolete Kuiper Linux page link Joyce Velascoresources:tools-software:linux-software:adi-kuiper_images_for_ace [03 Apr 2024 01:21] (current) – Added r5 image, removed r1 and r2 images Michael Bradley
Line 17: Line 17:
  
 <note warning>If your computer has security restrictions imposed by your company's IT department, which prevent you from writing data to SD-cards (or the data is encrypted when written on the SD-card), then consider using a computer that doesn't have such restrictions or communicating with your IT department to find a solution. </note> <note warning>If your computer has security restrictions imposed by your company's IT department, which prevent you from writing data to SD-cards (or the data is encrypted when written on the SD-card), then consider using a computer that doesn't have such restrictions or communicating with your IT department to find a solution. </note>
 +
 +<WRAP hi round download 80%>
 +  * **28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 5, 2 April 2024**
 +    * Supports the following evaluation boards:
 +      * EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ, EVAL-AD4630-16FMCZ
 +      * EVAL-ADAQ8092-FMCZ
 +      * EVAL-AD4858FMCZ
 +      * EVAL-AD4080FMCZ
 +    * After writing this image to an SD card, the boot configuration needs to be set to match the evaluation board that is going to be used with ACE.
 +      * The default boot configuration is for an EVAL-ADAQ8092-FMCZ board.
 +    * To configure for a different evaluation board, boot the ZedBoard with the imaged SD card, and connect a USB cable to the ZedBoard USB UART or OtG port. Then using a terminal program, e.g. putty or Teraterm, open a serial port at 115200 baud to get a terminal shell. 
 +    * Then run the script that corresponds to the board you want to use with the options required.  
 +      * ''eval-ad4630'' - same script for EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ, EVAL-AD4630-16FMCZ
 +      * ''eval-adaq8092''
 +      * ''eval-ad4858''
 +      * ''eval-ad4080''
 +    * Add '' configure'' after the script name to get a list of the different configuration options required by a given script.  Each script has specific configure options.  
 +      * For Example: ''eval-ad4858 configure'' to get the options, and then ''eval-ad4858 configure cmos'' to do the configuration action
 +      * If an invalid set of options is selected, errors will be reported.
 +
 +    * [[https://swdownloads.analog.com/cse/kuiper/2021-07-28-ADI-Kuiper-full-for-ace-r5-2024-04-02.zip|Actual file]]
 +  * md5sum 2021-07-28-ADI-Kuiper-full-for-ace-r5-2024-04-02.zip    ''56901ab486d6d3f1b5e62b2661f53827''
 +  * md5sum 2021-07-28-ADI-Kuiper-full-for-ace-r5-2024-04-02.img    ''33349d31cad19197ac706b80486e07f7''
 +</WRAP>
 +
 +<hidden Older Releases (Click to expand)>
  
 <WRAP hi round download 80%> <WRAP hi round download 80%>
Line 31: Line 57:
   * Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r4-2022-09-16.img    ''4a8ad263bd8a7de6ef68078135728ad7''   * Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r4-2022-09-16.img    ''4a8ad263bd8a7de6ef68078135728ad7''
 </WRAP> </WRAP>
- 
-<hidden Older Releases (Click to expand)> 
  
 <WRAP hi round download 80%> <WRAP hi round download 80%>
Line 40: Line 64:
   * Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r3-2022-06-09.zip     ''ad07297789f48db0d3745f745f0eb19f ''   * Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r3-2022-06-09.zip     ''ad07297789f48db0d3745f745f0eb19f ''
   * Checksum 2021-07-28-ADI-Kuiper-full-for-ace 2022-06-09.img    ''90385ab164742f4174a3e97400dcc4c1''   * Checksum 2021-07-28-ADI-Kuiper-full-for-ace 2022-06-09.img    ''90385ab164742f4174a3e97400dcc4c1''
-</WRAP> 
- 
-<WRAP hi round download 80%> 
-  * **28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 2, 15 March 2022** 
-    * Supports EVAL-AD4630-24FMCZ and EVAL-AD4030-24FMCZ. 
-    * [[https://swdownloads.analog.com/cse/kuiper/2021-07-28-ADI-Kuiper-full-for-ace-r2.zip|Actual file]] 
-  * Checksum 2021-07-28-ADI-Kuiper-full-for-ace-r2.zip     ''de02c989dad3e6315962c4b411adb411 '' 
-  * Checksum 2021-07-28-ADI-Kuiper-full-for-ace v2c.img    ''3ECF2D57FAAB86635EFA0E7EDC582C3B'' 
-</WRAP> 
- 
-<WRAP hi round download 80%> 
-  * **28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 1, 15 September 2021** 
-    * Supports EVAL-AD4630-24FMCZ only. 
-    * [[https://swdownloads.analog.com/cse/kuiper/2021-07-28-ADI-Kuiper-full-for-ace.zip|Actual file]] 
-  * Checksum 2021-07-28-ADI-Kuiper-full-for-ace.zip     ''4527bfa06821ba02160487d8a8b7dba0'' 
-  * Checksum 2021-07-28-ADI-Kuiper-full-for-ace.img     ''f84e4f0094754d5eb84b48cbb50dfaba'' 
 </WRAP> </WRAP>
  
resources/tools-software/linux-software/adi-kuiper_images_for_ace.txt · Last modified: 03 Apr 2024 01:21 by Michael Bradley