ADI Kuiper Linux with support for Evaluation
This is a version of the standard ADI Kuiper Linux SD card image that has been customized to support product evaluation with the ACE software. This image is pre-configured to boot Linux on the ZedBoard and also enables the ZedBoard USB OtG port so that ACE can connect to the board for configuration and data capture using IIO over USB to simplify PC connections.
If you are looking for the normal ADI Kuiper Linux SD card image, that is available from this page: Kuiper Linux.
Requirements
Download Linux Image
The BOLD is what you should type. It's not too much more than Special Agent Oso's three special steps, and it also allows you to go for that specialty coffee you have been craving.
Make sure you unzip the image using either
7-zip or on Linux it can be done via command-line
unzip <image_name>.zip. The actual file that needs to be dumped to the
SD card has to have the
*.img extension.
Your
SD-card needs to be at least 16
GB.
If your computer has security restrictions imposed by your company's IT department, which prevent you from writing data to
SD-cards (or the data is encrypted when written on the
SD-card), then consider using a computer that doesn't have such restrictions or communicating with your IT department to find a solution.
28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 4, 16 September 2022
Supports EVAL-AD4630-24FMCZ, EVAL-AD4030-24FMCZ, EVAL-AD4630-16FMCZ and EVAL-ADAQ8092-FMCZ.
Default Image boot configuration expects an AD4630/4030 board.
To change to the ADAQ8092 board:
Configure the
SD card boot project to be the zynq-zed-adv7511 per these
Instructions and boot the ZedBoard
Connect to a ZedBoard
USB serial port using putty or Teraterm at 115200 baud to get a terminal shell window.
Run the command eval-adaq8092 configure LVDS_MODE
to change the boot configuration to the ADA8092 board.
Run the command eval-ad46430
to get a list of the options if you need to switch back to an AD4630/4030 board.
-
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace-r4-2022-09-16.zip
97f17a390601765bac28b4a5ba1a0fa5
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace-r4-2022-09-16.img
4a8ad263bd8a7de6ef68078135728ad7
Older Releases (Click to expand)
Older Releases (Click to expand)
28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 3, 9 June 2022
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace-r3-2022-06-09.zip
ad07297789f48db0d3745f745f0eb19f
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace 2022-06-09.img
90385ab164742f4174a3e97400dcc4c1
28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 2, 15 March 2022
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace-r2.zip
de02c989dad3e6315962c4b411adb411
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace v2c.img
3ECF2D57FAAB86635EFA0E7EDC582C3B
28 July 2021 ADI Kuiper Linux with support for ACE Evaluation - Release 1, 15 September 2021
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace.zip
4527bfa06821ba02160487d8a8b7dba0
Checksum 2021-07-28-
ADI-Kuiper-full-for-ace.img
f84e4f0094754d5eb84b48cbb50dfaba
Now, depending on if you are using Linux or Windows, follow these instructions to write the file to your SD card.
Once the SD card image is programmed it can be inserted into the host controller SD card slot. Follow the hardware setup guide for the evaluation board you are using to complete the setup to get up and running.