Wiki

This version is outdated by a newer approved version.DiffThis version (21 Apr 2023 14:13) was approved by Mark Thoren.The Previously approved version (31 Jan 2023 02:08) is available.Diff

This is an old revision of the document!


Release Notes

2021_r2

Release Image

  • Details about how to burn the SD card can be found on Kuiper Linux wiki page.

2021_r2 Release Image

  • Checksum image_2023-04-02-ADI-Kuiper-full.zip: 0cdcf6e131318113a137cf54335b9614
  • Checksum 2023-04-02-ADI-Kuiper-full.img: aeff476b577b45cc6ce6ce02403a57c2
  • 2021_r2 Boot Partition Files Only can be downloaded fromhere
  • MD5 checksum: 6d7dd2b202a84674f92e2fae4eb4cb4b

Known issues

1. Kuiper image does not extend to the capacity of SD Card.

Workaround: This happens when first use of a new created SD card is on a development board. If you see that the root fs partition is not extended to the SD card size minus 2 GB (fixed size of boot partition), just open a terminal and type:

raspi-config --expand-rootfs

2. Writing SD cards with Balena Etcher (version 1.7.9) from Windows10 or Ubuntu Disk Image Writer from Ubuntu 20.04/ 22.04 may give an error at the end, on validating SD card.

Even so, SD cards should be written properly, so you can ignore it. As alternatives you can use Win32 Disk Imager (version 1.0) from Windows or 'dd' command from linux systems.


3. Video output may not work. There are two scripts that can be run in Kuiper terminal: enable_dummy_display.sh - which is used to create a display for zynq based boards and fix_x11.sh - which is used to create display for zynqmp based boards. Running the one for zynq on a zynqmp device or vice versa will broke video output. The solution is to delete the wrong created file if there exists (/usr/share/X11/xorg.conf.d/xorg.conf is created by enable_dummy_display.sh and /etc/X11/xorg.conf is created by fix_x11.sh).

Also, if image is not shown properly using Display Port, check here the list of monitors supported by Xilinx


4. Keyboard layout may revert back to English(UK) - default one. This is expected behavior in Raspberry Pi OS ( you can find the whole discussion here ).


5. On Arria10 SOC with cn0506_mii, IPs are not assigned on both ports even if dhcp is enabled.


6. IIO-Oscilloscope v0.15 has an error regarding reading from DAC buffer. Previous version - v0.14 - should work fine. Newer versions, until v0.16 will be built, can be downloaded from github actions artifacts.

Supported Projects

Kuiper Linux Supported Projects and Platforms

Sources

Component Repo Branch Version/Git sha
Kuiper base image bullseye
Kernel 5.10
Scopy scopy.git v1.4.1
Libm2k libm2k.git v0.7.0
Pyadi-iio pyadi-iio.git v0.0.13
Gnuradio https://www.gnuradio.org/ 3.8.2
Kuiper adi-kuiper-gen.git 2021_R2 7100cab
HDL hdl.git hdl_2021_r2 a83056b
Linux linux.git 2021_R2 64e7a60
Linux_RPI linux.git rpi-5.10.y 877f062
Linux_image_ADI-scripts linux_image_ADI-scripts.git masterea26993
Libiio libiio.git 2021_R2 accb7b5
IIO-Osc iio-oscilloscope.git 2021_R2 d42513d
Libad9361-iio libad9361-iio.git 2021_R2 43643ab
Libad9166-iio libad9166-iio.git master 56ba037
Fru_tools fru_tools.git master 72951d8
IIO-fm-radio iio-fm-radio.git master 6c63519
Wiki-scripts wiki-scripts.git master b65ef59
Jesd-eye-scan-gtk jesd-eye-scan-gtk.git master 693567d
Diagnostic_report diagnostic_report.git master a39da05
Colorimeter colorimeter.git 2021_R2 524674a

Support

Analog Devices provides online support for anyone using Analog Devices reference designs via EngineerZone

Old Releases (Click to expand)

Old Releases (Click to expand)

  • 4 August 2022 release (2021_r1)
  • Checksum image_2022-08-04-ADI-Kuiper-full.zip: 9201b9e6580a0ce5c606f40f99c11b9a
  • Checksum 2022-08-04-ADI-Kuiper-full.img: dbbee112f5174dc23b4f5142994e4ff9
  • 28 July 2021 release (2019_r2)
  • Checksum image_2021-07-28-ADI-Kuiper-full.zip: 279097240dec7156ff5e15b7ce0b8a25
  • Checksum 2021-07-28-ADI-Kuiper-full.img: b160453396e482234094a92134769ec6
  • 22 June 2020 release (2019_r1)
  • Checksum 2019_R1-2020_06_22.img.xz 6ac6fc0733baba361acb66bd4cb050be
  • Checksum 2019_R1-2020_06_22.img 3135f400387c39f29dc877e68636a875
  • 23 May 2019 release (2018_R2)
  • Checksum 2018_R2-2019_05_23.img.xz c377ca95209f0f3d6901fd38ef2b4dfd
  • Checksum 2018_R2-2019_05_23.img 59c2fe68118c3b635617e36632f5db0b
  • 26 June 2018 release (2018_R1)
  • Checksum 2018_R1-2018_06_26.img.xz 5075da2695de84c88f086e85f1a6da51
  • Checksum 2018_R1-2018_06_26.img e48c63736517b4c4051be5486fd62ad5
  • 29 January 2018 release (2017_R1)
  • Checksum 2017_R1-2018_01_29.img.xz 020d696244655d19056ce1fff1f63f25
  • Checksum 2017_R1-2018_01_29.img a698a6ef59825bd63654c1d45b99f4c8
  • 29 June 2017 release (2016_R2)
  • Checksum 2016_R2-2017_06_29.img.xz 9f20adb27c5502a96fa56fa0f3088bd9
  • Checksum 2016_R2-2017_06_29.img 71b91e14dd1bd83779487850461440ea
  • 23 December 2016 release (2016_R1)
  • Checksum 2016_R1-2016_12_23.img.xz f167bfad87f9b9856d3b94297385a375
  • Checksum 2016_R1-2016_12_23.img edf8ea425576c9dd913e74e44c404e04
  • 26 July 2016 release (2015_R2)
  • Checksum 2015_R2-2016_07_26.img.xz 1520D974FBAADA6107B4C41606C40264
  • Checksum 2015_R2-2016_07_26.img E0D5748101D476FCA807C20EEF03E788
  • 22 December 2015 release (2015_R1)
  • Checksum 2015_R1-2015_12_22.img.xz a8f3ed68625043e180c95677123794bd
  • Checksum 2015_R1-2015_12_22.img fd1e4154e59e7dc62e508a4cdc522db5
  • 6 February 2015 release (2014_R2)
  • Checksum 2014_R2-2015_02_06.img.xz bb76031fcd68fd9b1a175a2f7fd3e053
  • Checksum 2014_R2-2015_02_06.img 132d03a2888db34f10f0ebbcb3100ae7
resources/tools-software/linux-software/adi-kuiper_images/release_notes.1682001839.txt.gz · Last modified: 20 Apr 2023 16:43 by Stefan-Robert Raus