This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:linux-software:adi-kuiper_images:release_notes [31 Jan 2023 02:08] Joyce Velasco Replaced the obsolete Kuiper Linux page link |
resources:tools-software:linux-software:adi-kuiper_images:release_notes [20 Apr 2023 16:43] Stefan-Robert Raus Add sources and link to supported projects for 2021_r2 |
||
---|---|---|---|
Line 2: | Line 2: | ||
<WRAP center round box 100%> | <WRAP center round box 100%> | ||
- | ===== 2021_r1 ===== | + | ===== 2021_r2 ===== |
| | ||
==== Release Image ==== | ==== Release Image ==== | ||
Line 9: | Line 9: | ||
<WRAP lo round download 80%> | <WRAP lo round download 80%> | ||
- | **2021_r1 Release Image** | + | **2021_r2 Release Image** |
- | * [[https://swdownloads.analog.com/cse/kuiper/image_2022-08-04-ADI-Kuiper-full.zip|Image file]] | + | * [[https://swdownloads.analog.com/cse/kuiper/image_2023-04-02-ADI-Kuiper-full.zip|Image file]] |
- | * Checksum image_2022-08-04-ADI-Kuiper-full.zip: ''9201b9e6580a0ce5c606f40f99c11b9a'' | + | * Checksum image_2023-04-02-ADI-Kuiper-full.zip: ''0cdcf6e131318113a137cf54335b9614'' |
- | * Checksum 2022-08-04-ADI-Kuiper-full.img: ''dbbee112f5174dc23b4f5142994e4ff9'' | + | * Checksum 2023-04-02-ADI-Kuiper-full.img: ''aeff476b577b45cc6ce6ce02403a57c2'' |
</WRAP> | </WRAP> | ||
<WRAP lo round download 80%> | <WRAP lo round download 80%> | ||
- | * 2021_r1 Boot Partition Files Only can be downloaded from [[https://swdownloads.analog.com/cse/boot_partition_files/2021_r1/latest_boot_partition.tar.gz|here]] | + | * 2021_r2 Boot Partition Files Only can be downloaded from[[https://swdownloads.analog.com/cse/boot_partition_files/2021_r2/latest_boot_partition.tar.gz|here]] |
- | * MD5 checksum: ''b164bc154aeecd3f5454a1c8c6af5479'' | + | * MD5 checksum: ''6d7dd2b202a84674f92e2fae4eb4cb4b'' |
</WRAP> | </WRAP> | ||
* For Microblaze images, see [[:resources:tools-software:linux-drivers:platforms:microblaze_loading| Microblaze images]] | * For Microblaze images, see [[:resources:tools-software:linux-drivers:platforms:microblaze_loading| Microblaze images]] | ||
* For Nios2 images, see [[:resources:tools-software:linux-drivers:platforms:nios2 | Nios2 Linux on the Altera Boards]] | * For Nios2 images, see [[:resources:tools-software:linux-drivers:platforms:nios2 | Nios2 Linux on the Altera Boards]] | ||
- | * [[repo>adi-kuiper-gen/releases/tag/2021_r1|Github Release Notes for Kuiper]] | + | * [[repo>adi-kuiper-gen/releases/tag/2021_r2|Github Release Notes for Kuiper]] |
==== Known issues ==== | ==== Known issues ==== | ||
Line 40: | Line 40: | ||
---- | ---- | ||
- | 3. Development boards may have a big delay (about 1.5 minutes) when are powered off ("poweroff", "reboot" of "shutdown" commands). | + | 3. Video output may not work. |
- | + | ||
- | Workaround: modify "DefaultTimeoutStopSec" in file "/etc/systemd/system.conf" from 90 sec to 10 sec (or any another smaller value), killing in this way all hanging processes after 10 seconds and begin "poweroff" procedure. | + | |
- | + | ||
- | ---- | + | |
- | + | ||
- | 4. Video output may not work. | + | |
There are two scripts that can be run in Kuiper terminal: enable_dummy_display.sh - which is used to create a display for zynq based boards and fix_x11.sh - which is used to create display for zynqmp based boards. | There are two scripts that can be run in Kuiper terminal: enable_dummy_display.sh - which is used to create a display for zynq based boards and fix_x11.sh - which is used to create display for zynqmp based boards. | ||
Running the one for zynq on a zynqmp device or vice versa will broke video output. | Running the one for zynq on a zynqmp device or vice versa will broke video output. | ||
Line 55: | Line 49: | ||
---- | ---- | ||
- | 5. Keyboard layout may revert back to English(UK) - default one. | + | 4. Keyboard layout may revert back to English(UK) - default one. |
This is expected behavior in Raspberry Pi OS ( you can find the whole discussion [[ https://forums.raspberrypi.com/viewtopic.php?t=191479 | here ]] ). | This is expected behavior in Raspberry Pi OS ( you can find the whole discussion [[ https://forums.raspberrypi.com/viewtopic.php?t=191479 | here ]] ). | ||
---- | ---- | ||
- | 6. On Arria10 SOC with cn0506_mii, IPs are not assigned on both ports even if dhcp is enabled. | + | 5. On Arria10 SOC with cn0506_mii, IPs are not assigned on both ports even if dhcp is enabled. |
---- | ---- | ||
- | 7. Arria10 SOC, Cyclone5 SOC and DE10 Nano boards will automatically start-up few seconds after "poweroff" commmand is given and the board shuts down. | + | 6. IIO-Oscilloscope v0.15 has an error regarding reading from DAC buffer. Previous version - v0.14 - should work fine. Newer versions, until v0.16 will be built, can be downloaded from [[repo>iio-oscilloscope/actions?query=branch%3Amaster|github actions artifacts]]. |
- | + | ||
- | Workaround: you can disable watchdog from u-boot, with the risk that boot process to hang if there are issues. | + | |
- | ---- | + | ==== Supported Projects ==== |
- | 8. ADI Diagnostic Report generate an empty report when is ran from System Tools Menu. | + | [[:resources:tools-software:linux-software:kuiper-linux:project-list|Kuiper Linux Supported Projects and Platforms]] |
+ | |||
+ | ==== Sources ==== | ||
+ | |||
+ | <WRAP round download 100%> | ||
+ | |< 100% 30% 30% 20% 20% 20% >| | ||
+ | ^Component ^Repo ^Branch ^Version/Git sha ^ | ||
+ | | Kuiper base image | | |**bullseye**| | ||
+ | | Kernel | | |**5.10** | | ||
+ | | Scopy | [[repo>scopy.git]] | |**v1.4.1** | | ||
+ | | Libm2k | [[repo>libm2k.git]] | |**v0.7.0** | | ||
+ | | Pyadi-iio | [[repo>pyadi-iio.git]] | |**v0.0.13** | | ||
+ | | Gnuradio | https://www.gnuradio.org/ | |**3.8.2** | | ||
+ | | Kuiper | [[repo>adi-kuiper-gen.git]] | 2021_R2 |**7100cab** | | ||
+ | | HDL | [[repo>hdl.git]] | hdl_2021_r2 |**a83056b** | | ||
+ | | Linux | [[repo>linux.git]] | 2021_R2 |**64e7a60** | | ||
+ | | Linux_RPI | [[repo>linux.git]] | rpi-5.10.y |**877f062** | | ||
+ | | Linux_image_ADI-scripts | [[repo>linux_image_ADI-scripts.git]] | master|**ea26993**| | ||
+ | | Libiio | [[repo>libiio.git]] | 2021_R2 |**accb7b5**| | ||
+ | | IIO-Osc | [[repo>iio-oscilloscope.git]] | 2021_R2 |**d42513d**| | ||
+ | | Libad9361-iio | [[repo>libad9361-iio.git]] | 2021_R2 |**43643ab**| | ||
+ | | Libad9166-iio | [[repo>libad9166-iio.git]] | master |**56ba037**| | ||
+ | | Fru_tools | [[repo>fru_tools.git]] | master |**72951d8**| | ||
+ | | IIO-fm-radio | [[repo>iio-fm-radio.git]] | master |**6c63519**| | ||
+ | | Wiki-scripts | [[repo>wiki-scripts.git]] | master |**b65ef59**| | ||
+ | | Jesd-eye-scan-gtk | [[repo>jesd-eye-scan-gtk.git]]| master |**693567d**| | ||
+ | | Diagnostic_report | [[repo>diagnostic_report.git]]| master |**a39da05**| | ||
+ | | Colorimeter | [[repo>colorimeter.git]] | 2021_R2 |**524674a**| | ||
+ | </WRAP> | ||
- | Workaround: run "adi_diagnostic_report" command from terminal. | ||
==== Support ==== | ==== Support ==== | ||
+ | |||
Analog Devices provides online support for anyone using Analog Devices reference designs via [[ez>community|EngineerZone]] | Analog Devices provides online support for anyone using Analog Devices reference designs via [[ez>community|EngineerZone]] | ||
</WRAP> | </WRAP> | ||
+ | |||
<WRAP> | <WRAP> | ||
<hidden Old Releases (Click to expand)> | <hidden Old Releases (Click to expand)> | ||
+ | |||
+ | <WRAP lo round download 80%> | ||
+ | * **4 August 2022 release (2021_r1) ** | ||
+ | * [[https://swdownloads.analog.com/cse/kuiper/image_2022-08-04-ADI-Kuiper-full.zip|Actual file]] | ||
+ | * Checksum image_2022-08-04-ADI-Kuiper-full.zip: ''9201b9e6580a0ce5c606f40f99c11b9a'' | ||
+ | * Checksum 2022-08-04-ADI-Kuiper-full.img: ''dbbee112f5174dc23b4f5142994e4ff9'' | ||
+ | </WRAP> | ||
<WRAP lo round download 80%> | <WRAP lo round download 80%> |