Wiki

This version is outdated by a newer approved version.DiffThis version (10 Jan 2022 17:31) is a draft.
Approvals: 0/1
The Previously approved version (10 Jan 2022 17:25) is available.Diff

This is an old revision of the document!


HDL and Linux projects are build whenever there are new commits in HDL or Linux repositories. Output boot files are structured in folders as they would be on SD card, and archived.

Master Boot partition files

  • MD5 checksum can be verified here
  • It is recommended to use master boot files only if you really need them (for example features that are not part of any release yet) since the files may not be always in a good state. Check Latest release for most recent tested boot files.
  • Inside downloaded archive is a ReadMe.txt file describing what files you need to copy on boot partition root depending on your hardware setup, and VERSION.txt file containing build dates and git commits.

Master Microblaze images

  • It is recommended to use master microblaze images only if you really need them (for example features that are not part of any release yet) since the files may not be always in a good state. Check Latest microblaze released images for most recent and tested images.
  • Inside every archive there is system_top.bit, simpleImage.<project name>.strip and a script to program it.

Master Nios2 images

  • It is recommended to use master nios2 images only if you really need them (for example features that are not part of any release yet) since the files may not be always in a good state. Check Latest nios2 released images for most recent and tested images.
  • Inside every archive, there is zimage, <project name>.sof and a script to program it.

Master NO-OS files

resources/tools-software/linux-software/adi-kuiper_images/master.1641832309.txt.gz · Last modified: 10 Jan 2022 17:31 by Stefan-Robert Raus