This is an old revision of the document!
ADAV801 and ADAV803 differs in serial interface. ADAV801 uses SPI, while ADAV803 uses I2C.
Function | File |
---|---|
driver | sound/soc/codecs/adav80x.c |
include | sound/soc/codecs/adav80x.h |
Name | Description |
---|---|
VINL | Left Analog Input |
VINR | Right Analog Input |
VOUTL | Left Analog Output |
VOUTR | Right Analog Output |
Name | Description |
---|---|
Master Playback Volume | DAC Volume |
Master Playback Switch | Mute/Unmute DAC output |
Master Capture Switch | ADC Volume |
Master Capture Volume | Mute/Unmute ADC input |
PGA Capture Volume | Input PGA gain |
ADC High Pass Filter Switch | Enable/Disable ADC high-pass filter |
Playback De-emphasis Switch | Enable/Disable playback de-emphassis |
Capture Select | Select the serial port capture source. Possible values: “ADC”, “Playback”, “Aux Playback” |
Aux Capture Select | Select the auxiliary serial port capture source. Possible values: “ADC”, “Playback”, “Aux Playback” |
DAC Select | Select the DAC signal source. Possible values: “ADC”, “Playback”, “Aux Playback” |
Name | Supported by driver | Description |
---|---|---|
SND_SOC_DAIFMT_I2S | yes | I2S Justified mode |
SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode |
SND_SOC_DAIFMT_LEFT_J | yes | Left Justified mode |
SND_SOC_DAIFMT_DSP_A | no | data MSB after FRM LRC |
SND_SOC_DAIFMT_DSP_B | no | data MSB during FRM LRC |
SND_SOC_DAIFMT_AC97 | no | AC97 mode |
SND_SOC_DAIFMT_PDM | no | Pulse density modulation |
SND_SOC_DAIFMT_NB_NF | yes | Normal bit- and frameclock |
SND_SOC_DAIFMT_NB_IF | no | Normal bitclock, inverted frameclock |
SND_SOC_DAIFMT_IB_NF | no | Inverted frameclock, normal bitclock |
SND_SOC_DAIFMT_IB_IF | no | Inverted bit- and frameclock |
SND_SOC_DAIFMT_CBM_CFM | yes | Codec bit- and frameclock master |
SND_SOC_DAIFMT_CBS_CFM | no | Codec bitclock slave, frameclock master |
SND_SOC_DAIFMT_CBM_CFS | no | Codec bitclock master, frameclock slave |
SND_SOC_DAIFMT_CBS_CFS | yes | Codec bit- and frameclock slave |
There is no dedicated Blackfin STAMP evaluation board for the ADAV80X. During test and driver development we used the EVAL-ADAV801/ADAV803 board.
It can be easily wired to the Blackfin STAMP SPORT header.
Function | File |
---|---|
driver | sound/soc/blackfin/bfin-eval-adav80x.c |
For ADAV801, enable SPI:
Device Drivers ---> [*] SPI support ---> *** SPI Master Controller Drivers *** <*> SPI controller driver for ADI Blackfin5xx
For ADAV803, enable I2C:
Device Drivers ---> [*] I2C support ---> [*] I2C Hardware Bus support ---> *** I2C system bus drivers (mostly embedded / system-on-chip) *** <*> Blackfin TWI I2C support (100) Blackfin TWI I2C clock (kHz)
Enable ALSA SoC evaluation board driver:
Device Drivers ---> <M> Sound card support ---> <M> Advanced Linux Sound Architecture ---> <M> ALSA for SoC audio support ---> <M> Support for the EVAL-ADAV80X boards on Blackfin eval boards
Default setting for the 12-way DIP switch: from SW11 to SW0 - 110001110001. Keep all switch and jumpers as default value defined in the manual, except:
To test using BF537-STAMP board, connect play and rec port on the ADAV80X evaluation board with SPORT0 on STAMP. Connect CPORT pins also to corresponding pins STAMP. Also, please make sure to connect the GND of the two boards together to get better signal.
Load the driver and make sure the sound card is properly instantiated.
This specifies any shell prompt running on the target
root:/> modprobe snd-bf5xx-i2s root:/> modprobe snd-soc-bf5xx-i2s root:/> modprobe snd-soc-adav80x root:/> modprobe snd-soc-bfin-eval-adav80x dma rx:3 tx:4, err irq:45, regs:ffc00800 asoc: ADAV80X <-> bf5xx-i2s mapping ok
This specifies any shell prompt running on the target
root:/> modprobe snd-pcm-oss root:/> tone TONE: generating sine wave at 1000 Hz... root:/> arecord -f cd | aplay Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo