Wiki

This version is outdated by a newer approved version.DiffThis version (05 Sep 2012 14:19) was approved by mhennerich.The Previously approved version (29 Apr 2012 22:49) is available.Diff

This is an old revision of the document!


ADAU1373 Sound CODEC Linux Driver

Supported Devices

Source Code

Status

Source Mainlined?
git Yes

Files

Example device initialization

For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.

For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.

21 Oct 2010 16:10

I2C

Declaring I2C devices

Unlike PCI or USB devices, I2C devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each I2C bus segment, and what address these devices are using. For this reason, the kernel code must instantiate I2C devices explicitly. There are different ways to achieve this, depending on the context and requirements. However the most common method is to declare the I2C devices by bus number.

This method is appropriate when the I2C bus is a system bus, as in many embedded systems, wherein each I2C bus has a number which is known in advance. It is thus possible to pre-declare the I2C devices that inhabit this bus. This is done with an array of struct i2c_board_info, which is registered by calling i2c_register_board_info().

So, to enable such a driver one need only edit the board support file by adding an appropriate entry to i2c_board_info.

For more information see: Documentation/i2c/instantiating-devices

21 Oct 2010 16:10
static struct i2c_board_info __initdata bfin_i2c_board_info[] = {
 
	[--snip--]
	{
		I2C_BOARD_INFO("adau1373", 0x1a),
	},
	[--snip--]
}
static int __init stamp_init(void)
{
	[--snip--]
	i2c_register_board_info(0, bfin_i2c_board_info,
				ARRAY_SIZE(bfin_i2c_board_info));
	[--snip--]
 
	return 0;
}
arch_initcall(board_init);

ASoC DAPM Widgets

Name Description
AIN1L Left Channel Input 1
AIN1R Right Channel Input 1
AIN2L Left Channel Input 2
AIN2R Right Channel Input 2
AIN3L Left Channel Input 3
AIN3R Right Channel Input 3
AIN4L Left Channel Input 4
AIN4R Right Channel Input 4
DMIC1DAT Serial Data Input Digital Microphone 1 and 2
DMIC2DAT Serial Data Input Digital Microphone 3 and 4
LOUT1L Left Channel Line Output 1
LOUT1R Right Channel Line Output 1
LOUT2L Left Channel Line Output 2
LOUT2R Right Channel Line Output 2
HPL Left Headphone Output
HPR Right Headphone Output
SPKL Left Speaker Output
SPKR Right Speaker Output
EP Eearpiece Output
MICBIAS1 Micbias 1 supply
MICBIAS2 Micbias 2 supply

ALSA Controls

Name Description Configuration
AIF1 Capture Volume Digital Audio Interface A Recording Volume
AIF2 Capture Volume Digital Audio Interface B Recording Volume
AIF3 Capture Volume Digital Audio Interface C Recording Volume
ADC Capture Volume ADC Recording Volume
DMIC Capture Volume DMIC Recording Volume
Input 1 Capture Volume Input 1 Gain
Input 2 Capture Volume Input 2 Gain
Input 3 Capture Volume Input 3 Gain
Input 4 Capture Volume Input 4 Gain
Input 1 Boost Capture Volume Input 1 ADC Boost (+20dB)
Input 2 Boost Capture Volume Input 2 ADC Boost (+20dB)
Input 3 Boost Capture Volume Input 3 ADC Boost (+20dB)
Input 4 Boost Capture Volume Input 4 ADC Boost (+20dB)
AIF1 Playback Volume Digital Audio Interface A Playback Datapath Volume
AIF2 Playback Volume Digital Audio Interface B Playback Datapath Volume
AIF3 Playback Volume Digital Audio Interface C Playback Datapath Volume
DAC1 Playback Volume DAC1 Playback Volume
DAC2 Playback Volume DAC2 Playback Volume
Lineout1 Playback Volume Lineout 1 Volume
Lineout2 Playback Volume Lineout 2 Volume Single-ended lineout
Speaker Playback Volume Speaker Out Volume
Headphone Playback Volume Heaphone Out Volume
Earpiece Playback Volume Earpiece Amplifier Gain
AIF1 Boost Playback Volume Digital Audio Interface A Playback Gain (+6dB)
AIF2 Boost Playback Volume Digital Audio Interface B Playback Gain (+6dB)
AIF3 Boost Playback Volume Digital Audio Interface C Playback Gain (+6dB)
AIF1 Boost Capture Volume Digital Audio Interface C Recording Gain (+6dB)
AIF2 Boost Capture Volume Digital Audio Interface C Recording Gain (+6dB)
AIF3 Boost Capture Volume Digital Audio Interface C Recording Gain (+6dB)
ADC Boost Capture Volume ADC Recording Gain (+6dB)
DMIC Boost Capture Volume DMIC Recording Gain (+6dB)
DAC1 Boost Playback Volume DAC1 Playback Gain (+6dB)
DAC2 Boost Playback Volume DAC1 Playback Gain (+6dB)
Speaker Boost Playback Volume Speaker Output Gain
Lineout1 LR Mux Lineout1 Left-Right Mux (Mono Stereo Control)
Valid values: “Mute”, “Right Channel (L+R)”, “Left Channel (L+R)”, “Stereo”
Lineout2 LR Mux Lineout2 Left-Right Mux (Mono Stereo Control)
Valid values: “Mute”, “Right Channel (L+R)”, “Left Channel (L+R)”, “Stereo”
Single-ended lineout
Speaker LR Mux Speaker Left-Right Mux (Mono Stereo Control)
Valid values: “Mute”, “Right Channel (L+R)”, “Left Channel (L+R)”, “Stereo”
HPF Cutoff High-pass-filter cutoff frequency.
Valid values: “3.7Hz”, “50Hz”, “100Hz”, … steps of 50Hz …, “800Hz”
HPF Switch Enable/Disable High-pass-filter
HPF Channel Hight-pass-filter channel.
Valid values: “Channel1”, “Channel2”, “Channel3”, “Channel4”, “Channel5”
Bass HPF Cutoff Bass High-pass-filter cutoff frequency.
Valid values: “158Hz”, “232Hz”, “347Hz”, “520Hz”
Bass Clip Level Threshold Signal Extend Density (Clip Level). Overdrive level for bass enhancement.
Valid values: “0.125”, “0.250”, “0.370”, “0.500”, “0.625”, “0.750”, “0.875”
Bass LPF Cutoff Bass Low-pass-filter cutoff frequency.
Valid values: “801Hz”, “1001Hz”
Bass Playback Switch Enable/Disable Bass Enhancement
Bass Playback Volume Bass Enhancement Gain
Bass Channel Bass Enhancement Channel.
Valid values: “Channel1”, “Channel2”, “Channel3”, “Channel4”, “Channel5”
3D Freq 3D Enhancement cutoff frequency (relative to the sampling rate).
Valid values: “No 3D”, “0.03125 fs”, “0.04583 fs”, “0.075 fs”, “0.11458 fs”, “0.16875 fs”, “0.27083 fs”
3D Level 3D Enhancement effect level.
Valid values: “0%”, “6.67%”, “13.33%”, “20%”, “26.67%”, “33.33%”, “40%”, “46.67%”, “53.33%”,
“60%”, “66.67%”, “73.33%”, “80%”, “86.67”, “93.33%”, “100%”
3D Playback Switch Enable/Disable 3D Enhancement
3D Playback Volume 3D Enhancement Gain
3D Channel 3D Enhancement Channel.
Valid values: “Channel1”, “Channel2”, “Channel3”, “Channel4”, “Channel5”
Zero Cross Switch Enable/Disable Zero-Cross-Detection for volume updates
DRC1 Channel Dynamic Range Control 1 Channel.
Valid values: “Channel1”, “Channel2”, “Channel3”, “Channel4”, “Channel5”
DRC2 Channel Dynamic Range Control 2 Channel.
Valid values: “Channel1”, “Channel2”, “Channel3”, “Channel4”, “Channel5”
DRC3 Channel Dynamic Range Control 3 Channel.
Valid values: “Channel1”, “Channel2”, “Channel3”, “Channel4”, “Channel5”

PLL Configuration

The ADAU1373 features two PLLs:

enum adau1373_pll {
    ADAU1373_PLL1 = 0,
    ADAU1373_PLL2 = 1,
};

Each PLLs input frequency can be selected from a variety of signals:

enum adau1373_pll_src {
    ADAU1373_PLL_SRC_MCLK1 = 0,
    ADAU1373_PLL_SRC_BCLK1 = 1,
    ADAU1373_PLL_SRC_BCLK2 = 2,
    ADAU1373_PLL_SRC_BCLK3 = 3,
    ADAU1373_PLL_SRC_LRCLK1 = 4,
    ADAU1373_PLL_SRC_LRCLK2 = 5,
    ADAU1373_PLL_SRC_LRCLK3 = 6,
    ADAU1373_PLL_SRC_GPIO1 = 7,
    ADAU1373_PLL_SRC_GPIO2 = 8,
    ADAU1373_PLL_SRC_GPIO3 = 9,
    ADAU1373_PLL_SRC_GPIO4 = 10,
    ADAU1373_PLL_SRC_MCLK2 = 11,
};

The input frequency must configured to be between 7813 and 27000000 Hz. The output frequency must be configured to be between 45158000 and 49152000. Configuring the PLL with other input or output frequency will fail.

The PLL runs at 1024 times the base sample rate. So for a 48000 Hz based sample rate you'd normally choose 49152000 Hz for the PLL output frequncey and for a 44100 Hz based sample rate 45158400 Hz.

DAI configuration

The codec driver registers three DAIs:

  • “adau1373-aif1” (Digital Audio Interface A)
  • “adau1373-aif2” (Digital Audio Interface B)
  • “adau1373-aif3” (Digital Audio Interface C)

Supported DAI formats

Name Supported by driver Description
SND_SOC_DAIFMT_I2S yes I2S Justified mode
SND_SOC_DAIFMT_RIGHT_J yes Right Justified mode
SND_SOC_DAIFMT_LEFT_J yes Left Justified mode
SND_SOC_DAIFMT_DSP_A no data MSB after FRM LRC
SND_SOC_DAIFMT_DSP_B yes data MSB during FRM LRC
SND_SOC_DAIFMT_AC97 no AC97 mode
SND_SOC_DAIFMT_PDM no Pulse density modulation
SND_SOC_DAIFMT_NB_NF yes Normal bit- and frameclock
SND_SOC_DAIFMT_NB_IF yes Normal bitclock, inverted frameclock
SND_SOC_DAIFMT_IB_NF yes Inverted frameclock, normal bitclock
SND_SOC_DAIFMT_IB_IF yes Inverted bit- and frameclock
SND_SOC_DAIFMT_CBM_CFM yes Codec bit- and frameclock master
SND_SOC_DAIFMT_CBS_CFM no Codec bitclock slave, frameclock master
SND_SOC_DAIFMT_CBM_CFS no Codec bitclock master, frameclock slave
SND_SOC_DAIFMT_CBS_CFS yes Codec bit- and frameclock slave

DAI sysclk

The DAIs can either use PLL1 or PLL2 as source. When configuring a DAI its rate should be set to the rate of the source PLL.

enum adau1373_clk_src {
    ADAU1373_CLK_SRC_PLL1 = 0,
    ADAU1373_CLK_SRC_PLL2 = 1,
};

Example DAI configuration

static int bfin_eval_adau1373_hw_params(struct snd_pcm_substream *substream,
	struct snd_pcm_hw_params *params)
{
	struct snd_soc_pcm_runtime *rtd = substream->private_data;
	struct snd_soc_dai *cpu_dai = rtd->cpu_dai;
	struct snd_soc_dai *codec_dai = rtd->codec_dai;
	int ret;
	int pll_rate;
 
	ret = snd_soc_dai_set_fmt(cpu_dai, SND_SOC_DAIFMT_I2S |
			SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBM_CFM);
	if (ret)
		return ret;
 
	ret = snd_soc_dai_set_fmt(codec_dai, SND_SOC_DAIFMT_I2S |
			SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBM_CFM);
	if (ret)
		return ret;
 
	switch (params_rate(params)) {
	case 48000:
	case 8000:
	case 12000:
	case 16000:
	case 24000:
	case 32000:
		pll_rate = 48000 * 1024;
		break;
	case 44100:
	case 7350:
	case 11025:
	case 14700:
	case 22050:
	case 29400:
		pll_rate = 44100 * 1024;
		break;
	default:
		return -EINVAL;
	}
 
	ret = snd_soc_dai_set_pll(codec_dai, ADAU1373_PLL1,
			ADAU1373_PLL_SRC_MCLK1, 12288000, pll_rate);
	if (ret)
		return ret;
 
	ret = snd_soc_dai_set_sysclk(codec_dai, ADAU1373_CLK_SRC_PLL1, pll_rate,
			SND_SOC_CLOCK_IN);
 
	return ret;
}
 
static int bfin_eval_adau1373_codec_init(struct snd_soc_pcm_runtime *rtd)
{
	struct snd_soc_dai *codec_dai = rtd->codec_dai;
	unsigned int pll_rate = 48000 * 1024;
	int ret;
 
	ret = snd_soc_dai_set_pll(codec_dai, ADAU1373_PLL1,
			ADAU1373_PLL_SRC_MCLK1, 12288000, pll_rate);
	if (ret)
		return ret;
 
	ret = snd_soc_dai_set_sysclk(codec_dai, ADAU1373_CLK_SRC_PLL1, pll_rate,
			SND_SOC_CLOCK_IN);
 
	return ret;
}
static struct snd_soc_ops bfin_eval_adau1373_ops = {
	.hw_params = bfin_eval_adau1373_hw_params,
};
 
static struct snd_soc_dai_link bfin_eval_adau1373_dai = {
	.name = "adau1373",
	.stream_name = "adau1373",
	.cpu_dai_name = "bfin-i2s.0",
	.codec_dai_name = "adau1373-aif1",
	.platform_name = "bfin-i2s-pcm-audio",
	.codec_name = "adau1373.0-001a",
	.ops = &bfin_eval_adau1373_ops,
	.init = bfin_eval_adau1373_codec_init,
};

ADAU1373 evaluation board driver

There is no dedicated Blackfin STAMP evaluation board for the ADAU1373. During test and driver development we used the EVAL-ADAU1373 board.

It can be easily wired to the Blackfin STAMP SPORT header.

Source

Status

Source Mainlined?
In progress

Files

Kernel configuration

Device Drivers  --->
[*] I2C support  --->
[*]   I2C Hardware Bus support  --->
***     I2C system bus drivers (mostly embedded / system-on-chip) ***
<*>       Blackfin TWI I2C support
(100)     Blackfin TWI I2C clock (kHz)

Enable ALSA SoC evaluation board driver:

Device Drivers  --->
<M> Sound card support  --->
<M>   Advanced Linux Sound Architecture  --->
<M>     ALSA for SoC audio support  --->
<M>       Support for the EVAL-ADAU1373 boards on Blackfin eval boards

Hardware configuration

Connect the STAMP SPORT 0 port (P6) to the EVAL-ADAU1373 J23 and J28 headers.

Note that the SPORT has separate signals for the capture and playback clocks, while the ADAU1373 uses the same clock signals for both, so the EVAL-ADU1373 clock signal pins need to be connected to two STAMP pins each.

STAMP pin EVAL-ADAU1373 pin Function
P6-26 (SPORT 0 - PJ2_SCL) J23-1 I2C SCL
P6-24 (SPORT 0 - PJ3_SDA) J23-3 I2C SDA
P6-6 (SPORT 0 - PJ9_TSCLK0), P6-16 (SPORT 0 - PJ6_RSCLK0) J28-6 (A_BCLK) BCLK
P6-11 (SPORT 0 - PJ10_TFS0), P6-7 (SPORT 0 - PJ7_RFS0) J28-8 (A_LRC) LRCLK
P6-14 (SPORT 0 - PJ11_DT0PRI J28-10 (A_DACDAT) Playback data
P6-8 (SPORT 0 - PJ8_DR0PRI) J28-12 (A_ADCDAT) Captrue data
P6-33 J28-1 GND

Driver testing

Load the driver and make sure the sound card is properly instantiated.

<box 100% green|shell prompt running on the target>

root:/> modprobe snd-bf5xx-i2s
root:/> modprobe snd-soc-bf5xx-i2s
root:/> modprobe snd-soc-adau1373
root:/> modprobe snd-soc-bfin-eval-adau1373
dma rx:3 tx:4, err irq:45, regs:ffc00800
asoc: ADAU1373 <-> bf5xx-i2s mapping ok
</box>

<box 100% green|shell prompt running on the target>

root:/> modprobe snd-pcm-oss
root:/> tone
TONE: generating sine wave at 1000 Hz...

root:/> arecord -f cd | aplay
Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
</box>

resources/tools-software/linux-drivers/sound/adau1373.1346847570.txt.gz · Last modified: 05 Sep 2012 14:19 by mhennerich