This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:sound:adau1373 [01 Sep 2011 19:33] – [Hardware configuration] Lars-Peter Clausen | resources:tools-software:linux-drivers:sound:adau1373 [23 Feb 2017 12:47] (current) – Lars-Peter Clausen | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADAU1373 Sound CODEC Linux Driver ====== | ====== ADAU1373 Sound CODEC Linux Driver ====== | ||
+ | |||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | This driver supports the\\ | + | * [[adi> |
- | [[adi> | + | |
- | ====== Source Code ====== | + | ===== Evaluation Boards ===== |
+ | * [[adi> | ||
+ | |||
+ | ===== Source Code ===== | ||
==== Status ==== | ==== Status ==== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
- | | [[bfgit>linux-kernel?sound/ | + | | [[git.linux.org>sound/ |
==== Files ==== | ==== Files ==== | ||
Line 20: | Line 23: | ||
| include | [[git.linux.org> | | include | [[git.linux.org> | ||
- | ====== Example device initialization | + | ===== Example device initialization ===== |
{{page> | {{page> | ||
Line 100: | Line 103: | ||
| DAC2 Playback Volume | DAC2 Playback Volume | | | | DAC2 Playback Volume | DAC2 Playback Volume | | | ||
| Lineout1 Playback Volume | Lineout 1 Volume | | | | Lineout1 Playback Volume | Lineout 1 Volume | | | ||
- | | Lineout2 Playback Volume | Lineout | + | | Lineout2 Playback Volume | Lineout |
| Speaker Playback Volume | | Speaker Playback Volume | ||
| Headphone Playback Volume | Heaphone Out Volume| | | | Headphone Playback Volume | Heaphone Out Volume| | | ||
Line 180: | Line 183: | ||
^ Name ^ Supported by driver ^ Description ^ | ^ Name ^ Supported by driver ^ Description ^ | ||
- | | SND_SOC_DAIFMT_I2S | + | | SND_SOC_DAIFMT_I2S |
| SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode | | | SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode | | ||
| SND_SOC_DAIFMT_LEFT_J | | SND_SOC_DAIFMT_LEFT_J | ||
Line 306: | Line 309: | ||
^ Source | ^ Source | ||
- | | [[bfgit>linux-kernel?sound/ | + | | [[git.linux.org>sound/ |
==== Files ==== | ==== Files ==== | ||
Line 353: | Line 356: | ||
Load the driver and make sure the sound card is properly instantiated. | Load the driver and make sure the sound card is properly instantiated. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> modprobe snd-bf5xx-i2s | root:/> modprobe snd-bf5xx-i2s | ||
Line 362: | Line 365: | ||
asoc: ADAU1373 <-> bf5xx-i2s mapping ok | asoc: ADAU1373 <-> bf5xx-i2s mapping ok | ||
</ | </ | ||
- | </box> | + | </WRAP> |
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> modprobe snd-pcm-oss | root:/> modprobe snd-pcm-oss | ||
Line 374: | Line 377: | ||
Playing WAVE ' | Playing WAVE ' | ||
</ | </ | ||
- | </box> | + | </WRAP> |