Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:tools-software:linux-drivers:sound:adau1373 [05 Sep 2012 14:19]
mhennerich [Status]
resources:tools-software:linux-drivers:sound:adau1373 [08 Jun 2016 20:12]
larsc [Supported DAI formats]
Line 4: Line 4:
  
   * [[adi>​ADAU1373]]   * [[adi>​ADAU1373]]
 +
 +===== Evaluation Boards =====
 +  * [[adi>​EVAL-ADAU1373Z]]
 +
 ====== Source Code ====== ====== Source Code ======
  
 ==== Status ==== ==== Status ====
  
- Source ​  Mainlined? ​ ^+^ Source ^ Mainlined? ^
 | [[git.linux.org>​sound/​soc/​codecs/​adau1373.c|git]] | [[git.linux.org>​sound/​soc/​codecs/​adau1373.c|Yes]] | | [[git.linux.org>​sound/​soc/​codecs/​adau1373.c|git]] | [[git.linux.org>​sound/​soc/​codecs/​adau1373.c|Yes]] |
  
Line 178: Line 182:
  
 ^ Name ^ Supported by driver ^ Description ^ ^ Name ^ Supported by driver ^ Description ^
-| SND_SOC_DAIFMT_I2S ​    | yes | I2S Justified ​mode |+| SND_SOC_DAIFMT_I2S ​    | yes | I2S mode |
 | SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode | | SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode |
 | SND_SOC_DAIFMT_LEFT_J ​ | yes | Left Justified mode  | | SND_SOC_DAIFMT_LEFT_J ​ | yes | Left Justified mode  |
Line 304: Line 308:
  
 ^  Source ​ ^  Mainlined? ​ ^ ^  Source ​ ^  Mainlined? ​ ^
-| [[bfgit>linux-kernel?sound/​soc/​blackfin/​bfin-eval-adau1373.c|In progress]] | [[git.linux.org>​sound/​soc/​blackfin/​bfin-eval-adau1373.c|In progress]]+| [[git.linux.org>sound/​soc/​blackfin/​bfin-eval-adau1373.c|git]] | [[git.linux.org>​sound/​soc/​blackfin/​bfin-eval-adau1373.c|yes]] |
  
 ==== Files ==== ==== Files ====
Line 351: Line 355:
 Load the driver and make sure the sound card is properly instantiated. Load the driver and make sure the sound card is properly instantiated.
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
 root:/> modprobe snd-bf5xx-i2s root:/> modprobe snd-bf5xx-i2s
Line 360: Line 364:
 asoc: ADAU1373 <-> bf5xx-i2s mapping ok asoc: ADAU1373 <-> bf5xx-i2s mapping ok
 </​xterm>​ </​xterm>​
-</box>+</WRAP>
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
 root:/> modprobe snd-pcm-oss root:/> modprobe snd-pcm-oss
Line 372: Line 376:
 Playing WAVE '​stdin'​ : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo Playing WAVE '​stdin'​ : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
 </​xterm>​ </​xterm>​
-</box>+</WRAP>
resources/tools-software/linux-drivers/sound/adau1373.txt · Last modified: 23 Feb 2017 12:47 by larsc