Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:linux-drivers:regulator:adp150 [29 Aug 2011 21:09] – [Example platform device initialization] Michael Hennerichresources:tools-software:linux-drivers:regulator:adp150 [11 Feb 2016 21:15] (current) – [Status] Lars-Peter Clausen
Line 3: Line 3:
 ===== Supported Devices ===== ===== Supported Devices =====
  
-This driver supports the\\ +  * [[adi>ADP122]] 
-[[adi>ADP122]]\\ +  [[adi>ADP123]] 
-[[adi>ADP123]]\\ +  [[adi>ADP124]] 
-[[adi>ADP124]]\\ +  [[adi>ADP125]] 
-[[adi>ADP125]]\\ +  [[adi>ADP150]] 
-[[adi>ADP150]]\\ +  [[adi>ADP5022]]
-[[adi>ADP5022]]+
  
 +===== Evaluation Boards =====
 +
 +  * [[adi>EVAL-ADP122|ADP122-3.3-EVALZ]]
 +  * [[adi>ADP123-EVALZ]]
 +  * [[adi>EVAL-ADP124|ADP124-3.3-EVALZ]]
 +  * [[adi>ADP125CP-EVALZ]]
 +  * [[adi>EVAL-ADP150|ADP150CB-3.3-EVALZ]]
 +
 +==== Reference Circuits ====
 +
 +  * [[adi>CN0134]]
 +  * [[adi>CN0144]]
 +  * [[adi>CN0147]]
 +  * [[adi>CN0285]]
 +  * [[adi>CN0228]]
 +  * [[adi>CN0290]]
 +  * [[adi>CN0311]]
 ===== Description ===== ===== Description =====
  
Line 27: Line 43:
 ===== Status ===== ===== Status =====
  
- Source   Mainlined?  +^ Source ^ Mainlined? ^ 
-| [[bfgit>linux-kernel?drivers/regulator/fixed.c|git]] |  [[git.linux.org>drivers/regulator/fixed.c|Yes]]  |+| [[git.linux.org>drivers/regulator/fixed.c|git]] | [[git.linux.org>drivers/regulator/fixed.c|Yes]] |
  
 ===== Files ===== ===== Files =====
resources/tools-software/linux-drivers/regulator/adp150.1314644981.txt.gz · Last modified: 29 Aug 2011 21:09 by Michael Hennerich