This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Last revision Both sides next revision | ||
resources:tools-software:linux-drivers:platforms:nios2 [16 Dec 2021 15:31] Liviu Adace Updated download of prebuild images and added links to quickstart guides |
resources:tools-software:linux-drivers:platforms:nios2 [10 Jan 2022 17:39] Stefan-Robert Raus |
||
---|---|---|---|
Line 16: | Line 16: | ||
| A5GT | FMCJESDADC1 | {{:resources:tools-software:linux-drivers:platforms:nios2:a5gt_fmcjesdadc1_2015_r1.zip|}} | | | A5GT | FMCJESDADC1 | {{:resources:tools-software:linux-drivers:platforms:nios2:a5gt_fmcjesdadc1_2015_r1.zip|}} | | ||
| A10GX (10AX115S2F45I2SG) | FMCDAQ2 | {{:resources:tools-software:linux-drivers:platforms:a10gx_daq2_2015_r1.zip|}} | | | A10GX (10AX115S2F45I2SG) | FMCDAQ2 | {{:resources:tools-software:linux-drivers:platforms:a10gx_daq2_2015_r1.zip|}} | | ||
+ | |||
+ | {{section>:resources:tools-software:linux-software:adi-kuiper_images:master#master_nios2_images&}} | ||
If you are using a Windows machine and Quartus II is installed, the easiest way of loading the design is to directly run program.bat script (make sure that the Quartus II path specified in the script match the one from your machine). It will program the board and will launch a nios2-terminal where the Linux console messages will be printed. | If you are using a Windows machine and Quartus II is installed, the easiest way of loading the design is to directly run program.bat script (make sure that the Quartus II path specified in the script match the one from your machine). It will program the board and will launch a nios2-terminal where the Linux console messages will be printed. |