Download the pre-built image for you setup:
FPGA Carrier | FMC Card | Download |
---|---|---|
A10GX (10AX115S2F45I1SG) | FMCDAQ2 | daq2_a10gx_2018_r1.zip |
A10GX (10AX115S3F45E2SGE3) | FMCDAQ2 | a10gx_daq2_2016_r1.zip |
A10GX (10AX115S3F45E2SGE3) | FMCDAQ3 | a10gx_daq3_2016_r1.zip |
A5GT | FMCJESDADC1 | a5gt_fmcjesdadc1_2015_r2.zip |
A10GX (10AX115S2F45I2SG) | FMCDAQ2 | a10gx_daq2_2015_r2.zip |
A5GT | FMCJESDADC1 | a5gt_fmcjesdadc1_2015_r1.zip |
A10GX (10AX115S2F45I2SG) | FMCDAQ2 | a10gx_daq2_2015_r1.zip |
If you are using a Windows machine and Quartus II is installed, the easiest way of loading the design is to directly run program.bat script (make sure that the Quartus II path specified in the script match the one from your machine). It will program the board and will launch a nios2-terminal where the Linux console messages will be printed.
An example of Linux console messages that are printed by the target:
Linux version 4.4.0-08393-g0e78611 (dragos@dragos-debian) (gcc version 5.3.0 (So urcery CodeBench Lite 2016.05-10) ) #149 Mon Jun 6 18:30:22 EEST 2016 bootconsole [early0] enabled early_console initialized at 0xf01814f0 On node 0 totalpages: 65536 free_area_init_node: node 0, pgdat c0695f8c, node_mem_map c06b98c0 Normal zone: 512 pages used for memmap Normal zone: 0 pages reserved Normal zone: 65536 pages, LIFO batch:15 pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 pcpu-alloc: [0] 0 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 Kernel command line: debug console=ttyJ0,115200 PID hash table entries: 1024 (order: 0, 4096 bytes) Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Sorting __ex_table... Memory: 252976K/262144K available (2957K kernel code, 93K rwdata, 672K rodata, 3 016K init, 99K bss, 9168K reserved, 0K cma-reserved) NR_IRQS:64 nr_irqs:64 0 clocksource: nios2-clksrc: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns Calibrating delay loop (skipped), value calculated using timer frequency.. 200.0 0 BogoMIPS (lpj=400000) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) devtmpfs: initialized cpu cpu0: Error -2 creating of_node link clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645 041785100000 ns NET: Registered protocol family 16 clocksource: Switched to clocksource nios2-clksrc NET: Registered protocol family 2 TCP established hash table entries: 2048 (order: 1, 8192 bytes) TCP bind hash table entries: 2048 (order: 1, 8192 bytes) TCP: Hash tables configured (established 2048 bind 2048) UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. futex hash table entries: 256 (order: -1, 3072 bytes) jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) 101814f0.serial: ttyJ0 at MMIO 0x101814f0 (irq = 2, base_baud = 0) is a Altera J TAG UART console [ttyJ0] enabled console [ttyJ0] enabled bootconsole [early0] disabled bootconsole [early0] disabled loop: module loaded spi_altera 10181400.spi: base f0181400, irq 74 libphy: altera_tse: probed altera_tse 10181000.ethernet (unnamed net_device) (uninitialized): MDIO bus alte ra_tse-0: created altera_tse 10181000.ethernet: Altera TSE MAC version 15.1 at 0x10181000 irq 3/4 mousedev: PS/2 mouse device common for all mice altera_xcvr 10000000.daq3_axi_jesd_xcvr: Altera XCVR probed iio iio:device0: ad9528 setup ad9528 spi32766.0: probed ad9528-1 ad9144 spi32766.1: Probed. NET: Registered protocol family 17 ad9467 spi32766.2: AD9680 PLL LOCKED cf_axi_dds 10024000.axi-ad9152-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (8.00.b ) at 0x10024000 mapped to 0xf0024000, probed DDS AD9152 cf_axi_adc 10010000.axi-ad9680-hpc: ADI AIM (9.00.b) at 0x10010000 mapped to 0xf 0010000, probed ADC AD9680 as MASTER Freeing unused kernel memory: 3016K (c02e5000 - c05d7000) Starting logging: OK Initializing random number generator... random: dd urandom read with 35 bits of entropy available done. Starting network... altera_tse 10181000.ethernet eth0: device MAC address b2:94:3d:6e:11:8f altera_tse 10181000.ethernet eth0: TSE revision f01 altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 1 ch 0 CDR/CMU PLL & RX offset cal ib OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 1 ch 1 CDR/CMU PLL & RX offset cal ib OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 1 ch 2 CDR/CMU PLL & RX offset cal ib OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 1 ch 3 CDR/CMU PLL & RX offset cal ib OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: RX transceiver ready altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 0 ATX PLL calibration OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 0 ch 0 TX termination and VOD cali b OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 0 ch 1 TX termination and VOD cali b OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 0 ch 2 TX termination and VOD cali b OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: Link 0 ch 3 TX termination and VOD cali b OK altera_xcvr 10000000.daq3_axi_jesd_xcvr: TX transceiver ready altera_tse 10181000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off Network cable is plugged udhcpc (v1.24.2) started Sending discover... Sending select for 10.50.1.132... Lease of 10.50.1.132 obtained, lease time 28800 deleting routers adding dns 10.32.51.110 adding dns 10.64.53.110 inet addr:10.50.1.132 Bcast:10.50.1.255 Mask:255.255.255.0 Starting dropbear sshd: OK Starting IIO Server Daemon Welcome to Buildroot buildroot login:
The IIO Oscilloscope application can be used to remotely connect to another platform that has a connected IIO device in order to configure the device and read data from it.
To install the application, please follow the instructions from here: Oscilloscope
Once the application is launched go to Settings → Connect and enter the IP address of the target in the popup window. Click Refresh and OK.
Note: The IP address of the target can be found by looking to the Linux console messages (Lease of 10.50.1.114 obtained, lease time 28800) or using the Linux ifconfig command (log in using user root and password analog):
Welcome to Buildroot buildroot login: root Password: # ifconfig eth0 Link encap:Ethernet HWaddr B2:94:3D:6E:11:8F inet addr:10.50.1.114 Bcast:10.50.1.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:47 errors:0 dropped:11 overruns:0 frame:0 TX packets:3 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:5386 (5.2 KiB) TX bytes:1026 (1.0 KiB) Memory:10181000-101813ff lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) #
Some examples of the IIO Oscilloscope running on Windows and connected remotely to a target that runs Linux:
We provide a script that does automates the build for Nios 2.
The script takes 4 parameters:
a10gx_adrv9371.dts
The script will:
wget https://raw.githubusercontent.com/analogdevicesinc/wiki-scripts/master/linux/build_nios2_kernel_image.sh && chmod +x build_nios2_kernel_image.sh && ./build_nios2_kernel_image.sh /home/<user>/intelFPGA/<version>/nios2eds/bin/gnu/H-x86_64-pc-linux-gnu/bin/nios2-elf-
user@pc:~/nios2$ git clone https://github.com/analogdevicesinc/linux.git Cloning into 'linux'... remote: Counting objects: 4331580, done. remote: Compressing objects: 100% (23/23), done. remote: Total 4331580 (delta 10), reused 5 (delta 5), pack-reused 4331552 Receiving objects: 100% (4331580/4331580), 1.27 GiB | 1.88 MiB/s, done. Resolving deltas: 100% (3598928/3598928), done. Checking connectivity... done. Checking out files: 100% (49759/49759), done. user@pc:~/nios2$
user@pc:~/nios2$ cd linux/ user@pc:~/nios2/linux$ git checkout altera_4.9 Branch altera_4.9 set up to track remote branch altera_4.9 from origin. Switched to a new branch 'altera_4.9' user@pc:~/nios2/linux$
user@pc:~/nios2/linux$ wget http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/nios2/rootfs_nios2.cpio.gz -P arch/nios2/boot/rootfs.cpio.gz --2015-07-21 09:30:19-- http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/nios2/rootfs_nios2.cpio.gz Resolving wiki.analog.com (wiki.analog.com)... 195.170.124.184 Connecting to wiki.analog.com (wiki.analog.com)|195.170.124.184|:80... connected. HTTP request sent, awaiting response... 200 OK Length: 2786418 (2.7M) [application/octet-stream] Saving to: ‘arch/nios2/boot/rootfs.cpio.gz’ arch/nios2/boot/rootfs.cpi 100%[=========================================>] 2.66M 111KB/s in 20s 2015-07-21 09:30:40 (134 KB/s) - ‘arch/nios2/boot/rootfs.cpio.gz’ saved [2786418/2786418] user@pc:~/nios2/linux$
user@pc:~/nios2/linux$ export ARCH=nios2 user@pc:~/nios2/linux$ export CROSS_COMPILE=~/nios2/tools/bin/nios2-linux-gnu- user@pc:~/nios2/linux$
user@pc:~/nios2/linux$ make adi_nios2_defconfig # # configuration written to .config # user@pc:~/nios2/linux$
your_setup.dts is a generic file name - it should be replaced by the desired devicetree file name.
Valid options: a5gt_fmcjesdadc1.dts , a10gx_daq2.dts , a10gx_daq3.dts
user@pc:~/nios2/linux$ cp arch/nios2/boot/dts/your_setup.dts arch/nios2/boot/devicetree.dts user@pc:~/nios2/linux$
user@pc:~/nios2/linux$ make zImage scripts/kconfig/conf --silentoldconfig Kconfig CHK include/config/kernel.release WRAP arch/nios2/include/generated/asm/atomic.h ....... LD arch/nios2/boot/compressed/vmlinux OBJCOPY arch/nios2/boot/zImage Kernel: arch/nios2/boot/zImage is ready user@pc:~/nios2/linux$
Prebuilt image: a10gx_adrv9371x_dev.zip
HDL Project: a10gx
Linux Kernel: altera_4.6
a10gx_adrv9371.dts: a10gx_adrv9371.dts
rootfs: rootfs_adrv9371x.cpio.gz