Wiki

This version is outdated by a newer approved version.DiffThis version (04 Dec 2015 11:23) was approved by Michael Hennerich.The Previously approved version (01 Apr 2015 12:34) is available.Diff

This is an old revision of the document!


ADF7242 Network MAC802154 Linux Driver

Supported Devices

Evaluation Boards

Description

2.4 GHz Wireless Transceiver PMOD

21 Jan 2015 00:50 · Glaizel Arinuelo

Source Code

Status

Source Mainlined?
git No

This driver is not mainline - it can be found in the IEEE802.15.4/ZigBee Stack for Linux Project.

Files

Function File
driver adf7242.c
include adf7242.h

Firmware for Automatic IEEE 802.15.4 Operating Modes (AN-1082)

Example platform device initialization

For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.

For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.

21 Oct 2010 16:10

Example Platform / Board file

Declaring SPI slave devices

Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.

This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().

For more information see: Documentation/spi/spi-summary.rst

21 Oct 2010 16:10
#include <linux/spi/adf7242.h>
 
static const struct adf7242_platform_data adf7242_pdata = {
 
	.mode = ADF_IEEE802154_AUTO_CSMA_CA | ADF_IEEE802154_HW_AACK,
/*
 * Specifies number of attempts to
 * retransmit unacknowledged
 * frames while in automatic CSMA-CA 
 * Tx mode.
 */
	.max_frame_retries = 4,
/*
 * Specifies number of attempts to
 * repeat CSMA-CA algorithm prior to
 * cancellation of RC_TX command.
 * Valid range is 0 to 5; 
 * 7: CSMA-CA algorithm is off
 */
	.max_cca_retries = 4,
/* 
 * Specifies the maximum back-off
 * exponent used in the CSMA-CA
 * algorithm; valid range is 4 to 8
 * 
 */
	.max_csma_be = 6,
/*
 * Specifies the minimum back-off
 * exponent used in the CSMA-CA
 * algorithm; valid range is 0 to
 * csma_max_be
 */
	.min_csma_be = 1,
};
static struct spi_board_info bfin_spi_board_info[] __initdata = {
#if defined(CONFIG_IEEE802154_ADF7242) || defined(CONFIG_IEEE802154_ADF7242_MODULE)
	{
		.modalias = "adf7242",
		.max_speed_hz = 10000000,     /* max spi clock (SCK) speed in HZ */
		.irq = IRQ_PF6,
		.bus_num = 0,
		.chip_select = 0,	/* GPIO controlled SSEL */
		.controller_data = &adf7242_spi_chip_info, /* Blackfin only */
		.platform_data = &adf7242_pdata,
		.mode = SPI_MODE_0,
	},
#endif
};

Alternatively, it is possible to declare the SPI devices from a DeviceTree file.
Read the documentation for more details.

Example:

adf7242@0 {
	compatible = "adi,adf7242";
	reg = <0>;
	spi-max-frequency = <10000000>;
	interrupts = <0x62 IRQ_TYPE_LEVEL_HIGH>;

	adi,hw-aack-mode-enable;
	adi,auto-csma-ca-mode-enable;
};

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The ADF7242 Driver depends on CONFIG_SPI and CONFIG_IEEE802154

------------------- Linux Kernel Configuration ----------------------

  [*] Networking support  --->
       Networking options  --->
         <*> IEEE Std 802.15.4 Low-Rate Wireless Personal Area Networks support
            <*>   Generic IEEE 802.15.4 Soft Networking Stack (mac802154)

  [*] Device drivers  --->
       [*] Network device support  --->
          --- Network device support
          [*]   Ethernet (10 or 100Mbit)  --->
          <*>   IEEE 802.15.4 drivers  --->
     	      --- IEEE 802.15.4 drivers
               <M>   ADF7242 transceiver driver

Hardware configuration

Interface Connector Signal Description



21 Jan 2015 00:50 · Glaizel Arinuelo

Driver testing

On this demo network, we will have two different boards communicating with each other using ADF7242 modules: a Raspberry Pi and a ZedBoard.

Userspace tools for Linux IEEE 802.15.4 stack

The next steps require the “iz” tool to be installed on your system. On Debian-based systems, it can be installed via the package lowpan-tools.
It can also be compiled from the sources, located at the following address: http://sourceforge.net/apps/trac/linux-zigbee

The minimum supported version is 0.3.1. Be sure to have this version (or newer) installed.

Configuration of the IEEE 802.15.4 layer

We will configure the two devices to use the PAN ID 0x0777, the hardware addresses a0::1 and a0::2, and the short addresses 0x8001 and 0x8002.

Then, we will give them IPv6 addresses and test 6loWPAN communication with standard GNU tools.

Configuration for the first node (ZedBoard)

root:/> HW_ADDR="a0:0:0:0:0:0:0:1"
root:/> DEVICE_ADDR=8001 # hexadecimal
root:/> PAN_ID=777 # hexadecimal
root:/> CHANNEL=11
root:/>
root:/> iz add wpan-phy0
Registered new device ('wpan0') on phy wpan-phy0

root:/> ip link set wpan0 address ${HW_ADDR}
root:/> ifconfig wpan0 up

root:/> iz set wpan0 ${PAN_ID} ${DEVICE_ADDR} ${CHANNEL}

Configuration for the second node (Raspberry Pi)

We only need to change the first two lines:

root:/> HW_ADDR="a0:0:0:0:0:0:0:2"
root:/> DEVICE_ADDR=8002 # hexadecimal
root:/> PAN_ID=777 # hexadecimal
root:/> CHANNEL=11
root:/>
root:/> iz add wpan-phy0
Registered new device ('wpan0') on phy wpan-phy0

root:/> ip link set wpan0 address ${HW_ADDR}
root:/> ifconfig wpan0 up

root:/> iz set wpan0 ${PAN_ID} ${DEVICE_ADDR} ${CHANNEL}

Some GNU/Linux distributions offered on the Raspberry Pi, like Raspbian, will auto-enable the wpan0 interface as soon as it is created. We can disable this behaviour with the following command:

root:/> ifplugd -S -i wpan0 && ifconfig wpan0 down

Chat application

Now that our two devices are correctly configured, we can verify that the two devices can communicate using the “izchat” application:

ZedBoard:

root:/> izchat 0x0777 0x8001 0x8002
Hello World!
>Thanks 

Raspberry Pi:

root:/> izchat 0x0777 0x8002 0x8001
>Hello World!
Thanks

This is a pretty simple two way communication. The ASCII strings are encapsulated in IEEE802.15.4 DATA frames.

Configuration of the 6loWPAN layer

The previous example shows that communication is working, but it is not very useful. By using the 6loWPAN protocol on top (the low-power equivalent of the IPv6 protocol), we can allow standard Linux network applications to communicate over the IEEE 802.15.4 link with standard sockets.

Configuration for the first node (ZedBoard)

root:/> HW_ADDR="a0:0:0:0:0:0:0:1" # Same as before
root:/> IPV6_ADDR="2001::1/128"
root:/>
root:/> ip link add link wpan0 name lowpan0 type lowpan
root:/> ip link set lowpan0 address ${HW_ADDR}
root:/>
root:/> ip addr add ${IPV6_ADDR} dev lowpan0
root:/> ip route add 2001::/64 dev lowpan0

Configuration for the second node (Raspberry Pi)

root:/> HW_ADDR="a0:0:0:0:0:0:0:2" # Same as before
root:/> IPV6_ADDR="2001::2/128"
root:/>
root:/> ip link add link wpan0 name lowpan0 type lowpan
root:/> ip link set lowpan0 address ${HW_ADDR}
root:/>
root:/> ip addr add ${IPV6_ADDR} dev lowpan0
root:/> ip route add 2001::/64 dev lowpan0

Some GNU/Linux distributions offered on the Raspberry Pi, like Raspbian, will auto-enable the lowpan0 interface as soon as it is created. We can disable this behaviour with the following command:

root:/> ifplugd -S -i lowpan0 && ifconfig lowpan0 down

Testing the communication

Ping!

From the Raspberry Pi, we can now ping the ZedBoard at the address fe80::a200:0:0:1%lowpan0:

root:/> ping6 fe80::a200:0:0:1%lowpan0
PING fe80::a200:0:0:1%lowpan0(fe80::a200:0:0:1) 56 data bytes
64 bytes from fe80::a200:0:0:1: icmp_seq=1 ttl=64 time=191 ms
64 bytes from fe80::a200:0:0:1: icmp_seq=2 ttl=64 time=170 ms
64 bytes from fe80::a200:0:0:1: icmp_seq=3 ttl=64 time=87.6 ms
64 bytes from fe80::a200:0:0:1: icmp_seq=4 ttl=64 time=139 ms
64 bytes from fe80::a200:0:0:1: icmp_seq=5 ttl=64 time=173 ms
^C
--- fe80::a200:0:0:1%lowpan0 ping statistics ---
5 packets transmitted, 5 received, 0% packet loss, time 4002ms
rtt min/avg/max/mdev = 87.627/152.533/191.436/36.491 ms
root:/>

We can as well ping the Raspberry Pi from the Zedboard using the address fe80::a200:0:0:2%lowpan0.

Standard tools

The following is just to demonstrate that any Linux program can, using standard sockets, communicate over the IEEE 802.15.4 link with 6loWPAN:

root@raspberrypi:/> ssh -6 analog@fe80::a200:0:0:1%lowpan0
analog@fe80::a200:0:0:1%lowpan0's password: 
Welcome to Linaro 14.04 (GNU/Linux 3.18.0-33199-g62cfd65-dirty armv7l)

Last login: Thu Jan  1 00:02:21 1970 from fe80::a200:0:0:2%lowpan0

root@analog:/>

resources/tools-software/linux-drivers/networking-mac802154/adf7242.1449224606.txt.gz · Last modified: 04 Dec 2015 11:23 by Michael Hennerich