Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (30 Sep 2010 13:04) is a draft.
Approvals: 0/1

This is an old revision of the document!


ADP5520/01 driver

Supported Devices

The driver for the ADP5520 also supports the ADP5501.

Description

The ADP5520/01 driver utilizes several Linux device-driver subsystems and provides various software interfaces. It is therefore implemented as a multifunction device (MFD). In this particular case the ADP5520 backlight driver and I/O expander, concurrently leverages the Linux backlight, LED, GPIO, and input subsystems for its keypad functionality.

Core

The ADP5520/01 core driver in drivers/mfd provides common services for the subsystem drivers. These services include register access, control and shared interrupt management.

The core registers/enumerates platform devices for the various subsystems via the platform device and driver system.

When a platform driver for one of the subsystems is instantiated, the core initializes the chip (which may be specified by the platform data).

The ADP5520/01 platform drivers follow the standard driver model convention, where discovery/enumeration is handled outside the drivers, and drivers provide probe() and remove() methods.

Resources

Each peripheral (subsystem device) has a view of the device which is implicitly narrowed to the specific set of resources that peripheral requires in order to function correctly.

Configuration

The device driver uses a set of platform data to pass configurations through to the core and the subsidiary drivers so that there can be support for multiple ADP5520/01 devices built into a single kernel image.

Software configurable features

Backlight:

  • Ambient Light Sensor Support
  • Configurable Fade On/Off times
  • Configurable Brightness/Intensity in 127 steps

LED:

  • Up to 3 LEDs configurable
  • Configurable Fade On/Off times
  • LED Blink On/Off times
  • Configurable Brightness/Intensity in 64 steps from [0..255]

Keypad:

  • Configurable keypad size matrix (rows, columns) up to 16 keys
  • Enabling and disabling automatic key repeat feature.

GPIO:

  • Configurable number of dedicated GPIOs, up to 8 GPIOs
  • Configurable Pull-Ups

Source Code

Status

Source Mainlined?
svn git Yes

Files

Example platform device initialization

Since Keypad, GPIO and optional LEDs (2, 3) are multiplexed, you need to avoid double configurations. Please refer to the table below.
ADP5520 PIN R3 R2 R1 R0 C0 C1 C2 C3
GPIO GPIO_R3 GPIO_R2 GPIO_R1 GPIO_R0 GPIO_C0 GPIO_C1 GPIO_C2 GPIO_C3
Keypad ROW_R3 ROW_R2 ROW_R1 ROW_R0 COL_C0 COL_C1 COL_C2 COL_C3
LED LED3 LED2
Please refer to include/linux/mfd/adp5520.h for detailed configuration defines.

Backlight

<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_backlight_data{} c linux-kernel>

LED

<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_leds[] c linux-kernel>

<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_leds_data{} c linux-kernel>

GPIO

<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_gpio_data{} c linux-kernel>

Keypad

<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_keymap[] c linux-kernel> <source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_keys_data{} c linux-kernel>

ADP5520/ADP5501 MFD Core Support

<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_pdev_data{} c linux-kernel> <source trunk/arch/blackfin/mach-bf537/boards/stamp.c:/CONFIG_PMIC_ADP5520/2-/#if/ c linux-kernel>

ADP5520 IRQ Usage:
If you aren’t planning to utilize the Keypad interface, you don’t need to specify an IRQ in bfin_i2c_board_info.

Adding Linux driver support

Fist of all you need to enable i2c support followed by the ADP5520 MFD Core Driver. Then you may select individual components like LCD backlight, LEDs, GPIOs and Keypad under the corresponding menus.

ADP5520 MFD Core Support

Device Drivers  ---> 
	<*> I2C support  --->
		<*> Blackfin TWI I2C support
		Or:
		<*> GPIO-based bitbanging I2C


Device Drivers  ---> 
	Multifunction device drivers  --->
		[*] Analog Devices ADP5520/01 MFD PMIC Core Support

Backlight

Device Drivers  ---> 
	Graphics support  --->
		[*] Backlight & LCD device support  --->
			<*>   Lowlevel Backlight controls
			<M>     Backlight Driver for ADP5520/ADP5501 using WLED

LED

Device Drivers  --->
	[*] LED Support  --->
		<*>   LED Class Support
		<M>   LED Support for ADP5520/ADP5501 PMIC

GPIO

Device Drivers  --->
	[*] GPIO Support  --->
		[*]   /sys/class/gpio/... (sysfs interface)
		<M>   GPIO Support for ADP5520 PMIC

Keypad

Device Drivers  --->
	Input device support  --->
		<*> Generic input layer (needed for keyboard, mouse, ...)
		<*>   Event interface
		[*]   Keyboards  --->
			<M>   Keypad Support for ADP5520 PMIC

Hardware configuration

ADP5520 Demo Mother/Daughter Board

There is no dedicated Blackfin STAMP evaluation board for the ADP5520. During test and driver development we used the ADP5520 Demo Mother/Daughter Board. Connect the ADP5520 Demo Mother to an USB port.

It can be easily wired to the Blackfin STAMP TWI/I2C header.

BF537-STAMP (P10) TWI/I2C header ADP5520 Daughter Board
PIN Function PIN/Function
5 SCL SCL
6 SDA SDA
10 GPIO_PG0 nINT
20 GND GND

Driver testing

Backlight

root:/> modprobe adp5520_bl
root:/>

root:/> cd sys/class/backlight/adp5520-backlight/
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> ls -l
-r--r--r--    1 root     root         4096 Nov 12 10:31 actual_brightness
-rw-r--r--    1 root     root         4096 Nov 12 10:31 bl_power
-rw-r--r--    1 root     root         4096 Nov 12 10:31 brightness
-rw-rw-r--    1 root     root         4096 Nov 12 10:31 dark_dim
-rw-rw-r--    1 root     root         4096 Nov 12 10:31 dark_max
-rw-rw-r--    1 root     root         4096 Nov 12 10:31 daylight_dim
-rw-rw-r--    1 root     root         4096 Nov 12 10:31 daylight_max
lrwxrwxrwx    1 root     root            0 Nov 12 10:31 device -> ../../../0-0032
-r--r--r--    1 root     root         4096 Nov 12 10:31 max_brightness
-rw-rw-r--    1 root     root         4096 Nov 12 10:31 office_dim
-rw-rw-r--    1 root     root         4096 Nov 12 10:31 office_max
drwxr-xr-x    2 root     root            0 Nov 12 10:31 power
lrwxrwxrwx    1 root     root            0 Nov 12 10:31 subsystem -> ../../../../../../../../class/backlight

root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> echo 127 > brightness
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> echo 50 > brightness
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> echo 0 > brightness

For more information on Backlight handling in Linux read: Documentation/ABI/stable/sysfs-class-backlight

LED

root:/> modprobe leds-adp5520
Registered led device: adp5520-led1
Registered led device: adp5520-led2
Registered led device: adp5520-led3

root:/> cd sys/class/leds/adp5520-led
sys/class/leds/adp5520-led1/  sys/class/leds/adp5520-led3/
sys/class/leds/adp5520-led2/

root:/> cd sys/class/leds/adp5520-led1
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> ls -l
-rw-r--r--    1 root     root         4096 Nov 12 10:34 brightness
lrwxrwxrwx    1 root     root            0 Nov 12 10:34 device -> ../../../0-0032
drwxr-xr-x    2 root     root            0 Nov 12 10:34 power
lrwxrwxrwx    1 root     root            0 Nov 12 10:34 subsystem -> ../../../../../../../../class/leds
-rw-r--r--    1 root     root         4096 Nov 12 10:34 trigger
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> echo 10 > brightness
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> echo 255 > brightness
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> echo 0 > brightness

root:/> modprobe -r leds-adp5520
root:/>

For more information on LEDs handling in Linux read: Documentation/leds-class.txt

GPIO

root:/> modprobe adp5520-gpio
root:/> cd sys/class/gpio/gpiochip50/
root:/sys/devices/virtual/gpio/gpiochip50> ls -l
-r--r--r--    1 root     root         4096 Nov 12 10:37 base
-r--r--r--    1 root     root         4096 Nov 12 10:37 label
-r--r--r--    1 root     root         4096 Nov 12 10:37 ngpio
drwxr-xr-x    2 root     root            0 Nov 12 10:37 power
lrwxrwxrwx    1 root     root            0 Nov 12 10:37 subsystem -> ../../../../class/gpio
-rw-r--r--    1 root     root         4096 Nov 12 10:37 uevent
root:/sys/devices/virtual/gpio/gpiochip50> cd
root:/>
Note that you will have to enable the event_test utility under “Blackfin test programs” in your user space configuration.
--- Blackfin test programs
                   [*] Input event device test

For more information on GPIO handling in Linux read: Documentation/gpio.txt

Keypad

root:/> modprobe adp5520-keys
input: adp5520-keys as /devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/adp5520-keys.5520/input/input0

root:/> event_test /dev/input/event0
Input driver version is 1.0.0
Input device ID: bus 0x18 vendor 0x1 product 0x5520 version 0x1
Input device name: "adp5520-keys"
Supported events:
  Event type 0 (Reset)
    Event code 0 (Reset)
    Event code 1 (Key)
  Event type 1 (Key)
    Event code 2 (1)
    Event code 3 (2)
    Event code 4 (3)
    Event code 5 (4)
    Event code 6 (5)
    Event code 7 (6)
    Event code 8 (7)
    Event code 9 (8)
    Event code 10 (9)
    Event code 11 (0)
    Event code 12 (Minus)
    Event code 13 (Equal)
    Event code 28 (Enter)
    Event code 41 (Grave)
    Event code 43 (BackSlash)
Testing ... (interrupt to exit)
Event: time 1415788674.340000, type 1 (Key), code 41 (Grave), value 1
Event: time 1415788674.340000, type 0 (Reset), code 0 (Reset), value 0
Event: time 1415788674.516000, type 1 (Key), code 41 (Grave), value 0
Event: time 1415788674.516000, type 0 (Reset), code 0 (Reset), value 0
Event: time 1415788674.912000, type 1 (Key), code 2 (1), value 1
Event: time 1415788674.912000, type 0 (Reset), code 0 (Reset), value 0
Event: time 1415788675.140000, type 1 (Key), code 2 (1), value 0
Event: time 1415788675.140000, type 0 (Reset), code 0 (Reset), value 0
Event: time 1415788675.892000, type 1 (Key), code 6 (5), value 1
Event: time 1415788675.892000, type 0 (Reset), code 0 (Reset), value 0
Event: time 1415788676.092000, type 1 (Key), code 6 (5), value 0
Event: time 1415788676.092000, type 0 (Reset), code 0 (Reset), value 0

root:/> modprobe -r adp5520-keys
root:/>

For more information on Input handling in Linux read: Documentation/input/input.txt

1) , 2)
ADP5520 only
resources/tools-software/linux-drivers/multifunction-device/adp5520.1285844697.txt.gz · Last modified: 30 Sep 2010 13:04 by hennerich