This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:linux-drivers:input-misc:ad714x [11 Feb 2016 21:10] Lars-Peter Clausen [Status] |
resources:tools-software:linux-drivers:input-misc:ad714x [03 Jan 2021 21:43] Robin Getz fix links |
||
---|---|---|---|
Line 19: | Line 19: | ||
Capacitance sensors detect a change in capacitance when something or someone approaches or touches the sensor. The technique has been used in industrial applications for many years to measure liquid levels, humidity, and material composition. A newer application, coming into widespread use, is in human-to-machine interfaces. Mechanical buttons, switches, and jog wheels have long been used as the interface between the user and the machine. Because of their many drawbacks, however, interface designers have been increasingly looking for more reliable solutions. Capacitive sensors can be used in the same manner as buttons, but they also can function with greater versatility, for example, when implementing a 128-position scroll bar. | Capacitance sensors detect a change in capacitance when something or someone approaches or touches the sensor. The technique has been used in industrial applications for many years to measure liquid levels, humidity, and material composition. A newer application, coming into widespread use, is in human-to-machine interfaces. Mechanical buttons, switches, and jog wheels have long been used as the interface between the user and the machine. Because of their many drawbacks, however, interface designers have been increasingly looking for more reliable solutions. Capacitive sensors can be used in the same manner as buttons, but they also can function with greater versatility, for example, when implementing a 128-position scroll bar. | ||
- | For more info on how these types of sensors work, take a peek at the [[http://www.analog.com/library/analogDialogue/archives/40-10/cap_sensors.html|ADI web site]]. | + | For more info on how these types of sensors work, take a peek at the [[adi>library/analogDialogue/archives/40-10/cap_sensors.html|ADI web site]]. |