This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:input-keyboard:adp5588 [05 Sep 2012 14:08] – [Status] Michael Hennerich | resources:tools-software:linux-drivers:input-keyboard:adp5588 [11 Feb 2016 21:09] (current) – [Status] Lars-Peter Clausen | ||
---|---|---|---|
Line 39: | Line 39: | ||
===== Status ===== | ===== Status ===== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
- | | [[git.linux.org> | + | | [[git.linux.org> |
===== Files ===== | ===== Files ===== | ||
Line 81: | Line 81: | ||
e> | e> | ||
The ADP5588 Driver depends on **CONFIG_I2C** | The ADP5588 Driver depends on **CONFIG_I2C** | ||
- | </note> | + | </WRAP> |
< | < | ||
Line 114: | Line 114: | ||
</ | </ | ||
- | <note tip> | + | <WRAP tip> |
Make sure the I2C SCL Clock is in the range of 60-400 kHz! | Make sure the I2C SCL Clock is in the range of 60-400 kHz! | ||
- | </note> | + | </WRAP> |
====== Hardware configuration ====== | ====== Hardware configuration ====== | ||
Line 135: | Line 135: | ||
| 20 | GND | GND | | | 20 | GND | GND | | ||
- | <note tip> | + | <WRAP tip> |
On the ADP5588 Demo Mother Board replace R30 (10kOhm PULL-UP resistor on /INTB strobe) with a 1-3kOhm resistor. | On the ADP5588 Demo Mother Board replace R30 (10kOhm PULL-UP resistor on /INTB strobe) with a 1-3kOhm resistor. | ||
The 10kOhm resistor is too weak - Blackfin might see an additional falling edge interrupt on the rising edge of / | The 10kOhm resistor is too weak - Blackfin might see an additional falling edge interrupt on the rising edge of / | ||
- | </note> | + | </WRAP> |
====== Driver testing ====== | ====== Driver testing ====== |