This is an old revision of the document!
The ADRV9002 is a highly integrated, RF transceiver offering dual channel transmitters and dual channel receivers, integrated synthesizers, and digital signal processing functions. The IC delivers a versatile combination of high performance and low power consumption required by battery powered radio equipment and can operate in both FDD and TDD modes. The ADRV9002 operates from 30 MHz to 6000 MHz covering the VHF, licensed and unlicensed cellular bands, and ISM bands. The IC is capable of supporting both narrowband and wideband standards up to 40 MHz bandwidth on both receive and transmit. The transceiver consists of direct conversion signal paths with state-of-the-art noise figure and linearity. Each complete receiver and transmitter sub-system includes DC offset correction, quadrature error correction, and programmable digital filters, eliminating the need for these functions in the digital baseband. In addition, several auxiliary functions such as an auxiliary ADC, auxiliary DACs, and GPIOs are integrated to provide additional monitoring and control capability.
This is a Linux industrial I/O (IIO) subsystem driver, targeting RF Transceivers. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/adc/navassa/adrv9002.c |
driver | drivers/iio/adc/navassa/adrv9002_conv.c |
driver | drivers/iio/adc/navassa/adrv9002_debugfs.c |
include | drivers/iio/adc/navassa/adrv9002.h |
Navassa API driver | drivers/iio/adc/navassa/devices/adrv9001/ |
Navassa API driver | drivers/iio/adc/navassa/third_party |
Navassa API driver | drivers/iio/adc/navassa/common |
Navassa API driver | drivers/iio/adc/navassa/platforms |
Function | File |
---|---|
driver | drivers/iio/adc/cf_axi_adc_core.c |
include | drivers/iio/adc/cf_axi_adc.h |
driver | drivers/iio/adc/ad_adc.c |
Function | File |
---|---|
driver | drivers/iio/frequency/cf_axi_dds.c |
include | drivers/iio/frequency/cf_axi_dds.h |
Please follow the link here for detailed options and examples:
What is a stream processor and what is the purpose of that?
The stream processor is a processor within the device tasked with performing a series of configuration tasks upon an external request. Upon a request from the user, the stream processor performs a series of defined actions defined in the image loaded into the stream during device initialization. The stream processor therefore has “streams” (series of tasks) for:
The stream is not limited to path enabling events and can also react to other events such as a GPIO input signal. The stream processor image needs to be changed with every different configuration. It is recommended to use TES GUI and generate stream file for required configuration.
This was added to make sure the signal path is not disrupted when ARM crashes and still the link is available with reduced performance as tracking calibrations are not running.
The stream binary NavassaStream.bin
must be stored in the /lib/firmware folder, or compiled into the kernel using the CONFIG_FIRMWARE_IN_KERNEL, CONFIG_EXTRA_FIRMWARE config options. Multiple stream binaries can be added. However a unique name must be given.
Function | File |
---|---|
Stream | firmware/Navassa_Stream.bin |
For early versions of TES (before v0.14) streams were only made available in text form. However, the driver requires binary streams. To create the necessary binary stream, (1) generated the C Sample Code from TES and (2) pass the initialize.c file produced to this python helper script. This python script will extract the stream array and convert it to a binary file for the driver to consume.
The device incorporates an ARM processor that needs to be loaded with firmware during boot/setup phase. The processor is responsible, for example, to run the initial and the on the fly calibrations. The ARM binary is also loaded using the kernel firmware framework. Hence, the firmware image needs to be placed in the /lib/firmware folder or compiled into the kernel using the CONFIG_FIRMWARE_IN_KERNEL, CONFIG_EXTRA_FIRMWARE config options. The driver expects the file to have the following name:
Function | File |
---|---|
ARM firmware | firmware/Navassa_EvaluationFw.bin |
The Gain tables for the RX, ORX and TX paths must also be loaded durint boot/setup phase. They are also loaded using the firmware framework.
Function | File |
---|---|
RX Gain Correction table | firmware/RxGainTable.csv |
RX Gain Compensated table | firmware/RxGainTable_GainCompensated.csv |
ORX Gain table | firmware/ORxGainTable.csv |
TX Gain table | firmware/TxAttenTable.csv |
The ADRV9002 driver is a spi-bus driver and can currently only be instantiated via device tree.
Required devicetree properties:
Function | File |
---|---|
ADRV9002 Device Tree | zynqmp-zcu102-rev10-adrv9002.dts |
zynq-zed-adv7511-adrv9002.dts | |
zynq-zc706-adv7511-adrv9002.dts | |
ADRV9002 Device Tree MIMO | zynqmp-zcu102-rev10-adrv9002-rx2tx2.dts |
zynq-zed-adv7511-adrv9002-rx2tx2.dts | |
zynq-zc706-adv7511-adrv9002-rx2tx2.dts | |
socfpga_arria10_socdk_adrv9002_rx2tx2.dts |
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The ADRV9002 driver depends on CONFIG_SPI
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Analog to digital converters *** [--snip--] -*- Analog Devices High-Speed AXI ADC driver core < > Analog Devices AD9361, AD9364 RF Agile Transceiver driver < > Analog Devices AD9371 RF Transceiver driver <*> Analog Devices ADRV9001/ADRV9002 RF Transceiver driver < > Analog Devices AD6676 Wideband IF Receiver driver < > Analog Devices AD9467, AD9680, etc. high speed ADCs < > Analog Devices Motor Control (AD-FMCMOTCON) drivers [--snip--] Frequency Synthesizers DDS/PLL ---> Direct Digital Synthesis ---> <*> Analog Devices CoreFPGA AXI DDS driver
Depending on the devicetree compatible string used, the driver will behave differently in some aspects. There are two main modes of operaton:
compatible | Mode |
---|---|
adi,adrv9002-rx2tx2 | MIMO |
adi,adrv9002 | Independent |
In “MIMO” mode, only one DMA buffer is used and both RX1/RX2 physical ports are mapped into the RX1 channel in the hdl axi core. The same happens for TX. For the hdl core is as TX2/RX2 don't exist. As the name implies, this is useful for use cases as MIMO/Diversity. Naturally, in this case, both RX1/RX2 must have the same baseband sample rate.
In the Independent mode both channels are treated separately by the hdl core, each one with it's own DMA buffer. Useful for TDD applications for example.
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
TIP: An example program which uses the interface can be found here:
General attribute naming convention:
IIO sysfs attribute naming prefix | Target |
---|---|
Transceiver | |
in_temp0_input | Device Temperature |
in_voltage0_[…] | RX1 |
in_voltage1_[…] | RX2 |
out_voltage0_[…] | TX1 |
out_voltage1_[…] | TX2 |
out_altvoltage0_[…] | RX1 LO |
out_altvoltage1_[…] | RX2 LO |
out_altvoltage2_[…] | TX1 LO |
out_altvoltage3_[…] | TX2 LO |
This specifies any shell prompt running on the target
cd /sys/bus/iio/devices/ root@analog:/sys/bus/iio/devices# ls iio:device0 iio:device1 iio:device2 iio:device3 iio_sysfs_trigger root@analog:/sys/bus/iio/devices# cd iio:device1 root@analog:/sys/bus/iio/devices/iio:device1# ls -la total 0 drwxr-xr-x 3 root root 0 Jun 9 09:06 . drwxr-xr-x 5 root root 0 Jun 9 09:06 .. -rw-rw-rw- 1 root root 4096 Jun 9 09:04 dev -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_temp0_input -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_agc_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_bbdc_rejection_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_decimated_power -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_digital_gain_control_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_digital_gain_control_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_dynamic_adc_switch_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_ensm_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_ensm_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_gain_control_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_gain_control_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_hardwaregain -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_hd_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_interface_gain -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_interface_gain_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_nco_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_port_en_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_port_en_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_quadrature_fic_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_quadrature_w_poly_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_rf_bandwidth -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_rfdc_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_rssi -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_rssi_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage0_sampling_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_agc_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_bbdc_rejection_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_decimated_power -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_digital_gain_control_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_digital_gain_control_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_dynamic_adc_switch_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_ensm_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_ensm_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_gain_control_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_gain_control_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_hardwaregain -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_hd_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_interface_gain -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_interface_gain_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_nco_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_port_en_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_port_en_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_quadrature_fic_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_quadrature_w_poly_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_rf_bandwidth -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_rfdc_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_rssi -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_rssi_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 in_voltage1_sampling_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 name lrwxrwxrwx 1 root root 0 Jun 9 09:06 of_node -> ../../../../../../../../firmware/devicetree/base/amba/spi@ff040000/adrv9002-phy@0 -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_altvoltage0_RX1_LO_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_altvoltage1_RX2_LO_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_altvoltage2_TX1_LO_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_altvoltage3_TX2_LO_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_atten_control_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_atten_control_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_close_loop_gain_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_ensm_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_ensm_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_hardwaregain -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_lo_leakage_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_loopback_delay_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_pa_correction_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_port_en_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_port_en_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_quadrature_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_rf_bandwidth -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage0_sampling_frequency -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_atten_control_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_atten_control_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_close_loop_gain_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_ensm_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_ensm_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_hardwaregain -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_lo_leakage_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_loopback_delay_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_pa_correction_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_port_en_mode -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_port_en_mode_available -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_quadrature_tracking_en -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_rf_bandwidth -rw-rw-rw- 1 root root 4096 Jun 9 09:04 out_voltage1_sampling_frequency drwxrwxrwx 2 root root 0 Jun 9 09:04 power -rw-rw-rw- 1 root root 73728 Jun 9 09:04 profile_config lrwxrwxrwx 1 root root 0 Jun 9 09:06 subsystem -> ../../../../../../../../bus/iio -rw-rw-rw- 1 root root 4096 Jun 9 09:04 uevent
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat name adrv9002-phy
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_temp0_input 58000
For use cases where pin control mode is not used or required, these attributes can be used to enable/disable the Rx/Tx signal paths while in the ENSM radio_on state.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_en 1 root@analog:/sys/bus/iio/devices/iio:device1# echo 0 > in_voltage0_en root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_en 0
The ADRV9002 transceiver includes an Enable State Machine (ENSM), allowing real time control over the current state of the device. The ENSM has two possible control methods – SPI control (writing ensm_mode), and pin control. For pin control the below attributes can be inspected:
There are a pair of these attributes for all RX/TX channels.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_port_en_mode_available spi pin root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_port_en_mode spi root@analog:/sys/bus/iio/devices/iio:device1# echo pin > in_voltage0_port_en_mode root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_port_en_mode pin
For controlling the ENSM attribute there are also a pair of attributes for all the RX/TX channels:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_ensm_mode_available calibrated primed rf_enabled root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_ensm_mode calibrated root@analog:/sys/bus/iio/devices/iio:device1# echo rf_enabled > in_voltage0_ensm_mod root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_ensm_mode rf_enabled
port_en_mode
is set to spi
The device contains two RF PLLs. Each RF PLL uses the PLL block common to all synthesizers in the device and employ a 4 core VCO block which provides a 6dB phase noise improvement over the single core VCO. The tuneable range of the RF LO is 30-6000 MHz.It is possible to set the LO frequency independently for each port.
Attribute | Port |
---|---|
out_altvoltage0_RX1_LO_frequency | RX1 |
out_altvoltage1_RX2_LO_frequency | RX2 |
out_altvoltage2_TX1_LO_frequency | TX1 |
out_altvoltage3_TX2_LO_frequency | TX2 |
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat out_altvoltage2_TX1_LO_frequency 2700000000 root@analog:/sys/bus/iio/devices/iio:device1# echo 2400000000 > out_altvoltage2_TX1_LO_frequency root@analog:/sys/bus/iio/devices/iio:device1# cat out_altvoltage2_TX1_LO_frequency 2400000000
ADRV9002 uses profiles to designate different device configuration settings for the Tx/Rx channels. The profile dictates how the digital filters, analog filters, clock rates, and clock dividers are configured in the device. Some specific parameters set by profiles include the IQ data rate, ADC clock rate, analog filter corners, FIR filter coefficients, and interpolation/decimation factors in the half-band filters.
Several profiles can be examined in the ADRV9002 Transceiver Evaluation Software for given device clock frequencies. If the desired profile exists in the software, it is recommended to set up the desired profile in and use the generated JSON file by pressing the Generate Profile File
button. Custom profiles can be generated using other ADI software tools not described here MATLAB Profile/Filter Generator for ADRV9002.
There are some constraints with the loaded profiles due to the architecture of the reference design:
For each profile generated, there must be a correspondent stream binary that also must be loaded. To load a stream:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat stream.bin > stream_config root@analog:/sys/bus/iio/devices/iio:device1#
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat LTE_2_4G_40BW_61MSPS.json > profile_config root@analog:/sys/bus/iio/devices/iio:device1#
The ADRV9002 offers dual receive channels. With a minimum number of external components, each receive channel could build a complete RF-to-bits signal chain which serves as RF front end for a wide range of applications. It supports both time division duplexing (TDD) and frequency division duplexing (FDD) modes and reception of both narrowband (NB) and wideband (WB) signals up to 40MHz. Each receive path RX1 or RX2 contains 2 major subsystems, the Analog Front End (AFE) and a Digital Front End (DFE). The AFE contains the programmable attenuator, matched I and Q mixer, Low pass filter and ADC. The device provides 2 pairs of ADCs, a pair of high performance ADC's for high dynamic range and a pair of low performance ADC's for lower power consumption. The DFE subsystem contains a series of digital signal processing components such as sample rate decimation (DEC), dc offset correction (DC), quadrature error correction (QEC), digital down conversion (DDC) with numerically controlled oscillator (NCO), a programmable 128-tap FIR filter (PFIR), receiver signal strength indicator (RSSI), frequency offset correction, phase offset correction and overload detectors.
To query the RX Sample Rate and Primary Signal Bandwidth:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_sampling_frequency 15360000 root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_rf_bandwidth 10000000
The ADRV9002 receivers (Rx1/Rx2) feature automatic and manual gain control modes for flexible gain control in a wide array of applications. Automatic Gain Control (AGC) allows for receivers to autonomously adjust the receiver gain depending on variations of the input signal. It controls the gain of the device based on the information from a number of signal detectors named peak detector and power detector. The use can also control the gain using API functions through SPI communications or using external PINs to increment/decrement the gain.
Gain Control Modes
Mode | Description |
---|---|
spi | Provides the user full control over the current gain index. Gain controlled through sysfs file |
automatic | The AGC will determine when gain changes should be made. To setup the AGC block there are a vast number of properties the user can configure. This is done through devicetree. More info at ADRV9001/ADRV9002 Device Driver Customization |
pin | The gain is controlled trough external pins. The user can also select which pins to use through devicetree. More in ADRV9001/ADRV9002 Device Driver Customization |
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_gain_control_mode_available spi pin automatic root@analog:/sys/bus/iio/devices/iio:device1# echo pin > in_voltage0_gain_control_mode root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_gain_control_mode pin
Manually control the Gain
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_hardwaregain 36.000000 dB root@analog:/sys/bus/iio/devices/iio:device1# echo 25 > in_voltage0_hardwaregain root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_hardwaregain 25.000000 dB
The digital gain control has two major purposes, one for gain correction which is to correct the small step size inaccuracy in analog front-end attenuation and the other for gain compensation which is to compensate for the entire analog front-end attenuation. The digital gain block is controlled by the Rx gain table. Different digital gain will be applied when configured in gain correction or gain compensation mode. The Rx gain table has a unique front-end attenuator setting, with a corresponding amount of digital gain, programmed at each index of the table. In the end of the Rx data path, the interface gain could be further applied by using a “Slicer” block for 2 major purposes. One is to avoid digital saturation in gain compensation mode. The other one is to ensure the overall SNR is limited only by analog noise and unaffected by quantization noise.
Gain Control Modes
Mode | Description |
Gain_Correction_manual_control | The digital gain block is used. It applies a small amount of digital gain/attenuation to provide consistent gain steps in a gain table. |
Gain_Compensation_manual_control | In this mode gain compensation is used and the interface gain is determined manually by the user. |
Gain_Correction_automatic_control | Similar to 1 except that the device controls the interface gain automatically. |
Gain_Compensation_automatic_control | Similar to 2 except that the device controls the interface gain automatically |
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_digital_gain_control_mode Gain_Correction_manual_control root@analog:/sys/bus/iio/devices/iio:device1# echo Gain_Compensation_manual_control > in_voltage0_digital_gain_control_mode root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_digital_gain_control_mode Gain_Compensation_manual_control
Manually change the Interface Gain
The available values can be seen with:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_interface_gain_available 18dB 12dB 6dB 0dB -6dB -12dB -18dB -24dB -30dB -36dB
Ranges for setting the Slicer gain are:
[0dB 18dB] | NB and Correction table |
[0dB 0dB] | WB and Correction table |
[-36dB 18dB] | NB and Compensation table |
[-36dB 0dB] | WB and Compensation table |
Setting the value:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_interface_gain 0dB root@analog:/sys/bus/iio/devices/iio:device1# echo -6dB > in_voltage0_interface_gain root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_interface_gain -6dB
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_decimated_power 60.750 dB
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_rssi 65.535 dB
In the Rx data chain, a frequency offset correction block is provided as an option to further correct small carrier frequency offset in both NB and WB modes.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_nco_frequency 0 root@analog:/sys/bus/iio/devices/iio:device1# echo 1200 > in_voltage0_nco_frequency root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_nco_frequency 1200
The main difference between this setting and the bbdc tracking calibration is that disabling this setting will completely disable the bbdc algorithm and set the correction value to 0. Disabling the tracking calibration, just disables the algorithm but the last used correction value is still applied.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_bbdc_rejection_en 1 root@analog:/sys/bus/iio/devices/iio:device1# echo 0 > in_voltage0_bbdc_rejection_en root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_bbdc_rejection_en 0
The device provides 2 pairs of ADCs, a pair of high performance ADC's for high dynamic range and a pair of low performance ADC's for lower power consumption. This setting enables the dynamic switch between this ADC's.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_dynamic_adc_switch_en 0 root@analog:/sys/bus/iio/devices/iio:device1# echo 1 > in_voltage0_dynamic_adc_switch_en root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_dynamic_adc_switch_en 1
The ADRV9001 device integrates dual direct-conversion (Zero-IF) transmitters. It supports both time division duplexing (TDD) and frequency division duplexing (FDD) modes and is capable of transmitting both narrowband (NB) and wideband (WB) signal. Each transmitter consists of an independent I and Q signal path with separate digital filters, DACs, analog Tx low pass filters (LPF) and upconversion mixers. After mixers, an analog attenuator is employed to control the Tx output signal power. There are several signal conditioning functions, such as TX gain control, PA protection, PA digital pre-distortion (DPD), Tx quadrature error correction (QEC) and Tx LO leakage handling, before the data is passed on to the DACs.
To query the RX Sample Rate and Primary Signal Bandwidth:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_sampling_frequency 15360000 root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_rf_bandwidth 10000000
The Tx attenuation block controls the Tx output power. A Tx gain table with 840 entries is loaded into the ADRV9002’s memory during initialization. Each entry equals a 0.05dB gain step giving a range of 42dB.
Gain Control Modes
Mode | Description |
---|---|
spi | Provides the user full control over the current gain index. Gain controlled through sysfs file |
bypass | In this mode, the Tx attenuation functionality is not used which means 0dB total Tx attenuation |
pin | The gain is controlled trough external pins. The user can also select which pins to use through devicetree. More in ADRV9001/ADRV9002 Device Driver Customization |
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_atten_control_mode_available bypass spi pin root@analog:/sys/bus/iio/devices/iio:device1# echo bypass > out_voltage0_atten_control_mode root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_atten_control_mode bypass
Manually control the Gain
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_hardwaregain 0.000000 dB root@analog:/sys/bus/iio/devices/iio:device1# echo -10 > out_voltage0_hardwaregain root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_hardwaregain -10.000000 dB
As for the RX signal chain, it is also possible to apply a nco correction frequency on TX.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_nco_frequency 0 root@analog:/sys/bus/iio/devices/iio:device1# echo 1200 > out_voltage0_nco_frequency root@analog:/sys/bus/iio/devices/iio:device1# cat out_voltage0_nco_frequency 1200
In ADRV9002, to achieve optimal performance, an internal microcontroller performs calibrations which can be classified into two categories: initial calibrations performed at the initialization time before the device is operational; and tracking calibrations performed regularly while the device is operational. The following attributes control on the fly tracking calibrations.
Attribute | Data Path |
in_voltage[01]_agc_tracking_en | RX1/RX2 |
in_voltage[01]_bbdc_rejection_tracking_en | RX1/RX2 |
in_voltage[01]_hd_tracking_en | RX1/RX2 |
in_voltage[01]_quadrature_fic_tracking_en | RX1/RX2 |
in_voltage[01]_quadrature_w_poly_tracking_en | RX1/RX2 |
in_voltage[01]_rfdc_tracking_en | RX1/RX2 |
in_voltage[01]_rssi_tracking_en | RX1/RX2 |
out_voltage[01]_close_loop_gain_tracking_en | TX1/TX2 |
out_voltage[01]_lo_leakage_tracking_en | TX1/TX2 |
out_voltage[01]_loopback_delay_tracking_en | TX1/TX2 |
out_voltage[01]_pa_correction_tracking_en | TX1/TX2 |
out_voltage[01]_quadrature_tracking_en | TX1/TX2 |
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_agc_tracking_en 1 root@analog:/sys/bus/iio/devices/iio:device1# echo 0 > in_voltage0_agc_tracking_en root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage0_agc_tracking_en 0
The ADRV9002 driver supports advanced debug controls via the kernel debugfs. These controls are mostly to debug which settings are currently configured in the device. How these device files/controls can be used is described here.
There's a large number of options available. Through these controls, the user can debug if the device is properly configured with the wanted options or to test/tweak some features at runtime and then add them to the devicetree (if applicable). In order to identify if the IIO device in question (adrv9002-phy) you first need to identify the IIO device number. Therefore read the name attribute of each IIO device
This specifies any shell prompt running on the target
root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name /sys/bus/iio/devices/iio:device0/name:ams /sys/bus/iio/devices/iio:device1/name:adrv9002-phy /sys/bus/iio/devices/iio:device2/name:axi-adrv9002-rx-lpc /sys/bus/iio/devices/iio:device3/name:axi-adrv9002-tx-lpc root@analog:~#
Change directory to /sys/kernel/debug/iio/ iio:deviceX.
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# ls -la total 0 drwxr-xr-x 2 root root 0 Jan 1 1970 . drwxr-xr-x 5 root root 0 Jan 1 1970 .. -rw-r--r-- 1 root root 0 Jan 1 1970 direct_reg_access -rw------- 1 root root 0 Jan 1 1970 initialize -r-------- 1 root root 0 Jan 1 1970 pll_status -r-------- 1 root root 0 Jan 1 1970 rx0_adc_type -r-------- 1 root root 0 Jan 1 1970 rx0_agc_config -r-------- 1 root root 0 Jan 1 1970 rx0_gain_control_pin_mode -r-------- 1 root root 0 Jan 1 1970 rx1_adc_type -r-------- 1 root root 0 Jan 1 1970 rx1_agc_config -r-------- 1 root root 0 Jan 1 1970 rx1_gain_control_pin_mode -r-------- 1 root root 0 Jan 1 1970 tx0_attenuation_pin_control -r-------- 1 root root 0 Jan 1 1970 tx0_dac_boost_en -rw------- 1 root root 0 Jan 1 1970 tx0_nco_frequency_hz -r-------- 1 root root 0 Jan 1 1970 tx1_attenuation_pin_control -r-------- 1 root root 0 Jan 1 1970 tx1_dac_boost_en -rw------- 1 root root 0 Jan 1 1970 tx1_nco_frequency_hz
All the options available to tweak the automatic gain control are exposed through debugfs files for each RX.
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# ls | grep rx0_agc rx0_agc_agcMode rx0_agc_attackDelay_us rx0_agc_changeGainIfThreshHigh rx0_agc_config rx0_agc_enableFastRecoveryLoop rx0_agc_enableSyncPulseForGainCounter rx0_agc_gainUpdateCounter rx0_agc_lowThreshPreventGainInc rx0_agc_maxGainIndex rx0_agc_minGainIndex rx0_agc_peak.agcUnderRangeHighInterval rx0_agc_peak.agcUnderRangeLowInterval rx0_agc_peak.agcUnderRangeMidInterval rx0_agc_peak.apdGainStepAttack rx0_agc_peak.apdGainStepRecovery rx0_agc_peak.apdHighThresh rx0_agc_peak.apdLowThresh rx0_agc_peak.apdLowerThreshPeakExceededCount rx0_agc_peak.apdUpperThreshPeakExceededCount rx0_agc_peak.enableHbOverload rx0_agc_peak.feedback_high_threshold_counter_exceeded rx0_agc_peak.feedback_low_threshold_counter_exceeded rx0_agc_peak.hbGainStepHighRecovery rx0_agc_peak.hbGainStepLowRecovery rx0_agc_peak.hbGainStepMidRecovery rx0_agc_peak.hbHighThresh rx0_agc_peak.hbOverloadDurationCount rx0_agc_peak.hbOverloadPowerMode rx0_agc_peak.hbOverloadThreshCount rx0_agc_peak.hbUnderRangeHighThresh rx0_agc_peak.hbUnderRangeHighThreshExceededCount rx0_agc_peak.hbUnderRangeLowThresh rx0_agc_peak.hbUnderRangeLowThreshExceededCount rx0_agc_peak.hbUnderRangeMidThresh rx0_agc_peak.hbUnderRangeMidThreshExceededCount rx0_agc_peak.hbUpperThreshPeakExceededCount rx0_agc_peakWaitTime rx0_agc_power.feedback_high_threshold_exceeded rx0_agc_power.feedback_lowThreshold_gainChange rx0_agc_power.overRangeHighPowerGainStepAttack rx0_agc_power.overRangeHighPowerThresh rx0_agc_power.overRangeLowPowerGainStepAttack rx0_agc_power.overRangeLowPowerThresh rx0_agc_power.powerEnableMeasurement rx0_agc_power.powerMeasurementDelay rx0_agc_power.powerMeasurementDuration rx0_agc_power.rxTddPowerMeasDelay rx0_agc_power.rxTddPowerMeasDuration rx0_agc_power.underRangeHighPowerGainStepRecovery rx0_agc_power.underRangeHighPowerThresh rx0_agc_power.underRangeLowPowerGainStepRecovery rx0_agc_power.underRangeLowPowerThresh rx0_agc_resetOnRxon rx0_agc_resetOnRxonGainIndex rx0_agc_slowLoopSettlingDelay
The user can read/write on these files before committing the changes. For the changes to be applied, the user must do:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 1 > rx0_agc_config
The configurations can be read afterwards by reading the file:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# cat rx0_agc_config peakWaitTime: 4 maxGainIndex: 255 minGainIndex: 183 gainUpdateCounter: 11520 attackDelay_us: 10 slowLoopSettlingDelay: 16 lowThreshPreventGainInc: 0 changeGainIfThreshHigh: 3 agcMode: 0 resetOnRxon: 0 resetOnRxonGainIndex: 255 enableSyncPulseForGainCounter: 0 enableFastRecoveryLoop: 0 power.powerEnableMeasurement: 1 power.underRangeHighPowerThresh: 10 power.underRangeLowPowerThresh: 4 power.underRangeHighPowerGainStepRecovery: 2 power.underRangeLowPowerGainStepRecovery: 4 power.powerMeasurementDuration: 10 power.powerMeasurementDelay: 2 power.rxTddPowerMeasDuration: 0 power.rxTddPowerMeasDelay: 0 power.overRangeHighPowerThresh: 0 power.overRangeLowPowerThresh: 7 power.overRangeHighPowerGainStepAttack: 4 power.overRangeLowPowerGainStepAttack: 4 power.feedback_lowThreshold_gainChange: 0 power.feedback_high_threshold_exceeded: 0 peak.agcUnderRangeLowInterval: 50 peak.agcUnderRangeMidInterval: 2 peak.agcUnderRangeHighInterval: 4 peak.apdHighThresh: 26 peak.apdLowThresh: 18 peak.apdUpperThreshPeakExceededCount: 6 peak.apdLowerThreshPeakExceededCount: 3 peak.apdGainStepAttack: 4 peak.apdGainStepRecovery: 0 peak.enableHbOverload: 1 peak.hbOverloadDurationCount: 1 peak.hbOverloadThreshCount: 1 peak.hbHighThresh: 16383 peak.hbUnderRangeLowThresh: 5826 peak.hbUnderRangeMidThresh: 8230 peak.hbUnderRangeHighThresh: 11626 peak.hbUpperThreshPeakExceededCount: 6 peak.hbUnderRangeHighThreshExceededCount: 3 peak.hbGainStepHighRecovery: 4 peak.hbGainStepLowRecovery: 6 peak.hbGainStepMidRecovery: 4 peak.hbGainStepMidRecovery: 4 peak.hbOverloadPowerMode: 0 peak.hbUnderRangeMidThreshExceededCount: 3 peak.hbUnderRangeLowThreshExceededCount: 3 peak.feedback_low_threshold_counter_exceeded: 0 peak.feedback_high_threshold_counter_exceeded: 0
The data mode available can be different depending on whether CMOS or LVDS is being used. To check the available modes:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# cat rx_ssi_test_mode_data_available TESTMODE_DATA_NORMAL TESTMODE_DATA_FIXED_PATTERN TESTMODE_DATA_RAMP_16_BIT TESTMODE_DATA_PRBS15 TESTMODE_DATA_PRBS7
We then, set the desired mode:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo TESTMODE_DATA_PRBS15 > rx0_ssi_test_mode_data root@analog:/sys/kernel/debug/iio/iio:device1#
To start the test:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 1 > rx0_ssi_test_mode_configure root@analog:/sys/kernel/debug/iio/iio:device1#
The available configurations for the SSI delays are:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# ls | egrep [rt]x*.*_delay rx0_ssi_clk_delay rx0_ssi_i_data_delay rx0_ssi_q_data_delay rx0_ssi_strobe_delay rx1_ssi_clk_delay rx1_ssi_i_data_delay rx1_ssi_q_data_delay rx1_ssi_strobe_delay tx0_ssi_clk_delay tx0_ssi_i_data_delay tx0_ssi_q_data_delay tx0_ssi_refclk_delay tx0_ssi_strobe_delay_delay tx1_ssi_clk_delay tx1_ssi_i_data_delay tx1_ssi_q_data_delay tx1_ssi_refclk_delay tx1_ssi_strobe_delay_dela
After doing the wanted changes to the previous files, we apply them by:
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 1 > ssi_delays root@analog:/sys/kernel/debug/iio/iio:device1#
This specifies any shell prompt running on the target
echo 1 > initialize
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# cat rx0_gain_control_pin_mode min_gain_index: 183 max_gain_index: 255 increment_step_size: 1 decrement_step_size: 1 increment_pin: dgpio2 decrement_pin: dgpio1
Some IIO drivers feature an optional debug facility, allowing users to read or write registers directly. Special care needs to be taken when using this feature, since you can modify registers on the back of the driver.
Accessing debugfs requires root privileges.
In order to identify if the IIO device in question feature this option you first need to identify the IIO device number.
Therefore read the name attribute of each IIO device
This specifies any shell prompt running on the target
root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name /sys/bus/iio/devices/iio:device0/name:ad7291 /sys/bus/iio/devices/iio:device1/name:ad9361-phy /sys/bus/iio/devices/iio:device2/name:xadc /sys/bus/iio/devices/iio:device3/name:adf4351-udc-rx-pmod /sys/bus/iio/devices/iio:device4/name:adf4351-udc-tx-pmod /sys/bus/iio/devices/iio:device5/name:cf-ad9361-dds-core-lpc /sys/bus/iio/devices/iio:device6/name:cf-ad9361-lpc root@analog:~#
Change directory to /sys/kernel/debug/iio/ iio:deviceX and check if the direct_reg_access file exists.
This specifies any shell prompt running on the target
root@analog:~# cd /sys/kernel/debug/iio/iio\:device1 root@analog:/sys/kernel/debug/iio/iio:device1# ls direct_reg_access direct_reg_access
Reading
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 0x40
Writing
Write ADDRESS VALUE
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 0x50 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 0x50
Accessing HDL CORE registers
Special ADI device driver convention for devices that have both:
In this case when accessing the HDL Core Registers always set BIT31.
The register map for typical ADI HDL cores can be found here: Register Map
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device6# echo 0x80000000 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device6# cat direct_reg_access 0x80062