Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:tools-software:linux-drivers:iio-transceiver:adrv9002 [17 Jul 2020 15:39] – Nuno Sá | resources:tools-software:linux-drivers:iio-transceiver:adrv9002 [17 Jul 2020 15:41] – Nuno Sá |
---|
| |
^ compatible ^ Mode ^ Devicetree ^ | ^ compatible ^ Mode ^ Devicetree ^ |
|adi,adrv9002-rx2tx2|MIMO mode|[[linux.github>adrv9001?arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-adrv9002-rx2tx2.dts| zynqmp-zcu102-rev10-adrv9002-rx2tx2.dts]]| | |adi,adrv9002-rx2tx2|MIMO|[[linux.github>adrv9001?arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-adrv9002-rx2tx2.dts| zynqmp-zcu102-rev10-adrv9002-rx2tx2.dts]]| |
|adi,adrv9002|Independent mode|[[linux.github>adrv9001?arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-adrv9002.dts| zynqmp-zcu102-rev10-adrv9002.dts]]| | |adi,adrv9002|Independent|[[linux.github>adrv9001?arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-adrv9002.dts| zynqmp-zcu102-rev10-adrv9002.dts]]| |
| |
In "MIMO" mode, only one DMA buffer is used and both RX1/RX2 physical ports are mapped into the RX1 channel in the hdl axi core. The same happens for TX. For the hdl core is as TX2/RX2 don't exist. As the name implies, this is useful for use cases as MIMO/Diversity. Naturally, in this case, both RX1/RX2 must have the same baseband sample rate. | In "MIMO" mode, only one DMA buffer is used and both RX1/RX2 physical ports are mapped into the RX1 channel in the hdl axi core. The same happens for TX. For the hdl core is as TX2/RX2 don't exist. As the name implies, this is useful for use cases as MIMO/Diversity. Naturally, in this case, both RX1/RX2 must have the same baseband sample rate. |