This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Last revision Both sides next revision | ||
resources:tools-software:linux-drivers:iio-transceiver:adrv9002 [14 Mar 2022 16:38] Nuno Sá [Local Oscillator Control (LO)] |
resources:tools-software:linux-drivers:iio-transceiver:adrv9002 [24 May 2023 14:50] Michael Hennerich [Profiles] |
||
---|---|---|---|
Line 398: | Line 398: | ||
ADRV9002 uses profiles to designate different device configuration settings for the Tx/Rx channels. The profile dictates how the digital filters, analog filters, clock rates, and clock dividers are configured in the device. Some specific parameters set by profiles include the IQ data rate, ADC clock rate, analog filter corners, FIR filter coefficients, and interpolation/decimation factors in the half-band filters. | ADRV9002 uses profiles to designate different device configuration settings for the Tx/Rx channels. The profile dictates how the digital filters, analog filters, clock rates, and clock dividers are configured in the device. Some specific parameters set by profiles include the IQ data rate, ADC clock rate, analog filter corners, FIR filter coefficients, and interpolation/decimation factors in the half-band filters. | ||
- | Several profiles can be examined in the ADRV9002 Transceiver Evaluation Software for given device clock frequencies. If the desired profile exists in the software, it is recommended to set up the desired profile in and use the generated JSON file by pressing the ''Generate Profile File'' button. Custom profiles can be generated using other ADI software tools not described here [[adi>en/design-center/landing-pages/001/transceiver-evaluation-software.html|MATLAB Profile/Filter Generator for ADRV9002]]. | + | Several profiles can be examined in the ADRV9002 Transceiver Evaluation Software for given device clock frequencies. If the desired profile exists in the software, it is recommended to set up the desired profile in and use the generated JSON file by pressing the ''Generate Profile File'' button. Custom profiles can be generated using other ADI software tools not described here [[adi>en/design-center/landing-pages/001/transceiver-evaluation-software.html|ADRV9002 transceiver evaluation software (TES) ]]. |
There are some constraints with the loaded profiles due to the architecture of the reference design: | There are some constraints with the loaded profiles due to the architecture of the reference design: |